RSL10 Sensor Development Kit - Industrial Sensing

Table of contents

image

 

{tabbedtable} Tab Label Tab Content
About

The RSL10 Sensor Development Kit is a compact and a comprehensive platform to easily develop IoT applications with leading sensor technology and the industry's lowest power Bluetooth ® Low Energy SoC. Several applications including industrial wearables, asset monitoring, smart sensing solutions can be easily developed on this platform.

 

image

 

 

The compact platform features a full range of sensors including environmental, inertial (3-axis accelerometer, 3-asix gyroscope and a low-power smart hub for motion sensing), a geomagnetic sensor, and an ambient light sensor. Example use cases and detailed documentation are provided in the CMSIS pack.

 

In addition to monitoring the various sensor values, the accompanying mobile application (RSL10 Sense and Control), connects to several cloud services (AWS, IBM®, Azure ™, etc.) enabling a true end-to-end solution development.

 

There are two variants of the RSL10 Sensor Kit:

 

  • RSL10-SENSE-GEVK (base version)
  • RSL10-SENSE-DB-GEVK (debug version)

 

Note: Either of the above kits will be roadtested.

 

Both variants ship with a CR2032 coin cell battery and a flexible NFC Antenna. On the debug (-DB) variant, the 10-pin debug header is populated and a Segger J-Link LITE CortexM debugger that connects to this header is also shipped.

 

A needle connector (E.g.:TC2050 ) is required on the base variant for debugging.

 

Additional Information

Important Dates

Enrollment Begin: June 24 2019

Enrollment Ends: July 24 2019

RoadTesters Selected: Aug 5 2019

Product Shipped: Aug 7 2019

RoadTesting Begins: Aug 14 2019

Reminder/Update Email: Sept 14 2019

Submit Reviews By: Oct 14 2019

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest

Terms and Conditions

RSL10 Sensor Development Kit

These are the terms and conditions which govern theRSL10 Sensor Development Kit contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on July 24 2019

Announcement of Winner (estimated): Aug 4 2019 2019

Prize: RSL10 Sensor Development Kit
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
  • One of the big questions, which I think is quite difficult to answer if you only have one of the variants (Debug version vs. non-debug), is which variant to choose. There will certainly be strengths and weaknesses between the two that only a road test can unravel if a road-tester had both to look at. I'm still trying to work out which is better for what purposes etc. Maybe others can see it clearer than I can. I would be intrigued to learn as surely a debug version does everything a non debug version would do.

Comment
  • One of the big questions, which I think is quite difficult to answer if you only have one of the variants (Debug version vs. non-debug), is which variant to choose. There will certainly be strengths and weaknesses between the two that only a road test can unravel if a road-tester had both to look at. I'm still trying to work out which is better for what purposes etc. Maybe others can see it clearer than I can. I would be intrigued to learn as surely a debug version does everything a non debug version would do.

Children
No Data