Avnet PicoZed XC7Z010 + FMC Carrier Card

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

PicoZed™ is a highly flexible, rugged, System-On-Module, or SOM that is based on the Xilinx Zynq®-7000 All Programmable SoC. It offers designers the flexibility to migrate between the 7010, 7015, 7020, and 7030 Zynq-7000 All Programmable SoC devices in a pin-compatible footprint.

 

The PicoZed module contains the common functions required to support the core of most SoC designs, including memory, configuration, Ethernet, USB, and clocks. It provides easy access to over 100 user I/O pins through three I/O connectors on the backside of the module. These connectors also support access to dedicated interfaces for Ethernet, USB, JTAG, power and other control signals, as well as the GTP/GTX transceivers on the 7015/7030 models.

 

The transceiver based 7015 and 7030 versions of PicoZed are a superset of the 7010/7020 version, adding four high-speed serial transceiver ports to the I/O connectors. Designers can simply design their own carrier card, plug-in PicoZed, and start their application development with a proven Zynq-7000 All Programmable SoC sub-system.

image

image

Important Dates

Enrollment Begin: Aug 5 2019

Enrollment Ends: Sept 13 2019

RoadTesters Selected: Sept 23 2019

Product Shipped: Sept 24 2019

RoadTesting Begins: Oct 1 2019

Reminder/Update Email: Nov 1 2019

Submit Reviews By: Dec 1 2019

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTester

Terms and Conditions

RoadTest

Terms and Conditions

Avnet PicoZed XC7Z010 + FMC Carrier Card

These are the terms and conditions which govern theAvnet PicoZed XC7Z010 + FMC Carrier Card contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 13 2019

Announcement of Winner (estimated): Sept 15 2019

Prize: Avnet PicoZed XC7Z010 + FMC Carrier Card
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
  • That breakout board appears to have a PCI-e connector in addition to the FMC connector: someone clever could drop the correct IP blocks into their Vivado design to interface their Zynq project to a host PC via PCI-e, write the associated source code for the Zynq-7000 and write PC drivers/software to do something impressive on the PC. Effectively you could make your own bespoke PC card to do whatever it is you cannot actually buy....that's really awesome !

  • wow this requires a lot of knowledge ....but great...

  • Hi   - don't let my comment put you off applying. You don't need to understand or use the PCI-e slot to experiment and roadtest the board. It is just an additional feature that could be used if someone wants to image

  • Please read me comment to Attila.

     

    I had talked to one of the Avnet product specialists about this board. I knew going into this roadtest that there were some limitations. But like everyone I work with limitations. I wanted to get the PicoZed involved in the roadtest program, but I also had some budget restrictions. If the roadtest group is really excited about this board, I can bring your feedback to my boss and we can plan a future roadtest.

     

    Randall

Comment
  • Please read me comment to Attila.

     

    I had talked to one of the Avnet product specialists about this board. I knew going into this roadtest that there were some limitations. But like everyone I work with limitations. I wanted to get the PicoZed involved in the roadtest program, but I also had some budget restrictions. If the roadtest group is really excited about this board, I can bring your feedback to my boss and we can plan a future roadtest.

     

    Randall

Children
  • Ok - thanks for the correction. I saw the PCI-e on the FMC carrier card and thought it could be the ideal 'extra' that some clever person was looking for. Sometimes it is better not to overcomplicate things anyway image

     

    I look forward to seeing what the selected roadtesters get up to with this board.