Experiment with Blockchain Tech

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

What is Blockchain and How Do I use it?

Blockchain technology is perhaps the most talked about topic in the tech world today. The buzz about it started with  cryptocurrencies, but the use of blockchain technology for IoT security has a lot of potential for many industry verticals and counteless number of applications.

 

If I am New To Blockchain Technology, How Do I Get Started?

In a nutshell, blockchain is a decentralized digital ledger that manages a continuously growing list of data points (chain of blocks). Every block is cryptographically linked to the previous block. The ledger records all transactions which are used to send assets (e.g. crypto currency) from one account to another. Each transaction is protected by a digital signature. To create such a digital signature, a secret private key that corresponds to the public key of an account is needed.

 

Why is Blockchain so important to security?

The private key of a user plays a critical role. If the private key is lost, all assets are lost. Moreover, if the private key is stolen and hacked, the attacker has full access to all assets which allows the creation of seemingly valid transactions. Private key storage requires best possible protection! Hardware-based security tokens are the most effective way against attacks and unauthorized access.

 

An Easy way to Experiment with Blockchain Technology

Infineon’s Blockchain Security 2Go starter kit features hardware-based protection mechanisms to generate and store private keys in a secured way. The starter kit is a fast and easy way to design of Blockchain applications.It supports an evaluation environment for many different kinds of Blockchain technologies. It provides a lean feature set as well as open source application examples, which enable new ideas to flourish and to generate a secured physical link from the digital to the real world.

 

The Blockchain Security 2Go starter kit includes:

  • Five ready-to-use NFC cards, supporting basic blockchain functionalities such as secure
  • key generation, signing methods, pin protection and many more
  • On-card software that supports commands for key-management, signature creation
  • and PIN authentication
  • Access to Infineon’s blockchain git hub: Open source example application code, such as
  • a smartphone app operating with the card

image

Where to get support

https://github.com/Infineon/Blockchain

 

For more Information

Important Dates

Enrollment Begin: Aug 8 2019

Enrollment Ends: Sept 9 2019

RoadTesters Selected: Oct 21 2019

Product Shipped: Oct 24 2019

RoadTesting Begins: Oct 31 2019

Reminder/Update Email: Dec 1 2019*

Submit Reviews By: Jan 1 2020*

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

Terms and Conditions

These are the terms and conditions which govern theBlockchain Security 2Go Starter Kite contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Blockchain Security 2Go Starter Kit

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 9 2019

Announcement of Winner (estimated): Sept 16 2019

Prize: Blockchain Security 2Go Starter Kit
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
  • To all roadtesters.....

     

    This was a "first ever" roadtest for this kind of product, so I expected me might experience some hiccups. that's fine. I see it as the nature of the work.

     

    I was told today that you need an Andriod device.

     

    Also, a need for an NFC card reader.

     

    question: what else do you need for this roadtest?

     

    Randall

  • Would like to know more for the compatibility of NFC card reader for the given Infineon's Security2Go specific card, denying the use of Android device.

  • This is to all roadtesters....

     

    I went to the user manual for this product. Initially it just says you need an NFC enabled smart phone.

     

    Then I read this:

     

    In contrast to a standard NFC USB reader, the reader antenna of mobile devices is not always located around the center. If you have troubles when communicating with the Blockchain Security 2Go cards, investigate the positioning of the card in combination with the used NFC phone. Figure 9 shows the backside of a Google Pixel smartphone. In this case the NFC antenna is located in the upper area of the smartphone. For more details check out the hardware diagram of the Pixel smartphone [13].

     

    The manual uses an Andriod phone as an example....

     

    So, my question is: Are people with android phones having problems? I presume they should not. Perhaps there is another issue?

     

    Randall

  • As long as they are on Android 7.0 or up it shouldn't be a issue.

Comment Children
No Data