Keithley 2450 SMU with I-V Tracer Software

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

1. RoadTest Overview

In this roadtest, we would like you to test and experiment with both the Keithley 2450 SourceMeter Instrument and the I-V Tracer software, and report your experiences and final conclusions.

 

To provide you with more information about the Keithley 2450 SourceMeter Instrument and the I-V Tracer software, we have posted detailed information about the product, along with various supplementary information and links to the manuals on the Tektronix website.

 

2. Introduction to the Keithley Model 2450 SourceMeter Instrument

Keithley Model 2450 SourceMeter Instrument is the fourth-generation member of Keithley’s SourceMeter family of SMU instruments. It offers a highly flexible, four-quadrant voltage and current source/load coupled with precision voltage and current meters. This all-in-one instrument gives you the capabilities of a:

  • Precision power supply with V and I readback
  • True current source
  • Digital multimeter (DCV, DCI, ohms, and power with 6½-digit resolution)
  • Precision electronic load
  • Trigger controller

 

The 2450 is Keithley’s next-generation SourceMeter source measure unit (SMU) instrument that truly brings Ohm’s law (current, voltage, and resistance) testing right to your fingertips. Its innovative graphical user interface (GUI) and advanced, capacitive touchscreen technology allow intuitive usage and minimize the learning curve to enable engineers and scientists to learn faster, work smarter, and invent easier.

imageimage

The 2450 is the SMU for everyone: a versatile instrument, particularly well-suited for characterizing modern scaled semiconductors, nano-scale devices and materials, organic semiconductors, printed electronics, and other small-geometry and low-power devices. All this combined with Keithley SMU precision and accuracy allows users to Touch, Test, Invent® with the new favorite go-to instrument in the lab for years to come.

image

 

Unlike conventional instruments with dedicated pushbutton technology and small, obscure, limited-character displays, the 2450 features a five-inch, full-color, high-resolution touchscreen that facilitates ease of use, learning, and optimizes overall speed and productivity. A simple icon-based menu structure reduces configuration steps by as much as 50 percent and eliminates the cumbersome multi-layer menu structures typically used on soft-key instruments. Built-in, context-sensitive help enables intuitive operation and minimizes the need to review a separate manual. These capabilities combined with its application versatility make the 2450 the SMU instrument inherently easy to use for basic and advanced measurement applications, regardless of your experience level with SMU instruments.

 

Key Features

  • Capabilities of analyzers, curve tracers, and I-V systems at a fraction of their cost
  • Five-inch, high resolution capacitive touchscreen GUI
  • 0.012% basic measure accuracy with 6½-digit resolution
  • Enhanced sensitivity with new 20mV and 10nA source/measure ranges
  • Source and sink (four-quadrant) operation
  • Four “Quickset” modes for fast setup and measurements
  • Built-in, context-sensitive front panel help
  • Front panel input banana jacks; rear panel input triaxial connections
  • 2450 SCPI and TSP® scripting programming modes
  • 2400 SCPI-compatible programming mode
  • Front panel USB memory port for data/programming/configuration I/O

 

3. Package Contents

  • 2450 SourceMeter® unit
  • Calibration Certificate
  • CS-1616-3 safety interlock mating connector
  • Power Cable
  • USB-B-1 USB cable, Type A to type B
  • CA-180-3A TSP-link/Ethernet cable
  • 4mm Safety test lead kit (012173001)
  • Kickstart start-up software (supplied on CD)
  • Quick start guide

 

4. I-V Tracer Software

Keithley I-V Tracer Software leverages the unique touchscreen interface of the 2400 Series SourceMeter® Source Measure Unit (SMU) instruments to recreate the familiar user experience of a curve tracer for two-terminal devices. Adding the I-V Tracer to your SourceMeter instrument gives you a dedicated user interface for tracing the characteristics of your devices through both current and voltage. With a range of compatible instruments, I-V Tracer can utilize the full capabilities of each source measure unit, including the dual high-speed digitizers of the 2461 to perform tracing with AC polarity and pulsed DC, in addition to standard DC polarity.

image

 

Tektronix introduced the industry’s first curve tracer in 1955 to display characteristic curves for vacuum tubes, followed over the years by models for testing transistors, diodes and other solid-state devices. Approximating a power supply and an oscilloscope packaged in the same box, curve tracers source voltage while plotting voltage vs. current. For labs that prefer to continue using traditional curve tracers, the reliance on vintage instrumentation presents its share of obstacles. Keeping existing instruments functional requires sourcing and stocking old replacement components, and the large footprint consumes limited lab space. Traditional curve tracers also have no methods for easily capturing and sharing data.

 

This all changes with Keithley I-V Tracer Software. Since an SMU can source voltage or current while measuring voltage and current, it has similar hardware qualities to a curve tracer. Rather than pooling resources for shared, outdated equipment, labs can now equip individual engineers with their own I-V curve tracer for applications in failure analysis, semiconductor R&D, and education.

 

Key Features

  • Compatible with Keithley 2450, 2460, 2461, and 2470 Graphical SourceMeter SMUs
  • +DC, –DC, AC polarity modes (AC mode only compatible with the 2461 SMU)
  • Compare mode to display a reference device next to a measured curve
  • Save curve data to disk with KickStart for analysis in Excel
  • Screen capture curves
  • Pinch and zoom on the touchscreen to analyze data immediately
  • Current sourcing capabilities allowing the user to sweep current across the device and plot current versus voltage

 

Roadtesters will be given 1 free license for I-V Tracer.  They will be contacted when their units ship with instructions for installing I-V Tracer on their 2450.

 

5. Additional Information

 

6. Informational Videos

  • Go to the following pages to watch several informational videos:

https://www.tek.com/keithley-source-measure-units/keithley-smu-2400-series-sourcemeter

https://www.tek.com/keithley-i-v_tracer

Important Dates

Enrollment Begin: Mar 5 2020

Enrollment Ends: Apr 8 2020

RoadTesters Selected: May 3 2020

Product Shipped: May 8 2020

RoadTesting Begins: May 15 2020

Reminder/Update Email: June 15 2020*

Submit Reviews By: August 15 2020*

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest

Terms and Conditions

These are the terms and conditions which govern the Keithley 2450 SMU with I-V Tracer Software contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment or component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

 

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Keithley 2450 SMU with I-V Tracer Software

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Apr 8 2020

Announcement of Winner (estimated): Apr 13 2020

 

Prize: TKeithley 2450 SMU with I-V Tracer Software
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
U.S. Tax  ResponsibilityFor U.S. taxpayers, an official roadtester will be required to complete a W-9 form prior to element14 shipping you the unit. Taxpayers from other countries need to follow the tax code in their resident countries. (See 3.6 of Terms and Conditions).
Comment List
Anonymous
Parents
  • Just wondering, did you guys get a permanent or trial version of Kickstart?

  • I am running on a trial of KickStart, as I have been informed that the KICKSTARTFL-BASE is not included in this RoadTest. However, I've also been told by the representative that the node-locked license for I-V Tracer (KICKSTARTNL-ACT1) can be deployed and updated without the need for the KICKSTARTFL-BASE license.

     

    However, in my instance, the I-V Tracer app license seems to come up as a 1-year "trial" which is very confusing and I've since tried to follow up with Keithley/Tektronix without a clear answer as to why.

     

    I'm also following up with them and awaiting a resolution to some unusual behaviour with my unit that suggests there may be a fault (inability to reliably source current in the 200V range causing issues with spurious overheat/output shutdown messages and strange noises, wildly incorrect readings during I-V Characteriser runs especially with current measurements in the uA/nA ranges, failure to auto-range with Overflow message and output offset voltages jumping wildly). It appears that the current COVID-19 situation is causing a delay in responses but I am still committed to delivering my RoadTest on time if at all possible.

     

    - Gough

Comment
  • I am running on a trial of KickStart, as I have been informed that the KICKSTARTFL-BASE is not included in this RoadTest. However, I've also been told by the representative that the node-locked license for I-V Tracer (KICKSTARTNL-ACT1) can be deployed and updated without the need for the KICKSTARTFL-BASE license.

     

    However, in my instance, the I-V Tracer app license seems to come up as a 1-year "trial" which is very confusing and I've since tried to follow up with Keithley/Tektronix without a clear answer as to why.

     

    I'm also following up with them and awaiting a resolution to some unusual behaviour with my unit that suggests there may be a fault (inability to reliably source current in the 200V range causing issues with spurious overheat/output shutdown messages and strange noises, wildly incorrect readings during I-V Characteriser runs especially with current measurements in the uA/nA ranges, failure to auto-range with Overflow message and output offset voltages jumping wildly). It appears that the current COVID-19 situation is causing a delay in responses but I am still committed to delivering my RoadTest on time if at all possible.

     

    - Gough

Children
  • But with I-V licence you still can't do the I-V tracing the usual way, can you? Can you share more details on your issues, I suspect we may have some issues in common...

  • How do you mean by "the usual way"?

     

    The license gives access to the I-V Tracer app which can be installed through Kickstart V2.3.0 (or later) onto the 2450. This can only happen if you've updated the 2450's firmware to 1.7.1 which is the first firmware to support this feature. My unit was shipped with firmware 1.6.7, so that was the first thing I did. Once you have imported the license into your TekAMS account, installed Kickstart onto your computer, checked out the license from TekAMS with your Host ID (a .lic file) which may require you to create a site for the license to be used at, you should be able to add it to the Kickstart list of licenses:

    image

     

    Then, you need to install it onto the instrument through Kickstart by launching it with the intended instrument connected. Either you will be prompted, or you can use a button from the lower toolbar to install it into the instrument.

    image

     

    Once successful, the state of the licenses should be like this - note the 1-year trial for some reason which I'm still trying to get an answer about from Keithley/Tek:

    image

     

    Once installed, on the 2450 you'll find it under Apps via the main menu. The app runs solely on the 2450. If you're on the desktop, you will see I-V Tracer app under Kickstart, but it won't actually do anything except allowing you to readout the table of values used to create the I-V Tracer graph and draw the graph on the computer as well, if I recall correctly.

    image

     

    I-V Characteriser, which is the PC-controlled way of I-V measurement, is part of the Kickstart license and not the I-V Tracer license. Likewise the Sweep Generator and Graphing display is part the 2450's onboard features and is always available.

     

    As for the other issues, I'll send you a PM soon and follow up.

     

    - Gough

  • Hi Gough

     

    This must be a glitch. I finally received the license, it was just a mistake that it wasn't sent sooner. Everything looks fine when I add it to the list in kickstart:

    image

  • Did you get a  KickStart license as well?

  • No, I already had this one. It was a special offer that was bundled with a DMM6500

  • Did you check the status of the license from the I-V Tracer installer module inside Kickstart? That's where I had the trial date dialog seen above. The main licenses data is much the same.

     

    - Gough

  • It is not showing as a trial, so I assume the license is recognized.

     

    image

  • Hmm. It seems then the issue may be related to activating a full license for I-V Tracer on an evaluation copy of KickStart, which I was told by the rep, should not have been a problem. Thanks for the information - I'll feed this back to them.

     

    - Gough