Keithley 2450 SMU with I-V Tracer Software

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

1. RoadTest Overview

In this roadtest, we would like you to test and experiment with both the Keithley 2450 SourceMeter Instrument and the I-V Tracer software, and report your experiences and final conclusions.

 

To provide you with more information about the Keithley 2450 SourceMeter Instrument and the I-V Tracer software, we have posted detailed information about the product, along with various supplementary information and links to the manuals on the Tektronix website.

 

2. Introduction to the Keithley Model 2450 SourceMeter Instrument

Keithley Model 2450 SourceMeter Instrument is the fourth-generation member of Keithley’s SourceMeter family of SMU instruments. It offers a highly flexible, four-quadrant voltage and current source/load coupled with precision voltage and current meters. This all-in-one instrument gives you the capabilities of a:

  • Precision power supply with V and I readback
  • True current source
  • Digital multimeter (DCV, DCI, ohms, and power with 6½-digit resolution)
  • Precision electronic load
  • Trigger controller

 

The 2450 is Keithley’s next-generation SourceMeter source measure unit (SMU) instrument that truly brings Ohm’s law (current, voltage, and resistance) testing right to your fingertips. Its innovative graphical user interface (GUI) and advanced, capacitive touchscreen technology allow intuitive usage and minimize the learning curve to enable engineers and scientists to learn faster, work smarter, and invent easier.

imageimage

The 2450 is the SMU for everyone: a versatile instrument, particularly well-suited for characterizing modern scaled semiconductors, nano-scale devices and materials, organic semiconductors, printed electronics, and other small-geometry and low-power devices. All this combined with Keithley SMU precision and accuracy allows users to Touch, Test, Invent® with the new favorite go-to instrument in the lab for years to come.

image

 

Unlike conventional instruments with dedicated pushbutton technology and small, obscure, limited-character displays, the 2450 features a five-inch, full-color, high-resolution touchscreen that facilitates ease of use, learning, and optimizes overall speed and productivity. A simple icon-based menu structure reduces configuration steps by as much as 50 percent and eliminates the cumbersome multi-layer menu structures typically used on soft-key instruments. Built-in, context-sensitive help enables intuitive operation and minimizes the need to review a separate manual. These capabilities combined with its application versatility make the 2450 the SMU instrument inherently easy to use for basic and advanced measurement applications, regardless of your experience level with SMU instruments.

 

Key Features

  • Capabilities of analyzers, curve tracers, and I-V systems at a fraction of their cost
  • Five-inch, high resolution capacitive touchscreen GUI
  • 0.012% basic measure accuracy with 6½-digit resolution
  • Enhanced sensitivity with new 20mV and 10nA source/measure ranges
  • Source and sink (four-quadrant) operation
  • Four “Quickset” modes for fast setup and measurements
  • Built-in, context-sensitive front panel help
  • Front panel input banana jacks; rear panel input triaxial connections
  • 2450 SCPI and TSP® scripting programming modes
  • 2400 SCPI-compatible programming mode
  • Front panel USB memory port for data/programming/configuration I/O

 

3. Package Contents

  • 2450 SourceMeter® unit
  • Calibration Certificate
  • CS-1616-3 safety interlock mating connector
  • Power Cable
  • USB-B-1 USB cable, Type A to type B
  • CA-180-3A TSP-link/Ethernet cable
  • 4mm Safety test lead kit (012173001)
  • Kickstart start-up software (supplied on CD)
  • Quick start guide

 

4. I-V Tracer Software

Keithley I-V Tracer Software leverages the unique touchscreen interface of the 2400 Series SourceMeter® Source Measure Unit (SMU) instruments to recreate the familiar user experience of a curve tracer for two-terminal devices. Adding the I-V Tracer to your SourceMeter instrument gives you a dedicated user interface for tracing the characteristics of your devices through both current and voltage. With a range of compatible instruments, I-V Tracer can utilize the full capabilities of each source measure unit, including the dual high-speed digitizers of the 2461 to perform tracing with AC polarity and pulsed DC, in addition to standard DC polarity.

image

 

Tektronix introduced the industry’s first curve tracer in 1955 to display characteristic curves for vacuum tubes, followed over the years by models for testing transistors, diodes and other solid-state devices. Approximating a power supply and an oscilloscope packaged in the same box, curve tracers source voltage while plotting voltage vs. current. For labs that prefer to continue using traditional curve tracers, the reliance on vintage instrumentation presents its share of obstacles. Keeping existing instruments functional requires sourcing and stocking old replacement components, and the large footprint consumes limited lab space. Traditional curve tracers also have no methods for easily capturing and sharing data.

 

This all changes with Keithley I-V Tracer Software. Since an SMU can source voltage or current while measuring voltage and current, it has similar hardware qualities to a curve tracer. Rather than pooling resources for shared, outdated equipment, labs can now equip individual engineers with their own I-V curve tracer for applications in failure analysis, semiconductor R&D, and education.

 

Key Features

  • Compatible with Keithley 2450, 2460, 2461, and 2470 Graphical SourceMeter SMUs
  • +DC, –DC, AC polarity modes (AC mode only compatible with the 2461 SMU)
  • Compare mode to display a reference device next to a measured curve
  • Save curve data to disk with KickStart for analysis in Excel
  • Screen capture curves
  • Pinch and zoom on the touchscreen to analyze data immediately
  • Current sourcing capabilities allowing the user to sweep current across the device and plot current versus voltage

 

Roadtesters will be given 1 free license for I-V Tracer.  They will be contacted when their units ship with instructions for installing I-V Tracer on their 2450.

 

5. Additional Information

 

6. Informational Videos

  • Go to the following pages to watch several informational videos:

https://www.tek.com/keithley-source-measure-units/keithley-smu-2400-series-sourcemeter

https://www.tek.com/keithley-i-v_tracer

Important Dates

Enrollment Begin: Mar 5 2020

Enrollment Ends: Apr 8 2020

RoadTesters Selected: May 3 2020

Product Shipped: May 8 2020

RoadTesting Begins: May 15 2020

Reminder/Update Email: June 15 2020*

Submit Reviews By: August 15 2020*

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest

Terms and Conditions

These are the terms and conditions which govern the Keithley 2450 SMU with I-V Tracer Software contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment or component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

 

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Keithley 2450 SMU with I-V Tracer Software

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Apr 8 2020

Announcement of Winner (estimated): Apr 13 2020

 

Prize: TKeithley 2450 SMU with I-V Tracer Software
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
U.S. Tax  ResponsibilityFor U.S. taxpayers, an official roadtester will be required to complete a W-9 form prior to element14 shipping you the unit. Taxpayers from other countries need to follow the tax code in their resident countries. (See 3.6 of Terms and Conditions).
Comment List
Anonymous
Parents
  • To all applicants....

     

    I'm going through the first read of all the applications.

     

    Only one application was incomplete. All the other 71 applications with be included in the package I send to the sponsor, along with my recommendations.

     

    Overall, a lot of great applications. Total, it's 104 pages of applications. Now for my 2nd reading...

     

    Randall Scasny

    RoadTest Program Manager

  • Thanks for the update, Randall.

    I expect the review to take longer than usual due to the Corona-Virus situation.

    Cheers,

    M.

Comment Children
No Data