Microduino Quadcopter Kit

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The build-it-yourself Microduino Quadcopter is a flying four-motor rotorcraft controllable with the included Microduino Joypad. The Microduino Series is our original product, created for those looking for the most flexibility in their DIY projects. Its quarter-sized profile makes it easier to integrate into projects of all shapes and sizes. Smart, flexible, and compatible with the Arduino ecosystem, designers have everything they need to build their own applications.

image

Detailed Description

The Microduino Quadcopter is a flying four motor rotorcraft kit. The kit is designed to be fun and easy to assemble. When building this, kids learn about the different modules and the functions required to create the quadcopter.

 

Positioning and Orientation

The quadcopter utilizes a 3-axis accelerometer and a 3-axis gyroscope chip (MPU-6050) to determine its positioning and orientation. With this data, the quadcopter’s motors are able to compensate for orientation during operation.

 

Wireless Control

The CoreRF module (Core + nRF) adds wireless communication to the Microduino Quadcopter. The quadcopter can be remotely controlled by the included Microduino Joypad. Additionally, the included Microduino Joypad can be reprogrammed and used for other projects.

 

Microduino Series Modules

This kit incorporates various Microduino Series modules. The Microduino Series is a set of modules which are Arduino compatible, have a small form factor, stack-able, modular, and reusable. The modules were designed for hobbyists and tinkers to quickly create and prototype projects.

 

A Complete Kit

The kit contains everything needed to make the Microduino Quadcopter. Electronic hardware from the embedded processor (CoreRF module) to the motors and propellers are included. Also included are frame pieces for the quadcopter. A recharge-able battery is also included which can be recharged with a MicroUSB Cable plugged into the base board. The Open Source code is provided and can be modified for personal customization. Similarly, the Microduino Joypad contains everything needed to be assembled (including the rechargable li-ion battery).

 

Additional Information

Tutorial

Important Dates

Enrollment Begin: June 20 2020

Enrollment Ends: July 20 2020

RoadTesters Selected: July 23 2020

Product Shipped: July 24 2020

RoadTesting Begins: July 30 2020

Reminder/Update Email: Aug 30 2020

Submit Reviews By: Oct 15 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTester

Terms and Conditions

Microduino Quadcopter Kit – RoadTest

Terms and Conditions

These are the terms and conditions which govern the Microduino Quadcopter KitRoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on July 20 2020

Announcement of Winner (estimated): July 21 2020

Prize:  Microduino Quadcopter Kit
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
  • Important dates update

     

    Enrollment Begin: June 20 2020

    Enrollment Ends: July 20 2020

    RoadTesters Selected: July 23 2020

    Product Shipped: July 24 2020

    RoadTesting Begins: July 30 2020

    Reminder/Update Email: Aug 30 2020

    Submit Reviews By: Sept 30 2020

    *The element14 RoadTest Staff will send this reminder/update email.

    **If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

     

  • Needing some help with Road Test - is there someone from the microduino team available for something simple ?

    installed Arduino IDE for Microduino 1.8.4  per tutorials

    https://wiki.microduinoinc.com/Microduino-Quadcopter_Tutorial

    https://wiki.microduinoinc.com/Microduino-Joypad_Getting_start

    https://wiki.microduinoinc.com/Quadcopter_Kit:_Quickstart_Guide

    https://wiki.microduinoinc.com/AVR_Core%EF%BC%9AGetting_started

    https://wiki.microduinoinc.com/Getting_started:_Microduino_IDE_for_Windows

     

    Joypad - Use cable to connect Microduino-USBTTL, and stack it together with your core to prepare to upload the program.

    • Note:You’d better upload the program before stacking all modules together.

     

     

    The board detected by the IDE is supposed to br MicroDuino Core (328p).

    I cant select this type of board.

    I've searched the BOARDS MANAGER, have Arduino AVR boards installed and Marduino SAM boards installed ,find nothing for microduino.

     

    Using the board selection shown, after the joypad code compiles, and tries to load , it returns an error:

             System wide configuration file is "C:\Program Files (x86)\Arduino IDE for Microduino-1.8.4-V6.0\hardware\tools\avr/etc/avrdude.conf"

     

             Using Port                    : COM3

             Using Programmer              : arduino

             Overriding Baud Rate          : 115200

    avrdude: stk500_getsync() attempt 1 of 10: not in sync: resp=0x00

    avrdude: stk500_recv(): programmer is not responding

     

    The same error occurs when using MicroDuino TTLUSB-C alone or when piggybacked with MicroDuino Core-RF ( there are 2 RF boards, both behaved the same)

     

    image

    image

     

    looking for suggestions to move forward loading code

    Thanks

    Gary

  • umm, as I remember you might have to install a zip package to add boards.

    Let me try with my Arduino IDE...

     

    Nope/

     

    I've searched this, I think there's a separate Arduino IDE revised version that Microduino made for their products.

     

    It's the last link in your list.

  • Thanks Hugo

    Yep MicroDuino is a separate tool load (1.8.4) that seems to coexist peacefully with the regular Arduino IDE ( Im using 1.8.12)

    image

    The quadcopter and joypad both have zip files that include their .ino.

     

    I havent found anything useful on Arduino's FAQ or Forum yet.

     

    Instructions says the board pick should look like this, but mine wont get there ( see my prior post for what I get )

    image

  • Hmm

    Did you install the Microduino thing and then the drivers?

  • Thanks Hugo, yes drivers and tools installed .

    very very strange

    After some fiddling, the software download was successful with the settings I used that didnt work before. so life goes on.

    Thanks for comments !  Gary

  • That’s good, good luck on your roadtest.

    Who knows I might find you for help if I get accepted for a roadtest

  • After scouring You Tube for examples, and Arduino CC for FAQs and Forums,........I did find in the Quadcopter Quickstart the Core-RF board selection similar to what I had previously used.. The other tutorials showed using a different board selection in the Arduino for MicroDuino IDE. The Quickstart must have been older referring the the Core-RF as 127rfa1  whereas my Core-RF is a 128rfa1)

     

    Today I retried Joypad, and the JoyPad software loaded to the Core-RF.

    Diagnostics lines showed:

             Using Port                    : COM3

             Using Programmer              : arduino

             Overriding Baud Rate          : 57600

          

    One of the diagnostic files I had saved, from a failed attempt, overrode the Baud Rate to 115200, so either I inadvertently fat fingered a board pick or the PC and boards needed to reboot with installed software to initialize correctly.

    So thank you to all the comments and suggestions. I look forward to putting this bird in the air.

  • I see in an earlier post you put a call out for vendor support, did that produce any returns?

  • No Sean it didnt this time, but its OK.

    I'd done previous Road Tests with the vendor was actually watching the chat traffic closely and offering to help. In those cases, there were alot more kits on trial, and higher complexity..

     

    In this case, there is only one kit being Road Tested, The vendor appears to be in Japan, which automatically adds 48 hrs to even the fastest response. I took a shot at iit.

     

    Element14 community is only one way of many to get advice and collaboration.

    I also just found the link to contact the vendor directly, a much better way to request clarifications. :-)

Comment
  • No Sean it didnt this time, but its OK.

    I'd done previous Road Tests with the vendor was actually watching the chat traffic closely and offering to help. In those cases, there were alot more kits on trial, and higher complexity..

     

    In this case, there is only one kit being Road Tested, The vendor appears to be in Japan, which automatically adds 48 hrs to even the fastest response. I took a shot at iit.

     

    Element14 community is only one way of many to get advice and collaboration.

    I also just found the link to contact the vendor directly, a much better way to request clarifications. :-)

Children
  • I have an affinity for the RoadTest. It was a review I was hoping to secure. After reading your posts I am a bit relieved I wasn't awarded it. I'm not confident I would have had the knowledge to pull it off.

     

    Pulling on a thread of knowledge to find it takes you no where, I find frustrating. Lack of documentation and its poor quality seems to be a theme in RoadTests. I was going to suggest it be a scoring metric on the RoadTest Review post. I'm not sure if it would change the way vendors view documentation.

     

    Can you clarify the status. Have you succeeded in getting the vehicle off the ground? Other than carrying it to the car:)

  • Thanks Sean - This kit is labeled for ages 12+ , so it should be cookbook.

    There is alot of documentation, however there is maybe too much. The tutorial is not translated well and has old info in it. It seems a Quickstart guide was generated with alot of documentation improvements, however I started with the tutorial and kind of waded thru it, and then referenced the Quickstart Guide, and found some of my noted conflicts were answered. Some of the documents need condensed together with all updates.

     

    The quadcopter is still grounded. There is a simple procedure to execute using the JoyPad joysticks on quadcopter power up, to prove to the quadcopter it has a valid and active controller before enabling it to fly. I'm stuck there right now, and have emailed microduino for help. The procedure doesnt seem to be very dependable.

     

    I have several Flysky Radio controllers for my robot projects. Those RC controllers have a separate procedure called binding, selectable on the receiver by jumper, to acquire the signature of the transmitter and bind to it. Those radio controllers use spread spectrum on 2.4 Ghz , and this allows multiple controllers to operate in their immediate vicinity, and not to interfere with each other.   

     

    The joypad and quadcopter use a Microduino CoreRF is an AVR core board with 802.15.4 Wireless Protocol integrated. It supports any wireless modules based on 802.15.4 Protocol, including Zigbee, MAC/6LoWPAN and RF4CE. The 801.15. 4 uses a multi-code modulation technique called parallel sequence spread spectrum (PSSS). I copied and pasted this info. :-)  

     

    With this tidbit of knowledge, I wonder if the code of the Joypad and quadcopter could be hacked to get rid of this wacky and awful "pairing" routine that doesnt seem to work reliably since the Wiki says if it doesnt work, keep trying several times, and then if still doesnt work reboot everything and start again. I'd rather set an ID number in the JoyPad and use the Quadcopter code to load a matching ID number so the pairing happens automaticaly. If doesnt then the JoyPad says it doesnt see the quadcopter.

     

    I've unsuccessfully so far waded thru the software to find the code that drives that Blue LED, even if I had schematics, the silkscreen nomenclature doesnt always translate to the software name. I figured if I backtrack thru the code, maybe I can hack that particular permissive. All that takes alot of time and perserverence.

     

    The Joypad is pretty cool, the quadcopter is pretty solid hardware wise, however sitting on the ground trying to get a blue LED to light isnt very fun, and also considering I dont have faith that the document is accurate. 

  • Thanks GY for the share. I was reluctant to ask you questions for fear it would take away from your review. It sounds like you still have some obstacles to overcome before a review is on the horizon.

     

    My RoadTest Siretta Cellular Signal Strength Data Logger - Review was a struggle. The product was developed for Europe and then expanded to fill the American market. US cell phone networks use a different standard than Canadian cell phone networks. Lot's of things didn't work as described in the documentation.  It took a considerable bit of time and many remote log-ins to my home computer network in order for the vendor to gain access to the unit before a code release that worked was developed. I learned a lot from sharing with the vendor in England.

     

    I would expect with all that is published on the Microduino, that getting this product into the air would be relatively easy. It sound from your commentary you have considerable experience. I suspect like most companies the vendor is off to bigger and better things and the continued struggles in their old markets is something users have to live with.

     

    I picture these struggles coupled with kids saying "is it working yet" the formula for keeping kids for STEM:)

     

    I wish you the best of luck on your quad-copters first launch. I look forward to your RoadTest Review posting.

  • Please feel free to ask any questions, Ill see if I can give answers or insights. Questions can make thinking, testing, and report out better.

  • I do look forward to seeing your review.

     

    Maybe a few points to test:

     

    Remixing the code to do what you want

     

    Remixing the hardware, for better motors, better battery, etc.

  • Hugo - Seeing the design so far, the microduino itself with motion module could be retained to make a bigger copter, and retain joypad. The copter Shield is very limited to the motor driver current ( wire traces and component selection). The copter is using low inertia DC motors and gearboxes, which will likely need to be upgraded to outrigger brushless motors nd their drivers. The copter chassis is designed for a 3.3V battery 600 mAhr battery., which also limits motor size and flight time -- i.e. need also a new copter chassis for a bigger design.