Microduino Quadcopter Kit

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The build-it-yourself Microduino Quadcopter is a flying four-motor rotorcraft controllable with the included Microduino Joypad. The Microduino Series is our original product, created for those looking for the most flexibility in their DIY projects. Its quarter-sized profile makes it easier to integrate into projects of all shapes and sizes. Smart, flexible, and compatible with the Arduino ecosystem, designers have everything they need to build their own applications.

image

Detailed Description

The Microduino Quadcopter is a flying four motor rotorcraft kit. The kit is designed to be fun and easy to assemble. When building this, kids learn about the different modules and the functions required to create the quadcopter.

 

Positioning and Orientation

The quadcopter utilizes a 3-axis accelerometer and a 3-axis gyroscope chip (MPU-6050) to determine its positioning and orientation. With this data, the quadcopter’s motors are able to compensate for orientation during operation.

 

Wireless Control

The CoreRF module (Core + nRF) adds wireless communication to the Microduino Quadcopter. The quadcopter can be remotely controlled by the included Microduino Joypad. Additionally, the included Microduino Joypad can be reprogrammed and used for other projects.

 

Microduino Series Modules

This kit incorporates various Microduino Series modules. The Microduino Series is a set of modules which are Arduino compatible, have a small form factor, stack-able, modular, and reusable. The modules were designed for hobbyists and tinkers to quickly create and prototype projects.

 

A Complete Kit

The kit contains everything needed to make the Microduino Quadcopter. Electronic hardware from the embedded processor (CoreRF module) to the motors and propellers are included. Also included are frame pieces for the quadcopter. A recharge-able battery is also included which can be recharged with a MicroUSB Cable plugged into the base board. The Open Source code is provided and can be modified for personal customization. Similarly, the Microduino Joypad contains everything needed to be assembled (including the rechargable li-ion battery).

 

Additional Information

Tutorial

Important Dates

Enrollment Begin: June 20 2020

Enrollment Ends: July 20 2020

RoadTesters Selected: July 23 2020

Product Shipped: July 24 2020

RoadTesting Begins: July 30 2020

Reminder/Update Email: Aug 30 2020

Submit Reviews By: Oct 15 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTester

Terms and Conditions

Microduino Quadcopter Kit – RoadTest

Terms and Conditions

These are the terms and conditions which govern the Microduino Quadcopter KitRoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on July 20 2020

Announcement of Winner (estimated): July 21 2020

Prize:  Microduino Quadcopter Kit
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
  • One of my thoughts for the RoadTest was how to measure lift?

     

    A number of suggestions were posted on tasks the quad-copter could perform. I kept thinking about lift. Any payload added to the vehicle increase the lift requirement or more thrust from each propeller.

     

    My understanding (limited) in the realm, is that thrust determined by a number of factors. My initial thought was just speed of the motors but that is only one of a few that can impact thrust. I discovered the thrust must be balanced across all four motors if the platform is to hover in a fixed point. The electronics engaged to accomplish this feat is fascinating!

     

    So do you have any plans to measure thrust?

    image

    I'm curious about the results of such an experiment. The copter and known weight are placed on a scale. The copter is engaged to lift the load. The scale results will change as the copter engages. If the weight is sufficient so that the copter can't fully carry it, can you calculate the maximum carrying capacity? I made the  physical size of the weight size extend past the area of the four propellers. Maybe the load should be small enough to be inside the center of the vehicle? I seem to recall a fan on a sailboat blowing wind on the sails doesn't cause the boat to move.

     

    You have a excellent experiemental platform in the quad-copter when you get it operational. Or maybe not?

  • Hi Sean - Maximum lift (force)- thrust is first on everyone's wish list to measure.:-)

     

    If you've ever done vector diagram ( also know as Free Body Diagrams)  if you know maximum thrust, you can figure out maximum payload lifting -- but of course if all the lift is used for weight, the copter never lifts.

    Lift is a function of motor speed, blade pitch, blade length and also restricted by the available motor torque. Motor torque is also variable based on the battery voltage - so there needs to be margin for a low battery.

     

    What lift is not used to actually lift the copters weight is available to use for upwards acceleration, and also the copter moves forward by tilting, so acceleration is done in x axis and also y axis , and then even some in Z dimension for turning.

     

    At the end , weight, motor speed & available torque, and propeller type are a compromise with flight time and aerial responsiveness.


    The easiest way to measure lift is to place the quadcopter upside down on a scale. At rest, the scale measures weight, at full speed  the scale measures weight + thrust.

    If that does work because of gyroscopes, then can mount the propellers upside down, and reverse the motor direction, to make the same measurement.

     

    I may just write simple code to brute force make the measurements rather than hack the open source code ( depending if microduino will share the shield schematics) .

    The copter code seems written by someone really good with embedded systems software , it is fairly complex, and has some comments. The joypad code is shorter ( not simpler)  with no helpful annotation. 

    It may take alot more time than Road Test allows to understand it well enough to make significant changes.

     

    Keep up the good discussions.

  • Had seen a nice Youtube video recently on how to measure thrust with ducting propellers.

    1943, The Luftwaffe Fa 223 Dragon had just 2 propellers and later model was designed with 4 which is similar to most of the quadcopters available nowadays.image