MAX31889EVSYS# Temperature Sensor Eval Board

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The MAX31889 evaluation system (EV system) provides a single platform to evaluate the MAX31889, a temperature sensor with ±0.3°C accuracy. The EV system consists of two boards connected through headers, a MAX32630FTHR microcontroller board, and the MAX31889 EV kit board. The MAX32630FTHR contains the firmware necessary to use the PC GUI program and also provides power to the MAX31889 EV kit board. The MAX31889 EV kit board ships with jumpers preinstalled to allow quick evaluation of the MAX31889.

 

The MAX31889 operates from a 1.7V to 3.6V supply voltage, and is a low-power, high-accuracy digital temperature sensor with ±0.25ºC accuracy from -20ºC to +105ºC and ± 0.65ºC accuracy from -40ºC to +125ºC. The MAX31889 has 16-bit resolution (0.005ºC). The device uses a standard I2C serial interface to communicate with a host controller. Two GPIO pins are available. GPIO1 can be configured to trigger a temperature converison, while GPIO0 can be configured to generate an interrupt for selectable status bits. The MAX31889 includes a 32-word FIFO for the temperature data and also includes high and low threshold digital temperature alarms. The device is available in a 2mm x 2mm x 0.8mm, 6-pin, μDFN package.

image

image

Applications/Uses

  • Internet of Things (IoT) Sensors
  • Precision Temperature Monitoring
  • RTD Replacement

 

Additional Information

Important Dates

Enrollment Begin:July 23 2020

Enrollment Ends: August 17 2020

RoadTesters Selected: August 27 2020

Product Shipped: August 28 2020

RoadTesting Begins: Sept 4 2020

Reminder/Update Email: Oct 4 2020

Submit Reviews By: Nov 4 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest: Terms and Conditions

MAX31889EVSYS# Temperature Sensor Eval Board

 

These are the terms and conditions which govern the MAX31889EVSYS# Temperature Sensor Eval Board KIT contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Aug 17 2020

Announcement of Winner (estimated): Aug 18 2020

Prize: MAX31889EVSYS# Temperature Sensor Eval Board
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
  • I'm working on this from a Windows7 laptop, installed drivers, 2 failed, mbed serial and something else.

     

    The application isn't picking anything up.

     

    Could someone please offer some help?

     

    Thanks!

  • You're going to have to provide more information - for example,

    • which microcontroller board are you trying to use with the evaluation kit,
    • what development environment are you setting up to use with the board,
    • what application are you referring to about not picking anything up,
    • what have you tried to resolve the issue (e.g. changed cables, tried different port, tried different computer)?

     

    - Gough

  • Gough,

     

    In my opinion, that might be a tad outdated. Firstly, you can now get small batches of PCB's made with stencil for a fraction of the cost and reflow ovens are much cheaper these days too,  so the bottom line has dropped to make a dev kit. Even PCB design tools are now free (e.g. KiCad) so no more expensive license to be paid for. Then secondly, with the necessity for early field testing of any proof of concept this requires many more dev kits (and sensor shields) to purchased. Hence this increases the top line as demand for dev kits has now exploded with the rise of IoT. Gone are the days where you sit in a lab to test one design and then analyse the heck out of it before going out and procuring a couple of expensive customer boards to test prior to planning for manufacture.

     

    As such, there should be no technical or direct cost reason for dev boards to cost more the $50 a piece, unless uber complicated.

     

    I think, based on my experience, what really eats into the profit margin of a dev kit is corporate overhead, management dithering and changing of minds along the way (usually once designs have been sent for production).

     

    Sometimes the tail (i.e. the dev kit) ends up wagging the dog (i.e. the module itself) for a product launch. This is where the money goes down the proverbial plug hole as external contractors are usually hired in to do the multimedia and marketing stuff only because management are not aware that most of their own young engineers/staff are digi savvy, having been brought up on YouTube etc. and therefore could readily do the same videos in-house for a fraction of the cost (for silos will always remain). Then last but not least there is the documentation workflow, which can often require multiple parties to review and sanction... but this is often cut short to meet deadlines and budgets.

     

    Colin

  • I think that this 60 dollar kit comes with the Microcontroller. The MCU itself is 30 dollars so 30 dollar EV kit isn't as bad as a 60 dollar one.

     

    And, it comes with the EV kit preinstalled.

     

    Sweet.

  • UPDATE: The software simply doesn't work. It doesn't. The board does, transmitting the temperature in hexadecimal format using the COM communication(Putty and Tera), but the software simply can't pick it up.

     

    Maxim support is currently still reviewing my case and I hope I don't have to give a one for software.

  • Sorry your post is a little confusing.

     

    So what software does not work? What's on the board that allows temperature to be read? Is this a correct value or a dummy hex value, for example? You say you can receive hex format via Putty/Tera but software cannot pick it up??

     

    If you post online the code using the

     

    Syntax highlighter option

     

    We can try and help you troubleshoot.

  • As part of the roadtest I'm supposed to use the Maxim Integrated GUI software for the MAX31889 Evaluation kit.

     

    The MAX31889EVSYS has a MAX31889 temperature sensor chip on top.

     

    The hex value is separated into two parts, mostly something like 0x16 0x4B, eg. I converted these back to decimal base10 and it's 22 degrees and whatever 4B is. Makes sense, that's the temperature in my house usually, dropped around 10 degrees putting it in a box with a cold soda bottle.

     

    The values come about once per second, each staying relatively the same.

     

    The drivers simulated UART and thus I was able to establish a COM link to COM4(location of the board).

     

    I copied the .bin file that makes the board and EV kit send the data... this shows that the board is indeed detected by the computer, and is actively transmitting with the computer, Device manager shows it's there as well, but the software maxim provided is not able to find it, showing "not connected" despite the board being there and me pressing the scan button and relaunching application multiple times.

  • @BigG - Hugo is referring to the MAX3119 EV Kit GUI program, as this RoadTest is an EVSYS bundle of the MAX32630FTHR and the MAX31889 "wing" that connects to it. The board was supposed to ship pre-programmed with a program that allows for the GUI to speak to I2C devices attached to the MAX32630FTHR and tweak register values, set logging, etc. That program appears to have been wiped during set-up, but I think Hugo managed to reload the program based on my suggestions.

     

    - Sorry, I don't think I can help too much since I don't have the equipment - I'm going my best based on what I can see online and based on my previous experiences with other products. Have you tried launching the software first and then connecting the EV board? Does the text in the bottom right corner say Disconnected or Connected? (If it says connected but no devices show, are you sure the "wing" is properly attached?) Do you perhaps have a lot of COM ports on your computer - perhaps you might want to change the COM port number for the MAX32630FTHR to a lower port in case that helps the software pick it up? Have you tried running the software with Administrative privileges? Have you tried another computer?

     

    Failing all of that, it's probably best to ask your fellow RoadTesters directly (, , ) if they have encountered any issues or have any tips for you.

     

    - Gough

     

    EDIT: Sorry, I wrote my reply just as you wrote yours.

  • I'll try again later with an admin account. There's only 1 COM port active which is COM4(it says it in Device Manager)

     

    I've done everything mbed said to do including to re-do the image for the programmer. I did manage to restore the board to its original state, the board is inserted properly.

     

    I think I remember someone saying that the Windows7 system had driver issues with Maxim Boards... if this is true then it's on me for not taking that into account.

     

    On the plus side, I've filed a case with Maxim Support. Further, I'll probably do a more complex project to make up for the loss of the GUI testing part.

     

    Perhaps if I can figure out how this board interfaces with the EV kit I might use Arduino IDE or mbed to make it data log... I think I might have bitten off more than I can chew, perhaps.

  • The board is being quite tempermental.

     

    It was working 5 hours ago and now I'm stuck with a blank screen, again.

  • Or... not... Figured out you can activate it by pressing switch two.

     

    , @BigG, I've remembered, after windows 10 build 1809, or something, device ID and vendor are no longer required for operation. The build came out in 2018, and this EV software came out in 2019. Will probably look into the source code to find/edit if possible.

  • The Evaluation System document only says the following about the switches:

    If an SD card is present in the MAX32630FTHR, pressing SW2 on the MAX32630FTHR initiates measurements and saves log files to the SD card. Logging is stopped by pressing SW2 a second time.

     

    - Gough

Comment
  • The Evaluation System document only says the following about the switches:

    If an SD card is present in the MAX32630FTHR, pressing SW2 on the MAX32630FTHR initiates measurements and saves log files to the SD card. Logging is stopped by pressing SW2 a second time.

     

    - Gough

Children