MAX31889EVSYS# Temperature Sensor Eval Board

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The MAX31889 evaluation system (EV system) provides a single platform to evaluate the MAX31889, a temperature sensor with ±0.3°C accuracy. The EV system consists of two boards connected through headers, a MAX32630FTHR microcontroller board, and the MAX31889 EV kit board. The MAX32630FTHR contains the firmware necessary to use the PC GUI program and also provides power to the MAX31889 EV kit board. The MAX31889 EV kit board ships with jumpers preinstalled to allow quick evaluation of the MAX31889.

 

The MAX31889 operates from a 1.7V to 3.6V supply voltage, and is a low-power, high-accuracy digital temperature sensor with ±0.25ºC accuracy from -20ºC to +105ºC and ± 0.65ºC accuracy from -40ºC to +125ºC. The MAX31889 has 16-bit resolution (0.005ºC). The device uses a standard I2C serial interface to communicate with a host controller. Two GPIO pins are available. GPIO1 can be configured to trigger a temperature converison, while GPIO0 can be configured to generate an interrupt for selectable status bits. The MAX31889 includes a 32-word FIFO for the temperature data and also includes high and low threshold digital temperature alarms. The device is available in a 2mm x 2mm x 0.8mm, 6-pin, μDFN package.

image

image

Applications/Uses

  • Internet of Things (IoT) Sensors
  • Precision Temperature Monitoring
  • RTD Replacement

 

Additional Information

Important Dates

Enrollment Begin:July 23 2020

Enrollment Ends: August 17 2020

RoadTesters Selected: August 27 2020

Product Shipped: August 28 2020

RoadTesting Begins: Sept 4 2020

Reminder/Update Email: Oct 4 2020

Submit Reviews By: Nov 4 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

RoadTest: Terms and Conditions

MAX31889EVSYS# Temperature Sensor Eval Board

 

These are the terms and conditions which govern the MAX31889EVSYS# Temperature Sensor Eval Board KIT contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Aug 17 2020

Announcement of Winner (estimated): Aug 18 2020

Prize: MAX31889EVSYS# Temperature Sensor Eval Board

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comment List
Anonymous
Parents
  • I'm working on this from a Windows7 laptop, installed drivers, 2 failed, mbed serial and something else.

     

    The application isn't picking anything up.

     

    Could someone please offer some help?

     

    Thanks!

  • You're going to have to provide more information - for example,

    • which microcontroller board are you trying to use with the evaluation kit,
    • what development environment are you setting up to use with the board,
    • what application are you referring to about not picking anything up,
    • what have you tried to resolve the issue (e.g. changed cables, tried different port, tried different computer)?

     

    - Gough

  • Since I was quite stupid I didn't do everything on the mbed page. I'm currently in the process of installing some lovely drivers. Which, has been successfully done.

     

    Followed and finished the instructions on the mbed site successfully.

     

    Sorry for the not so clear question.

     

    - MAX32630FTHR

    - I'm currently still trying to get it to work with the software provided for the Evaluation kit of the MAX31889.

    - ^^^

    - the cables I know are working since I've tested them, Data and Power are both good, different ports, tried, different computer, the one I'm using is my only windows laptop.

     

    Here are all the specs of my laptop in case you need them...

    Core2 duo @ 1.6GHz

    Windows 7 Enterprise 32 bits

    4GB RAM

    3x USB 2.0

    Thinkpad x61s

     

    I've followed all the instructions and it should work, the device is currently sitting at COM4.

     

    There are no other COM ports.

     

    However, the Evaluation kit software, found here, https://www.maximintegrated.com/en/design/software-description.html/swpart=SFW0013950A , does not seem to be able to find the board.

     

    Currently investigating about the laptop's port outputs.

     

    There is virtually no documentation on the software.

     

    If you need me to clarify on anything else or if you have any advice I'll read it in a few hours since it's nearly midnight for me.

  • Someone sent me a MAX32630FTHR board the other day and I've been learning what works and what doesn't. The best way I can describe this board is that it reminds me of that well known "spaghetti western" film, titled "The Good, the bad and the ugly". At face value it's a dev board in the Adafruit Feather form factor with a Cortex M4 processor and some nice sensors and peripherals included. Dig deeper and you'll find the software libraries limited and the documentation woeful.

     

    Anyway, if you have problems with the board, let me know and will try and help. Note, I found the Bluetooth module to me particularly problematic (takes over 5 minutes before it starts advertising when running the Mbed example) and the SD card reader is temperamental. Other than that it's a pretty good board. Did you know you can develop code with the Arduino IDE too.

  • I think it is pretty good and the Arduino IDE compatibility better. I managed to make it blink the LED red over and over.

     

    The application is still not being nice, so I'm hoping another one of the other 3 roadtesters are smarter than me and managed to work around this or just solve it.

     

    I guess I'll reach out to Maxim Support in the meantime.

     

    Once I get to the board testing part I'll have a 99% chance of asking you for help.

     

    Thanks!

  • I'm not sure but my previous experience with other Maxim EVSYS products seem to suggest that the boards may come pre-programmed with the code necessary to make them function with the demo app. If you've tried reprogramming the microcontroller, you might have replaced the original program with your own, which may explain why the demo app isn't picking it up. Whether Maxim provides the code for the microcontroller to restore the original program, I'm not sure, but that's my best guess. Maybe someone else with this exact kit can comment.

     

    - Gough

  • Well... I guess that was stupid thinking on my part.

     

    I guess I'll not do everything on the mbed page in the future, I guess.

     

    I opened a case with Maxim Support, hopefully I can convince them to send me a copy of the demo code.

     

    Also, I'm curious. This EV kit is just a PCB, a 2 dollar chip, a cap, and some jumpers, test probes, and headers. And terminal blocks. I don't understand why this is at the 56 dollar price mark. Seems overly expensive for a simple breakout board and software.

  • Or I'll call them in the afternoon if they aren't busy.

     

    lesson learned for road testing: if they don't come with 600 page user manuals like that Eaton thing don't' apply unless if you're willing to run in circles and call support 10 times.

  • It's common for many evaluation boards to hit the $100-150 mark even, although the parts on the board may cost only a few dollars. I'm looking at one right now on a RoadTest.

     

    This is mainly because the products themselves are not mass market - they are often done as small batches (or even hand built in some cases) which increases cost. The product often comes with extra documentation, design recommendations, actual design gerbers, bill of materials for you to "short-cut" the design processes by basing your design off their (usually optimised) reference design. Other times, they provide source code as well which can be a reference point for developing your own.

     

    Overall, the value of the kits is not the sum of the parts, but in the time saved for an engineer who is deciding whether to integrate the part or not into their design and the reduction in effort required to do. Sometimes these kits are subsidised by the manufacturer to encourage adoption of their parts, but this seems to be rather rare nowadays as is getting free samples of chips as well.

     

    - Gough

  • Actually getting samples of chips are pretty easy, I've managed to get some I needed from Maxim, Analog, and Microchip.

     

    I guess it's true EV kits are produced in low quantities, but this EV kit only has one doc: the data sheet.

     

    I'm probably going to comb through that as well.

     

    And the data sheet is for the chip.

     

    You were correct.

     

    The MAX32630FTHR contains the firmware necessary to use the PC GUI program and also provides power to the MAX31889 EV kit board. The MAX31889 EV kit board ships with jumpers preinstalled to allow quick evaluation of the MAX31889.

     

    *sighs*

     

    I'll try to find this firmware I guess.

  • I suppose product support, quality of materials/documentation is a part of the RoadTest too. But having to discover things on your own and reaching out to support in case of issues is a very normal thing regardless of the "thickness of the manual". One of my RoadTest items has cost me several hundred dollars in return postage as it is undergoing repairs to fix an issue which was discovered during the RoadTest - so keep in mind that sometimes things don't go to plan and that's only natural.

     

    In fact - I'm looking at the page for the MAX31889EVSYS right now - right on the front page it says the following:

    The MAX32630FTHR contains the firmware necessary to use the PC GUI program and also provides power to the MAX31889 EV kit board.

    There are gerbers available, as well as the application itself. The datasheet linked in the RoadTest is for the chip and not the Evaluation Kit, the actual datasheet for the evaluation board is here: https://datasheets.maximintegrated.com/en/ds/MAX31889EVSYS.pdf

     

    Looking at the download of the MAX31889 Evaluation Kit Tool zip file, it seems that the file FTHR_Interrupt.MAX32630FTHR.bin is a firmware file for reprogramming the microcontroller and is included. As for what tool you might use to download this to the board, I'm not sure - if it's Mbed, then it might appear in your computer as a removable disk drive. Copying the BIN file into the removable disk drive and then safely removing it should cause it to be programmed onto the board (based on my experience with a Freescale Freedom board I previously tried).

     

    - Gough

     

    EDIT: Almost midnight here in Sydney, so I might have to leave it there. Hopefully you manage to get the firmware file programmed up and back on track. Good luck!

Comment
  • I suppose product support, quality of materials/documentation is a part of the RoadTest too. But having to discover things on your own and reaching out to support in case of issues is a very normal thing regardless of the "thickness of the manual". One of my RoadTest items has cost me several hundred dollars in return postage as it is undergoing repairs to fix an issue which was discovered during the RoadTest - so keep in mind that sometimes things don't go to plan and that's only natural.

     

    In fact - I'm looking at the page for the MAX31889EVSYS right now - right on the front page it says the following:

    The MAX32630FTHR contains the firmware necessary to use the PC GUI program and also provides power to the MAX31889 EV kit board.

    There are gerbers available, as well as the application itself. The datasheet linked in the RoadTest is for the chip and not the Evaluation Kit, the actual datasheet for the evaluation board is here: https://datasheets.maximintegrated.com/en/ds/MAX31889EVSYS.pdf

     

    Looking at the download of the MAX31889 Evaluation Kit Tool zip file, it seems that the file FTHR_Interrupt.MAX32630FTHR.bin is a firmware file for reprogramming the microcontroller and is included. As for what tool you might use to download this to the board, I'm not sure - if it's Mbed, then it might appear in your computer as a removable disk drive. Copying the BIN file into the removable disk drive and then safely removing it should cause it to be programmed onto the board (based on my experience with a Freescale Freedom board I previously tried).

     

    - Gough

     

    EDIT: Almost midnight here in Sydney, so I might have to leave it there. Hopefully you manage to get the firmware file programmed up and back on track. Good luck!

Children