Panasonic PAN 1780 Bluetooth LE Eval Kit

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The Panasonic PAN 1780 Bluetooth LE Evaulation kit is used as a quick prototyping platform and for software testing of the PAN 170 Bluetooth module, a Bluetooth 5 Low Energy (LE) module based on the Nordic nRF52840 single-chip controller.

 

The PAN1780 Evaluation Kit is an all-inclusive and comprehensive Evaluation Kit consisting of two USB dongles and two external NFC antennas.  Each dongle allows design engineers to develop, run and debug code with the PAN1780 Series Module.  The break-out headers provide an easy way to connect Sensors, as well as other devices for rapid prototyping. The USB Evaluation Boards are delivered without any preinstalled software examples, but an integration guide is available explaining how to use the recommended development environment and the free Nordic Semiconductors Software Development Kit, to run different kinds of Bluetooth, thread, ZigBee, 802.15.4 and Antennae software examples.

 

Features

  • Surface Mount Type Dimensions: 15.6 mm x 8.7 mm x 2 mm
  • Same Form Factor as PAN1026A and PAN1762 But Smaller Pitch And More Pins
  • Nordic nRF52840 Featuring ARM® Cortex®-M4F With 64 MHz
  • Bluetooth 5.0 Low Energy Including LE 2M And LE Coded PHY
  • Embedded 1 MB Flash Memory And 256 kB Internal RAM
  • Includes ARM® TrustZone® CryptoCell® 310 And Supports Secure Boot Including Root-of-Trust (RoT)
  • Up to 48 general purpose I/Os (GPIO), which are shared by up to 4 SPI, 2 I²C, 2 UART, 4 PWM, 8 ADC, 1 NFC-A, 32 kHz IN/OUT, nRESET
  • USB 2.0 Full-Speed Device Interface
  • Built-in Temperature Sensor

 

About the PAN1780 Bluetooth Module

The Bluetooth 5 features additionally a higher symbol rate of 2 Mbps using the high-speed LE 2M PHY or a significantly longer range using the LE coded PHY at 500 kb/s or 125 kb/s. The new channel selection algorithm (CSA#2) improves the performance in high interference environments. Furthermore, the new LE advertising extensions allow for much larger amounts of data to be broadcasted in connectionless scenarios. An output power of up to 8 dBm and the high sensitivity of the nRF52840 in combination with the LE coded PHY make the module very attractive in applications, where a long range is required. In addition the ultra-low current consumption of the PAN1780 make the module an ideal choice for battery powered devices. With the Cortex® M4F processor, 256 kB RAM and the build-in 1 MB flash memory the PAN1780 can easily be used in standalone mode, thereby eliminating the need for an external processor, saving complexity, space, and cost. The rich set of security features from the ARM TrustZone CryptoCell 310 security subsystem provide the necessary means for secure device operation in the IoT space. The PAN1780 also supports Type 2 Near Field Communication (NFC-A) for use in simplified pairing and payment solutions (external antenna required).

image

Contents

  • Two (2) PAN1780 USB-Evaluation Boards
  • Case

 

Additional Information

Important Dates

Enrollment Begin:July 27 2020

Enrollment Ends: Sept 1 2020

RoadTesters Selected: Sept 4 2020 (estimated)

Product Shipped: Sept 18 2020

RoadTesting Begins:Sept 25 2020

Reminder/Update Email: Oct 25 2020

Submit Reviews By: Nov 25 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

Roadtesters

Terms and Conditions

RoadTest: Terms and Conditions

Panasonic PAN 1780 Bluetooth LE Eval Kit

 

These are the terms and conditions which govern the Panasonic PAN 1780 Bluetooth LE Eval Kit contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 1 2020

Announcement of Winner (estimated): Sept 4 2020

Prize: Panasonic PAN 1780 Bluetooth LE Eval Kit
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
  • Hello!

     

    I'm currently going through the documentation as part of the road test, and I seem to have hit some confusing areas.

     

    I know that the nRF52840 has two modes of power input: normal voltage mode, and high voltage mode. See https://infocenter.nordicsemi.com/index.jsp?topic=%2Fps_nrf52840%2Fref_circuitry.html&cp=4_0_0_6_2

     

    By following the schematics and the comparing it to the current jumper configuration, I can see that the eval kit is set up for normal voltage mode (VCC and VDDH are shorted together, and VCC is getting power from the 3v LDO).

     

    I'm interested in setting up high voltage mode via the jumpers. I've tried this out myself on a bare module and it involves routing power to just the VDDH pin while leaving VCC hanging.

     

    However, I'm not sure exactly how to do this on the eval kit as the docs don't mention this directly. On JP12 it mentions

     

    Option to break 3.3 V supply

    via JP9 and connect 5 V

    supply to pin 1 of JP12 to

    power the module.

     

    But shouldn't I also break JP9 since that would still be sourcing 3v and would then likely kill the chip (since it's likely the UICR is cleared and so would be setup to use 1.8v for the built-in LDO).

     

    I wonder if I can ask someone from Panasonic Industry to help clear this for me? I'm making a note of this for now, and I will be trying it out towards the end of the road test (I don't really want to do it in the middle of my tests as I'd like to use the two boards for testing and comparing ranges).

     

    This is the doc I'm referring to btw: https://mediap.industry.panasonic.eu/assets/custom-upload/Devices/Wireless%20Connectivity/Bluetooth%20Low%20Energy%20Modules/PAN1780/WM%20PAN1780%20Module%20Integration%20Guide.pdf

  • Well, after re-reading that portion multiple times I think I should indeed break JP9 *as well as* break JP12 to provide power directly to the VDDH of the chip. Of course the question now becomes: which one is pin 1 image

    The schematic has it labeled clearly, but the silkscreen doesn't mention which is pin 1, and one of the things I noted in my road test was that the order of the pins in the schematic doesn't necessarily correspond to the order they are in the schematic. And of course depending on which way you orient the board left might be on the right (or on the top).

  • I seem to be answering more questions by myself lately image

     

    The proper way of reading the pin layout on the board so it matches the schematic is ... upside down. Well, the silk screen at the bottom is upside down compared to the one in the top, so if you read the bottom silk screen right way up, then flip the board, the pin layout matches the schematic layout and pin1 is at the uppermost pin.

Comment
  • I seem to be answering more questions by myself lately image

     

    The proper way of reading the pin layout on the board so it matches the schematic is ... upside down. Well, the silk screen at the bottom is upside down compared to the one in the top, so if you read the bottom silk screen right way up, then flip the board, the pin layout matches the schematic layout and pin1 is at the uppermost pin.

Children
No Data