Panasonic PAN 1780 Bluetooth LE Eval Kit

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content
About

The Panasonic PAN 1780 Bluetooth LE Evaulation kit is used as a quick prototyping platform and for software testing of the PAN 170 Bluetooth module, a Bluetooth 5 Low Energy (LE) module based on the Nordic nRF52840 single-chip controller.

 

The PAN1780 Evaluation Kit is an all-inclusive and comprehensive Evaluation Kit consisting of two USB dongles and two external NFC antennas.  Each dongle allows design engineers to develop, run and debug code with the PAN1780 Series Module.  The break-out headers provide an easy way to connect Sensors, as well as other devices for rapid prototyping. The USB Evaluation Boards are delivered without any preinstalled software examples, but an integration guide is available explaining how to use the recommended development environment and the free Nordic Semiconductors Software Development Kit, to run different kinds of Bluetooth, thread, ZigBee, 802.15.4 and Antennae software examples.

 

Features

  • Surface Mount Type Dimensions: 15.6 mm x 8.7 mm x 2 mm
  • Same Form Factor as PAN1026A and PAN1762 But Smaller Pitch And More Pins
  • Nordic nRF52840 Featuring ARM® Cortex®-M4F With 64 MHz
  • Bluetooth 5.0 Low Energy Including LE 2M And LE Coded PHY
  • Embedded 1 MB Flash Memory And 256 kB Internal RAM
  • Includes ARM® TrustZone® CryptoCell® 310 And Supports Secure Boot Including Root-of-Trust (RoT)
  • Up to 48 general purpose I/Os (GPIO), which are shared by up to 4 SPI, 2 I²C, 2 UART, 4 PWM, 8 ADC, 1 NFC-A, 32 kHz IN/OUT, nRESET
  • USB 2.0 Full-Speed Device Interface
  • Built-in Temperature Sensor

 

About the PAN1780 Bluetooth Module

The Bluetooth 5 features additionally a higher symbol rate of 2 Mbps using the high-speed LE 2M PHY or a significantly longer range using the LE coded PHY at 500 kb/s or 125 kb/s. The new channel selection algorithm (CSA#2) improves the performance in high interference environments. Furthermore, the new LE advertising extensions allow for much larger amounts of data to be broadcasted in connectionless scenarios. An output power of up to 8 dBm and the high sensitivity of the nRF52840 in combination with the LE coded PHY make the module very attractive in applications, where a long range is required. In addition the ultra-low current consumption of the PAN1780 make the module an ideal choice for battery powered devices. With the Cortex® M4F processor, 256 kB RAM and the build-in 1 MB flash memory the PAN1780 can easily be used in standalone mode, thereby eliminating the need for an external processor, saving complexity, space, and cost. The rich set of security features from the ARM TrustZone CryptoCell 310 security subsystem provide the necessary means for secure device operation in the IoT space. The PAN1780 also supports Type 2 Near Field Communication (NFC-A) for use in simplified pairing and payment solutions (external antenna required).

image

Contents

  • Two (2) PAN1780 USB-Evaluation Boards
  • Case

 

Additional Information

Important Dates

Enrollment Begin:July 27 2020

Enrollment Ends: Sept 1 2020

RoadTesters Selected: Sept 4 2020 (estimated)

Product Shipped: Sept 18 2020

RoadTesting Begins:Sept 25 2020

Reminder/Update Email: Oct 25 2020

Submit Reviews By: Nov 25 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

Roadtesters

Terms and Conditions

RoadTest: Terms and Conditions

Panasonic PAN 1780 Bluetooth LE Eval Kit

 

These are the terms and conditions which govern the Panasonic PAN 1780 Bluetooth LE Eval Kit contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 1 2020

Announcement of Winner (estimated): Sept 4 2020

Prize: Panasonic PAN 1780 Bluetooth LE Eval Kit

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comment List
Anonymous
Parents
  • Hello!

     

    I'm currently going through the documentation as part of the road test, and I seem to have hit some confusing areas.

     

    I know that the nRF52840 has two modes of power input: normal voltage mode, and high voltage mode. See https://infocenter.nordicsemi.com/index.jsp?topic=%2Fps_nrf52840%2Fref_circuitry.html&cp=4_0_0_6_2

     

    By following the schematics and the comparing it to the current jumper configuration, I can see that the eval kit is set up for normal voltage mode (VCC and VDDH are shorted together, and VCC is getting power from the 3v LDO).

     

    I'm interested in setting up high voltage mode via the jumpers. I've tried this out myself on a bare module and it involves routing power to just the VDDH pin while leaving VCC hanging.

     

    However, I'm not sure exactly how to do this on the eval kit as the docs don't mention this directly. On JP12 it mentions

     

    Option to break 3.3 V supply

    via JP9 and connect 5 V

    supply to pin 1 of JP12 to

    power the module.

     

    But shouldn't I also break JP9 since that would still be sourcing 3v and would then likely kill the chip (since it's likely the UICR is cleared and so would be setup to use 1.8v for the built-in LDO).

     

    I wonder if I can ask someone from Panasonic Industry to help clear this for me? I'm making a note of this for now, and I will be trying it out towards the end of the road test (I don't really want to do it in the middle of my tests as I'd like to use the two boards for testing and comparing ranges).

     

    This is the doc I'm referring to btw: https://mediap.industry.panasonic.eu/assets/custom-upload/Devices/Wireless%20Connectivity/Bluetooth%20Low%20Energy%20Modules/PAN1780/WM%20PAN1780%20Module%20Integration%20Guide.pdf

  • Well, after re-reading that portion multiple times I think I should indeed break JP9 *as well as* break JP12 to provide power directly to the VDDH of the chip. Of course the question now becomes: which one is pin 1 image

    The schematic has it labeled clearly, but the silkscreen doesn't mention which is pin 1, and one of the things I noted in my road test was that the order of the pins in the schematic doesn't necessarily correspond to the order they are in the schematic. And of course depending on which way you orient the board left might be on the right (or on the top).

Comment
  • Well, after re-reading that portion multiple times I think I should indeed break JP9 *as well as* break JP12 to provide power directly to the VDDH of the chip. Of course the question now becomes: which one is pin 1 image

    The schematic has it labeled clearly, but the silkscreen doesn't mention which is pin 1, and one of the things I noted in my road test was that the order of the pins in the schematic doesn't necessarily correspond to the order they are in the schematic. And of course depending on which way you orient the board left might be on the right (or on the top).

Children
  • I seem to be answering more questions by myself lately image

     

    The proper way of reading the pin layout on the board so it matches the schematic is ... upside down. Well, the silk screen at the bottom is upside down compared to the one in the top, so if you read the bottom silk screen right way up, then flip the board, the pin layout matches the schematic layout and pin1 is at the uppermost pin.

  • Hi ,

    you seem to have figured this out, but for what its worth here's my take.

     

    in order to provide power to the VDDH aka input to the on-chip LDO, you should remove the JP9 and JP12 jumpers entirely, and connect your VDDH input (2.5V to 5.5V) to pin 1 of J12

    pin 1 of J12 according to the layout diagram on page 15 is the one nearest to the j-link & LEDs, furthest from the antenna keep out and uf.l connector. first hint is from the routing to C44, but you can also see that it routes to pin G2.

     

    be careful that you check all the pins IO voltages - it looks like the FT232 will put 3v3 on some of them at least - I haven't looked to see if the module is tolerant when running lower VCCIO but you could remove the jumpers.

  • Thanks! I'll keep this as a reference for later when I try out high voltage mode image I was worried about stray 3v3 power from the other peripherals going into the io but like you mentioned, I can just remove those jumpers (at least until I've reprogrammed the UICR)