AVNET Monarch LTE-M Development Kit -- EU

Table of contents

image

Sign Up Now: Monarch Go Workshop: Part 1: Deep Dive into the Monarch LTE-M Development Kit Advantage to learn more about this hardware and how to get started with it.

 

This Roadtest is for an EU-based Roadtester.

 

{tabbedtable} Tab LabelTab Content
About

ABOUT THIS ROADTEST (May 2021): We are seeking a roadtester to test the kit and documentation that would be used by a European customer to use their local carriers network and run the out of box example. We would like a road tester to go through and document this process.

 

 

ABOUT THIS KIT (DEC 2020):The Monarch LTE-M Development Kit is a cellular IoT enablement platform featuring the NXP LPC55S69-EVK and the Monarch Go Arduino Shield. This kit is an ideal entry point for starting your next LTE IoT application development. The LPC55S69 dual-core Arm Cortex-M33 microcontroller chipset with the production certified Monarch Go modem allows for easy transition from development to production.

image

BUY NOW

 

Out of box, the Monarch LTE-M Development Kit is enabled with Microsoft Azure and AWS cloud support. This includes an Azure IoT Central and Avnet IoTConnect cloud example. Having these examples available for user development out of box will save the user hundreds of hours in application development cost in addition to providing a time-to-market advantage.

 

In addition to providing Monarch Go LTE connectivity, the Monarch Go Arduino shield is fitted with a MikroElektronika shuttle click expansion connector for click module ecosystem enablement. The click module ecosystem enables over 700 3.3V I/O, I2C, SPI, UART and GPIO-based click modules. This click module ecosystem enables sensors, interfaces, displays, motor controls and more to allow for thousands of LTE IoT development applications.

 

In addition to the click module interface, the Monarch Go Arduino Shield also has an onboard VEML6030 ambient light sensor and a SE050 plug-andtrust secure element. The availability of these capabilities on board enables prototyping of both motion and secure LTE applications out of box.

 

The Monarch Go Cat-M1 modem delivers the shortest possible route to market and lowest development cost for cellular IoT-connected devices. Unlike traditional cellular modules, this modem is certified for use on the Verizon network, which avoids costly lab testing while improving time to market. The Monarch Go has an integrated antenna and pre-installed Verizon ThingSpace IoT SIM card, giving developers an easy, cost-effective approach to developing LTE IoT solutions.

 

Contents

  • Avnet Monarch Go Arduino Shield
  • Sequans Monarch Go LTE modem
  • Verizon ThingSpace IoT SIM card
  • NXP LPC55S69-EVK
  • Quick start card

 

Additional Information

Important Dates

Enrollment Begin: Dec 8 2020

Enrollment Ends: Feb 19 2021

RoadTesters Selected: tbd

Product Shipped: tbd

RoadTesting Begins: tbd

Reminder/Update Email: tbd

Submit Reviews By: tbd

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

 

How to locate the official RoadTest review form:  How To Locate the Official RoadTest Review Form (duplicate)

RoadTesters

(deadline April 20 2021)

(deadline April 20 2021)

  (deadline  May 12 2021)

(deadline (May 22 2021)

  (deadline Sept 7 2021)

Terms and Conditions

AVNET Monarch LTE-M Development Kit – RoadTest

Terms and Conditions

These are the terms and conditions which govern the AVNET Monarch LTE-M Development Kit RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on Mar 10 2021

Announcement of Winner (estimated): Mar 10 2021

Prize:  AVNET Monarch LTE-M Development Kit

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comment List
Anonymous
Parents
  • It's definitely interesting but seems to be a regionally restricted RoadTest. I'm seeing "This RoadTest is not available in your country" across the top with no Enroll button. Oh well. Look forward to the reviews nonetheless.

     

    - Gough

  • It happens. Sad you won't be able to apply- your experience for this could be greatly beneficial.

     

    It's a LTE development kit. From what I recall, different continents have different standards.

     

    North America uses a different band(typically) than Europe, and presumably Asia, Oceania(where I believe you live, Australia, right?)

    Different from Africa, and South America too.
    I think most likely, since the kit's RoadTest is available for my region, the kit is intended for North America LTE bands.

     

    image

     

    Yeah. It sucks.

  • Alternatively, just looked at the product brief.

     

    "Countries available for purchase: United States"

     

    Looks like this is only available to RoadTesters in the US.

     

    Ouch,

     

    Maybe because it's because of the SIM card? It claims to be a Verizon one- maybe they didn't want to incur extra costs with international cellular.

  • It seems we have bet on multiple horses in Australia - NB-IoT has a slight lead with two carriers running it, while LTE-M is run by one of the three carriers. But getting any SIMs for devices here is a nightmare - carriers only want to deal in bulk, so most of the time we have to deal with a reseller of sorts and there's a bit of paperwork involved. Definitely a plus for solutions that come with a SIM image - a lot less work for the prototyper.

     

    I suspect you're right - it seems the Monarch Go module itself (https://www.sequans.com/monarch-go/ ) is "certified" for Verizon and USA-centric. Verizon/ThingSpace doesn't operate in Australia and I'm not sure roaming agreements for LTE-M even exist yet ... whether the mobile network is ready to handle the "migration" of IoT devices overseas will be a rather interesting thing to see. While I see many NB-IoT modules have multiple bands, based on the datasheets on the Avnet site for the Monarch Go (https://www.avnet.com/wps/portal/us/products/new-product-introductions/npi/sequans-monarch-go ), it operates on LTE Band 13 so that wouldn't work outside of the USA.

     

    - Gough

  • Yeah. Seems like that.

     

    Thanks for the technical perspective.

Comment Children
No Data