Digilent 1x1 USB Software-Defined Radio Platform

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The USRP B205mini-i is a flexible and compact platform that is ideal for both hobbyist and OEM applications. It is designed by Ettus Research™ and provides a wide frequency range (70 MHz to 6 GHz) and a user-programmable, industrial-grade Xilinx Spartan-6 XC6SLX150 FPGA.

 

The RF front end uses the Analog Devices AD9364 RFIC transceiver with 56 MHz of instantaneous bandwidth. The board is bus-powered by a high-speed USB 3.0 connection for streaming data to the host computer. The USRP B205mini-i also includes connectors for GPIO, JTAG, and synchronization with a 10 MHz clock reference or PPS time reference input signal.

USRP B205mini-i: 1x1 USB Software-Defined Radio Platform

 

 

The hardware is conveniently accessible through the USRP Hardware Driver (UHD). UHD provides both a C/C++ and Python API that supports all USRP products and enables users to efficiently develop applications then seamlessly transition designs between platforms as requirements expand. UHD also offers cross-platform support for multiple industry standard development environments and frameworks, including RFNoC, LabVIEW, and Matlab/Simulink. To ensure you have no restrictions on how you use UHD, it is available on Linux, Windows, and Mac OS. Do you prefer graphical programming? Try out GNU Radio, a free and open-source software development framework offering a graphical design approach.

 

Features

  • USB powered (5V)
  • Operating temperature range from 0 to 45°C
  • USRP hardware driver 3.9.2 (or later), GNU radio
  • Dimensions is 83.3 x 50.8 x 8.4mm, weight is 24g
  • IIP3 (at typical NF) of -20dBm, power output is >10dBm, receive noise figure is <8dB
  • Connectors for GPIO, JTAG and synchronization with 10MHz clock or PPS time reference input signal
  • Hardware is conveniently accessible through the USRP Hardware Driver (UHD)

 

Contents

  • USRP B205mini-i (board only), USB 3.0 cable.

 

Additional Information

 

Discussion

Poll: Are You Interested in Roadtesting a USB Software-Defined Radio Platform?

Important Dates

Enrollment Begin: Feb 24 2021

Enrollment Ends: Mar 26 2021

RoadTesters Selected: Apr 14 2021 (estimated)

Product Shipped: Apr 21 2021

RoadTesting Begins: Apr 28 2021

Reminder/Update Email: May 28 2021

Submit Reviews By: Jun 28 2021

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

 

How to locate the official RoadTest review form:  How To Locate the Official RoadTest Review Form (duplicate)

RoadTesters

Terms and Conditions

USRP B205mini-i: 1x1 USB Software-Defined Radio Platform– RoadTest

Terms and Conditions

These are the terms and conditions which govern the USRP B205mini-i: 1x1 USB Software-Defined Radio PlatformRoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on Mar 26 2021

Announcement of Winner (estimated): Mar 30 2021

Prize: USRP B205mini-i: 1x1 USB Software-Defined Radio Platform
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
  • You don't really need to get into FPGA programming to use the board.You could just use it through the SDR drivers. Unless you need something that's impossible to implement through the driver interface.

  • This looks interesting, however since they are using the older Xilinx Spartan-6 XC6SLX150 FPGA, it is not supported with the newer design tools from Xilinx like Vivado or Vitis.  You have to use Xilinx ISE which technically is not supported on Windows 10 outside of running in a virtual machine. There might be an issue with licensing for the XC6SLX150 device as well.

  • I'm interested in this as I've had a fascination with the idea of HAM radio all my life but given that I haven't ever moved past research / reading about it, I doubt I'm a good choice for the road test. Any idea what pricing is like on one of these?

  • Or make one    I was looking at some that use a handful of 3d printed parts and readily available pvc plumbing tubing

  • I think it is important to state if the board will be supplied with an antenna. Potential roadtesters should be aware that if no antenna is supplied they may need to buy one (if they don't have one already).

  • Ooh! This looks quote promising! I wish I had more time to mess around with it, though, or I'd totally sign up!

  • The b200 and b210 have been around for ~8 years, and the B205 appears to be a stripped down version of the B200. The issues here are my experience with Windows, so again it may be a completely different story on Linux. On windows the UHD drivers rely on LibUSB, and downstream it gets more complex and I cant remember the details much. I think LibUSB can use different USB drivers which can make a whole difference between them. You can select which driver to use through a 3d party tool called "zadig" (https://zadig.akeo.ie/ ). It allows you to select 3 USB drivers, but there was one that did not work for me.

     

    I've experienced many times issues like that for some reason the SDR can't all of a sudden can't handle certain sampling rate speed  anymore, without having anything suspicious running in the background (taskbar shows all resources available). Also apparently some USB controllers cant handle high throughput.

     

    Anyway even 32 msps is a lot and actually allows you to do all kind of fun stuff, and the SDR can even transmit so you can do stuff as crazy creating a mobile phone network.

  • Maybe I've been blinkered from much of the issues with big software names...but on reflection you are right. I, like many others, have huge issues with a very common software package...namely Windows10: simple things you'd expect an OS to be able to accomplish like the volume up down not working or dual screen support just stopping ! Regarding big names in development support - I feel they are often produced at a price based on expected sales, once a board is redundant the support to fix bugs drops rapidly.

     

    I wasn't aware of all the online discussion re: 56Msps and therefore stand corrected, thank you. Maybe it is something Ettus can address as the board becomes more popular - or am I being naive again image. I know my version of GNU Radio and NeoSmart SDR don't work very well on Windows - however all works well under Debian - I think GNU Radio even suggest it should be on Linux platforms.

  • > I don't see why a big companies would release good software

     

    Sometimes it's a matter of feedback, which's why we do these roadtests for the supplier to get a good sample of engineer's opinions image So whoever's chosen for the roadtest need to make sure they put the software used if supplied by Digilent through as much of a test as the hardware image

  • I've used a lot of the Ettus products over the years and network is usually better then USB for throughput, though less convenient.  You're spot on with the ballpark though, regardless of OS or software you'll get 32MS/s fairly easily, 56MS/s needs some seriously good hardware, usually a top of the range Intel USB host chip, no hubs (lots of laptops/desktops have hubs in them these days) and a very well tuned operating system to support real-time data acquisition.  Generally Windows just doesn't let you tweak the kernel parameters with enough control to get the absolute best out of the USB.

     

    All that said 32MS/s is enough to do a lot of useful and interesting stuff! And if you're application is worth the effort you _can_ get more than 50MS/s out of these boards.