Infineon 3-Phase Motor Drive EVB with FOC

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

This roadtest will test drive a three-phase inverter power stage with half-bridge gate-driver IC based on CoolMOS™ PFD7, the latest Infineon’s SJ technology with fast body diode. It includes a debugger and a fan motor.

 

About the Evaluation Board

This is a complete evaluation board that includes IPN60R1K5PFD7S discrete Superjunction (SJ) MOSFET and 2ED28073J06F gate-driver ICs for motor drives application. Ready-to-use three-phase inverter power stage with 600V blocking voltage - up to 100W. In combination with iMOTION™ controller, the user can run a motor within one hour with a smooth start-up using inductive sensing.

 

The EVAL_DRIVE_3PH_PFD7 is designed to provide easy to use power stage based on Infineon's discrete CoolMOS™ Superjunction MOSFET. The board is equipped with all assembly groups for sensorless field oriented control (FOC). It provides a single-phase AC-connector, rectifier, and three-phase output for connecting the motor. The power stage also contains emitter shunts for current sensing and a voltage divider for DC-link voltage measurement.

gate drive evb

Features

  • Low BOM count due to the CoolMOS™ PFD7 and latest iMOTION™ algorithm
  • Smooth startup using inductive sensing
  • Best light-load efficiency solution
  • Sensorless field-oriented control (FOC)
  • Ease of use with graphical user interface (GUI)

 

Applications

  • Drives
  • Heating
  • Home appliances
  • Household
  • IoT
  • Motor control & drives
  • Power supply (SMPS)
  • Pumps

 

About Debug Probe

It is a functional Isolated Debug Probe, based on SEGGER J-Link Technology. XMC™ Link is an Isolated Debug Probe for all XMC™ Microcontrollers. The debug probe is based on SEGGER J-Link debug firmware, which enables use with DAVE™ and all common third-party compiler/IDEs (Altium Limited, Atollic, ARM/KEIL, IAR Systems, iSystem, Rowley Associates) known from the wide ARM® ecosystem.

debugger

Features

  • 1kV DC functional isolation
  • Debug protocols
  • JTAG
  • Serial Wire Debug (SWD)
  • Serial Wire Viewer/Output (SWV/SWO)
  • Infineon's Single Pin Debug (SPD)
  • Virtual COM Port (UART-to-USB Bridge)

 

About the Fan Motor

An ebm-pabst 3-phase axial fan motor with the following specs.

axial fan motor

image

Additional Information

Important Dates

Enrollment Begin: Apr 11 2021

Enrollment Ends: May 12 2021

RoadTesters Selected: May 26 2021 (estimated)

Product Shipped: May 28 2021

RoadTesting Begins: June 4 2021

Reminder/Update Email:July 5 2021

Submit Reviews By: Sept 20 2021

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

 

How to locate the official RoadTest review form:  How To Locate the Official RoadTest Review Form (duplicate)

RoadTesters

Terms and Conditions

Infineon 3-Phase Motor Drive EVB with FOC– RoadTest

Terms and Conditions

These are the terms and conditions which govern the Infineon 3-Phase Motor Drive EVB with FOC RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on May 12 2021

Announcement of Winner (estimated): May 15  2021

Prize: Infineon 3-Phase Motor Drive EVB with FOC
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
  • To all roadtesters,

     

    I spoke with the sponsor today. They are working though the problem you have described. They are also trying to get another tech resource to help. I would expect there might be some delays. So, I have extended the deadline for the review.

     

    I'm not sure you can move forward while we are waiting on the sponsor's feedback to the problem.

     

    I appreciate your efforts and Infineon told me they recognize your efforts and commitment to producing a review.

     

    Sincerely,

     

    Randall Scasny

    RoadTest Program Manager

     

Comment
  • To all roadtesters,

     

    I spoke with the sponsor today. They are working though the problem you have described. They are also trying to get another tech resource to help. I would expect there might be some delays. So, I have extended the deadline for the review.

     

    I'm not sure you can move forward while we are waiting on the sponsor's feedback to the problem.

     

    I appreciate your efforts and Infineon told me they recognize your efforts and commitment to producing a review.

     

    Sincerely,

     

    Randall Scasny

    RoadTest Program Manager

     

Children
  • Hi,

    Did Infineon solved the issue? Any feedback, promised help from their side?

    If I missed any updates - sorry for confusion but browsing product sites I didn't find updated papers or new resources.

    I still hope we can move on!

    Best!

    Marek

  • Apologies - I had intended to write a response to you but the response was eaten up by site maintenance/outage and I forgot to try answering again.

     

    I am still awaiting further communications from Infineon. They have provided me with a combined firmware + parameter .ldf file for loading onto the unit which seems to operate but with a number of issues - incorrect RPM reporting, hesitant start-up, audible "clunk" on start-up. The reason why the original parameters did not work still have not been ascertained and they have not provided the parameter selections necessary for generating the combined file. Unfortunately, with just the combined file, testing other modes of operation (e.g. Vsp control) becomes impossible.

     

    But perhaps the biggest issue concerns programming stability. I was not able to load the .ldf file onto the unit using either one of two Windows 10-based PCs (one AMD, one Intel). The choice of USB controller did seem to make a difference to some degree. I had to pull a Windows 7-based PC out of retirement to get reliable programming and have fed this back in an attempt to have it solved, but it has been a few weeks without a response and it seems 's attempts to follow-up have not been greatly fruitful.

     

    As for ' suggestions, yes, this fan is designed for up to 60Hz operation ordinarily on AC mains for the maximum (rated) rotation speed. Running it on a VFD such as this kit should allow for synthesising an arbitrary rotation speed (i.e. frequency), although over-speeding at greater than 60Hz is likely to cause safety problems. Throwing in a soft-start and getting steady 3-phase output from the board is not really what the product is about as it is "intelligent" with sensorless field-oriented control which should be able to regulate speed, ramp-up/ramp-down rate and provide some feedback control to regulate speed under load as well. It already has per-phase shunt resistors for measurement of current for the flux estimation and overcurrent protection features (in addition to a thermistor for over-temperature protection). It really seems to be pretty "bulletproof" in its design.

     

    The PWM frequency can ordinarily be set - higher frequencies are preferable for reducing audible noise from coils but can cause increased switching losses, so it can be customised. However, the reason why the provided incomplete parameter set in the manual and datasheets does not allow the motor to start up is still not determined - the PWM frequency does not affect this much from what I could tell as I did try changing the parameter.

     

    - Gough