RX23W BLE 5.0 Module Target Development Board

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content

About

If you are building IOT projects that require Bluetooth Low Energy and easy access to MCU pins for fast prototyping to a bread board, you should consider applying for this roadtest.

 

This target development board has an RX23W BLUETOOTH® 5.0 Low Energy Module with integrated antenna and oscillator. This product provides through-holes for pin headers that allow access to all MCU signal pins, allowing an easy prototyping with a breadboard.

 

Target Board vs. Development Board vs. Fast Prototyping Board

Traditionally, a target board is the board that contains the MCU that requires programming with often times an external programmer, which increases the cost. Many MCU development boards today have an onboard debuggers or emulators. A fast prototyping board has the additional features of through-holes for pin headers that give you access to all MCU signal pins, allowing an easy prototyping with a breadboard. The RX23W Module Target Development Board combines all these elements onto one board. In addition, The RX Target Board allows the reuse of the same PCB for all MCU variations

 

Let's Talk about the RX23W Bluetooth® 5.0 Low Energy Module

The RX23W Module has  full Bluetooth® 5.0 Low Energy support for system control and wireless communication on IoT endpoint devices. Featuring the RX23W 32-bit RX MCU supporting fully integrated Bluetooth Low Energy communication, the module is equipped with an antenna, oscillator and custom-matched circuit. It is certified under Radio Law for multiple countries, including Japan and the United States, and is Bluetooth SIG certified. This eliminates the need for additional RF design work, tuning, or specialized RF knowledge. The very small 6.1 mm x 9.5 mm, 83-pin LGA package makes it possible to design more compact devices with fewer external components, reducing the bill of materials (BOM) cost.

 

The RX23W MCU incorporated in the new module supports full Bluetooth 5.0 Low Energy communication support including long-range and 2 Mbps data throughput. It delivers excellent communication characteristics, with reception sensitivity level of −105 dBm at 125 kbps.The RX23W also incorporates Renesas’ exclusive security function, the Trusted Secure IP (TSIP), that provides robust protection against threats to IoT devices such as eavesdropping, tampering, and viruses. In addition, the RX23W MCU has a rich set of peripheral functions that is indispensable to IoT devices, including touch key, USB, and CAN functions.

target board for RX23W module

 

Key Features of the RX23W Module Target Development Board

  • On-board RX23W module
  • Excellent choice for basic evaluation and development of selected module
  • Full access to all pins by provided header through-hole connections
  • Included on-chip debugging can be used for own development
  • USB connector to power and debug the MCU (no USB cable included)
  • Development environment like e² studio can be downloaded for free
  • Board size is 54mm x 90mm, thickness is 1.6mm
  • USB connector: 5V input, power-supply IC: 5V input, 3.3V output
  • Power indicator: green x 1, user: green x 2. ACT LED: green x 1
  • Pmod™ connector, Arduino™ UNO connectors, MCU headers, Arduino™ UNO headers

 

image

The RX23W Module Target Development Board can handle the following tasks

  • Programming of the Renesas MCU
  • Debugging of user code
  • Evaluation of Bluetooth Low Energy communications
  • User circuits for switches and LEDs
  • Sample applications*
  • Samples of peripheral-function initialization code*

Note: These are available for downloading from the Renesas Website

 

image

Additional Information

Important Dates

Enrollment Begin: Jun 9 2021

Enrollment Ends: July 28 2021

RoadTesters Selected: Aug 4 2021 (estimated)

Product Shipped: Aug 4 2021

RoadTesting Begins: Aug 11 2021

Reminder/Update Email: Sept 11 2021

Submit Reviews By: Oct 11 2021

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

 

How to locate the official RoadTest review form:  How To Locate the Official RoadTest Review Form (duplicate)

RoadTesters

(due Oct 11 2021)

  (due Oct 11 2021)

(due Oct 15 2021)

  (due Oct 20 2021)

Terms and Conditions

Target Board for RX23W Module– RoadTest

Terms and Conditions

These are the terms and conditions which govern the Target Board for RX23W Module RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on July 28 2021

Announcement of Winner (estimated): July 29  2021

Prize: Target Board for RX23W Module Target Development Board

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comment List
Anonymous
  • If you have any content that's in progress, whether it's a RoadTest Review, Design Challenge application, blog, or other content that is 'saved as a draft' or in a 'draft status' then it will not be coming over to the new platform. Make sure you've either published your content, or saved the content that you currently have saved as a draft off the Community, as it will not be copied over to the new platform at all, before Friday the 5th of November 2021.

      (due Oct 20 2021)

  • The specs and member comments on the product sound interesting to me. I'm interested in experimenting with Evaluation kits. I'd like to compare this kit with other Evaluation Kits. I'm always interested in trying different Kits and experimenting  with embedded software development  environments

     

    I have experimented with several varieties of MCU evaluation kits, but never had the pleasure to try embedded programming on a fast prototyping board.The additional features of through-holes for pin headers allowing access to all MCU signal pins and allowing easy prototyping with a breadboard, is intriguing to me.

    Steve K

  • I updated the description of this product.

     

    Randall Scasny

    Roadtest Program Manager

  • I'm kinda curious how these Renesas RX23W modules compare to something like the Nordic nRF52 modules.

  •   wrote:

    ...  Looks like an interesting platform...

    Yes, with the CAN support as the extra highlight. From a company that's strong in the automotive sector.

    We don't see that often here, road tests that give access to CAN. Good for the curriculum.

  • I didn't know what an rx23w module was, so I looked it up:

     

    • 32-bit MCU with Bluetooth 5
      • RXv2 Core running 54 MHz (I don't know anything about these.)
    • 512 Kb Flash, 64Kb RAM (both are up to...)
    • USB 2.0 OTG support
    • CAN
    • SDIO 1- and 4-bit
    • Cap Touch Sensing
    • 14 channel 12-bit ADC
    • 2 channel 12-bit DAC

     

    Looks like an interesting platform on a highly accessible board.

  • I agree but with limits. Imagine searching for a pin on a board with MCU with over 200 GPIOs exposed....

  • I like this kind of evaluation board, where all controller pins are available.