Sanitary Metal Pipe Clamp HANI™ Temperature Sensor - Industrial Sensing

Table of contents

image

 

{tabbedtable} Tab Label Tab Content
About

In this roadtest, you will test out the use, ease-of-installation, and response times of a non-invasive Sanitary Metal Pipe Clamp HANI™ Temperature Sensor by Omega Engineering.

image

Omega’s clamp-on design makes sensor installation easy. Unlike invasive sensors, the HANI™ Clamp Sensor mounts to the outside of an sanitary metal pipe and measures the temperature of the process media inside the pipe.

 

This video gives you a good understanding of how the Clamp HANI™ Temperature Sensor is used and installed:

 

 

Back to Basics: Invasive versus Non-Invasive Temperature Sensor

Temperature sensors are crucial in food and beverage manufacturing applications. Invasive temperature sensors are installed in the pipe such that the sensor comes in direct contact with the media flowing in the pipe. Overtime, buildup can occur on the invasive sensor, which can affect accuracy, cause sensor draft, clog pipes, and reduce flow. A non-invasive sensor such as the HANI™ Clamp Sensor avoids these problems since it clamps on the metal pipe externally.

 

Features of the HANI™ Clamp Sensor

  • Non-invasive temperature measuring fluid inside the pipe
  • No process downtime or welding needed for install
  • Installation in a matter of seconds with clamping mechanism
  • As accurate as an invasive sensor, ±0.50°C accuracy
  • Response time = 5 sec (t63), 10 sec (t90)
  • Currently available for 1.5" and 2.0” pipe diameters
  • Process temperature from 0 to 100°C
  • M12 8-pin connection for versitile communication
  • 4-20mA loop powered analog output
  • Smart Core integration for LayerN interfacing
  • Patent pending and IP65 rated

 

Some More Basics: Pipe Types, Sizes, and Metals

Process metal piping is supplied in various materials, inner diameters (ID) and outer diameters (OD). There are two types of pipes often used, Industrial and Sanitary. Commonly used metal material for both types is stainless steel but industrial pipes are also available in carbon steel, galvanized steel, copper, brass and aluminum. The nominal size of the inside and outside diameters vary depending on the pipe size and must be considered when choosing piping for your process and when choosing the appropriate HANI clamp sensor.

 

  • Sanitary Metal Pipes: Sanitary pipes, also known as sanitary or hygienic tubing, do not have varying wall thickness. The thickness of the wall is defined in table below. Sanitary pipes are usually supplied in different grades of polish on the exterior and interior. Polish grade is sometimes referred to as Ra or Rz finish, but this can vary. Sanitary pipes have smoother/higher polish surface finishes when compared to industrial pipes. Please note, unlike industrial pipes, sanitary pipes have a nominal size equal to the outside diameter.
  • Industrial Metal Pipes: The nominal pipe size for industrial pipes is different from the outer diameter, please refer to table for actual pipe dimensions. Industrial pipes have different ID’s based on their “Schedule”. The pipe schedule identifies the pipe thickness based on the pipes nominal size. The higher the schedule the thicker the pipe, standard thickness is schedule 40. Schedules 40 and 80 are most commonly used but 10, 120, 160 and thicker schedules are available.
  • Thermal Conductivity: The process media or fluid is an important consideration when choosing a HANI clamp temperature sensor. Process fluids with a higher thermal conductivity will transfer heat to the pipe much better than fluids with lower thermal conductivity.

 

Sensor Model Table

The sensor you receive will depend on the diameter of the sanitary stainless steel metal pipe you will be using to measure temperature:

image

Note: All models have the following specs:

  • Sensor Application: Sanitary Metal Pipe
  • Accuracy: ±0.5°C
  • Response Time: 5 sec (t63), 10 sec (t90)
  • Output: 4-20mA
  • Connection Type: M12 8-Pin
  • Temp Range: 0° (32°F) to 100°C (212°F)

 

How To Install A HANI Sensor

There are three simple steps for installing an HANI Sensor:

  • Step 1: Clamp onto the pipe
  • Step 2: Connect cable to output device
  • Step 3: start measuring

 

To Learn more, go to these Resources:

 

Note: there are the following videos on the HANI support page:

  • Video: Mounting the Sensor
  • Video: Connecting the Hani Sensor to Synch Software
  • Video: Connecting the Hani Sensor to a 4-20mA Analog System
Important Dates

Enrollment Begin: Aug 3 2021

Enrollment Ends: Sept 17 2021

RoadTesters Selected: Sept 20 2021 (estimated)

Product Shipped: tbd

RoadTesting Begins: tbd

Reminder/Update Email: tbd

Submit Reviews By: tbd

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

 

How to locate the official RoadTest review form:  How To Locate the Official RoadTest Review Form (duplicate)

RoadTesters

  HANI-C-2.0S-M-MA  (2-inch piping)

  HANI-C-1.5S-M-MA  (1.5-inch piping)

Terms and Conditions

Sanitary Metal Pipe Clamp HANI™ Temperature Sensor– RoadTest

Terms and Conditions

These are the terms and conditions which govern the  Sanitary Metal Pipe Clamp HANI™ Temperature Sensor RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on Sept 17  2021

Announcement of Winner (estimated): Sept 20 2021

Prize:  Sanitary Metal Pipe Clamp HANI™ Temperature Sensor
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
  • IMPORTANT DATE UPDATE

    Enrollment Begin: Aug 3 2021

    Enrollment Ends: Sept 17 2021

    RoadTesters Selected: Oct 7 2021

    Product Shipped: Oct 8 2021

    RoadTesting Begins: Oct 18 2021

    Reminder/Update Email: Nov 18 2021

    Submit Reviews By: Dec 18 2021

Comment
  • IMPORTANT DATE UPDATE

    Enrollment Begin: Aug 3 2021

    Enrollment Ends: Sept 17 2021

    RoadTesters Selected: Oct 7 2021

    Product Shipped: Oct 8 2021

    RoadTesting Begins: Oct 18 2021

    Reminder/Update Email: Nov 18 2021

    Submit Reviews By: Dec 18 2021

Children
No Data