Freescale MMA845XQ Evaluation board and LFSTBUSB Accelerometer Interface Board

Table of contents

Freescale LFSTBEB8450 MMA845XQ Evaluation board provides an evaluation board for the MMA8450Q 3-axis high performance, high functionality low-g accelerometer. The LFSTBEB8450 includes an 8-bit MC9S08QE8CWL MCU for data acquisition, and an EEPROM for data storage. For customers already familiar with the Sensor Toolbox Platform, the LFSTBEB8450 is designed to work with the LFSTBBAT9 for power or LFSTBUSB for communication to a PC.

 

The STBUSB: Sensor Toolbox Accelerometer USB Interface boardSTBUSB: Sensor Toolbox Accelerometer USB Interface board provides a USB or BDM interface for use with Sensor Toolbox evaluation boards. It is designed to work with the various members of the Sensor Toolbox.

RoadTest Reviews
Comment List
Anonymous
Parents
  • When do I receive the part for review?

     

    EDIT 6.4.2011: got it this monday, review to be done next weekend.

    EDIT 18.4.2011: the review got postponed as i was participating a 24h coding competition. this is next on my TODO list.

    EDIT 9.5.2011: the review is blocked due to missing support for Linux. The development kit supports only Microsoft Windows, althought there are no operating system requirements anywhere. And freescale does not reply to the support ticket SR 1-742776043, which was raised 22.4.2011. The current review can be seen  http://code.google.com/p/quickanddirty/wiki/Review_Freescale_LFSTBUSB_LFSTBEB845x, But all in all the sensorkit is a good idea, but it has been implemented poorly with .NET. I just can not understand why they have not used any crossplatform framework like Qt. As the device itself is detected as serial port and can be used on other operating systems than Windows.

    EDIT 9.5.2011: Unable to submit review with Ubuntu 11.04 + Chromium 11. The review post will get a result of "An unexpected error has occurred"

     

    The end result with the Sensor Kit is that "it is a nice idea, but poor desktop software implementation is blocking the real usage". I would have wanted to use this in my robotics project with that usb-serial connectivity board. But for that I would have to implement my own 3rd party library, and as Freescale has not released any official documentation about the protocol and as they do not answer to the technical tickets in 48h as promised on their website, now it has been over three weeks..

  • Hello Juhapekka,

    I am from Freescale, I can´t comment on the technical review, not my specialty area. But I did a check on the open tickets and sorry to say, but you did _not_ submit one to us. You misinterpreted the automatic logging of your online chatting with us as an open ticket. Sorry for that misunderstanding but the ticket was created by the system and instantly closed again with your submitted chat survey result to timestamp the interaction. We do strive for 48hrs and honestly can often but not always meet them, but we don´t let our customers knowingly wait for weeks, sorry for the misunderstanding.

    I will create an empty ticket and write to you to let you reply back with your actual questions. Thanks for your interest in Freescale anyway. The rule says: complaining customers still have an interest, the silent ones are the ones that are lost. Hope we did not lose you ...

    Cheers,

    Toni

  • I am still interested about your products. But you must know that I received following email with status "public information":  http://pastebin.com/3zkD48UF

     

    And I got contacted by B16998 on 23.4.2011. But the email was with status "[x] Freescale Semiconductor Confidential Proprietary". So I will forward you the email asap. I also replied to that one, but there was no reply anymore.. The content of the email was that you do not support Linux at the moment and a promise to contact me further.. Thats why I was stating in my post "missing support for Linux".

     

    But anyway, thanks for hearing me. image ..and I would be able to write my own library for the kit with Qt/C++ for you, if you will give the technical support and provide officially the technical protocol documentation of the communication over the serial bridge for the community as public information. As I have also noted in my wiki page, that there is actually one protocol file included in the .NET application installation package SensorToolbox_SerialProtocol.2.0.doc, but it is labeled "Freescale Internal Use Only".

Comment
  • I am still interested about your products. But you must know that I received following email with status "public information":  http://pastebin.com/3zkD48UF

     

    And I got contacted by B16998 on 23.4.2011. But the email was with status "[x] Freescale Semiconductor Confidential Proprietary". So I will forward you the email asap. I also replied to that one, but there was no reply anymore.. The content of the email was that you do not support Linux at the moment and a promise to contact me further.. Thats why I was stating in my post "missing support for Linux".

     

    But anyway, thanks for hearing me. image ..and I would be able to write my own library for the kit with Qt/C++ for you, if you will give the technical support and provide officially the technical protocol documentation of the communication over the serial bridge for the community as public information. As I have also noted in my wiki page, that there is actually one protocol file included in the .NET application installation package SensorToolbox_SerialProtocol.2.0.doc, but it is labeled "Freescale Internal Use Only".

Children
No Data