Weller 200W High Powered Digital Soldering Stations

View table of contents ...  

This month, we are pleased to be giving away 3 Weller 200W High Powered Digital Soldering Stations – the WX1010, WX1012 and WX2020. The soldering stations have a temperature range of 150° F to 850° F, with an accuracy of +/- 17° F (9° C). The WX1012 station comes with a WXP65 Pencil which has a 0098" / 0.25mm Micro Tip. While the WX1010 an WX2020 both come with the WXP120 Pencil which has a .094" x 1.420" Reach Chisel Tip. The WX2020 has 2 soldering pencils and 2 iron stands. The stations are rated at an input of 120V.

 

image

 

 

The Weller WX system keeps your cost of ownership low with Intelligent power management to conserve energy and an exceptional degree of tool compatibility.

 

200 I   240W Total Power

Supports operation of one 200W tool or simultaneous   operation of two 120W tools (WX2 Only)

Viewable   From All Angles

Blue LED Backlighting to strengthen   visibility

Global   Language Support

Display multiple languages through menu selection

Intuitive   Interface

Six touch keys with radius finger guide for   turn-and-click navigation

Robust   Touch Screen

Patented, capacitive touch screen made of antistatic,   chemical and temperature resistant glass

Intelligent   Tool Recognition

Quick change connectors enable rapid tool   interchange

Multi-Purpose USB Port

Quick and localized software updates, parameter   configuration and data logging via USB stick

Intelligent   Accessory Management

Dual port configuration to manage fume extractors,   heating plates and programmable logic controllers

RoadTest Reviews
Comment List
Anonymous
Parents
  • I don't think that it is too much hard to adopt it to 220 V input. Yes, it is a very well product from Weller as it is usual. Though, i will not enroll. I do not think random choosing is a right choice for all roadtested products. It may be fine for some products in general use but not for all of them. So, waiting for a roadtest to end and expecting to be one of the 1200 members is to much optimistic. Sure a roadtester just enrolls and waits for the result. You did not win! Do not worry! Try the next. In a well-formed roadtest, one could say "Yes, i have a chance this time, i can win". This would make me in excitement, not the usual way. I should feel that i have a chance. Otherwise, there is no point.

     

    Good luck for the ones that enroll.

     

    Firat

Comment
  • I don't think that it is too much hard to adopt it to 220 V input. Yes, it is a very well product from Weller as it is usual. Though, i will not enroll. I do not think random choosing is a right choice for all roadtested products. It may be fine for some products in general use but not for all of them. So, waiting for a roadtest to end and expecting to be one of the 1200 members is to much optimistic. Sure a roadtester just enrolls and waits for the result. You did not win! Do not worry! Try the next. In a well-formed roadtest, one could say "Yes, i have a chance this time, i can win". This would make me in excitement, not the usual way. I should feel that i have a chance. Otherwise, there is no point.

     

    Good luck for the ones that enroll.

     

    Firat

Children
No Data