STMicroelectronics STM32F4DISCOVERY Discovery kit for STM32 F4 series

Table of contents

image

Introduction

 

 

The STM32F4DISCOVERY helps you to discover the STM32F4 high-performance features and to develop your applications easily. It includes everything required for beginners and experienced users to get started quickly.

 

 

 

Based on the STM32F407VGT6, it includes an ST-LINK/V2 embedded debug tool, two ST MEMS, digital accelerometer and digital microphone, one audio DAC with integrated class D speaker driver, LEDs and push buttons and an USB OTG micro-AB connector.

 

Key Features

 

  • STM32F407VGT6 microcontroller featuring 32-bit ARM Cortex-M4F core, 1 MB Flash, 192 KB RAM in an LQFP100 package
  • On-board ST-LINK/V2 with selection mode switch to use the kit as a standalone ST-LINK/V2 (with SWD connector for programming and debugging)
  • Board power supply: through USB bus or from an external 5 V supply voltage
  • External application power supply: 3 V and 5 V
  • LIS302DL, ST MEMS motion sensor, 3-axis digital output accelerometer
  • MP45DT02, ST MEMS audio sensor, omni-directional digital microphone
  • CS43L22, audio DAC with integrated class D speaker driver
  • Eight LEDs:
    • LD1 (red/green) for USB communication
    • LD2 (red) for 3.3 V power on
    • Four user LEDs, LD3 (orange), LD4 (green), LD5 (red) and LD6 (blue)
    • 2 USB OTG LEDs LD7 (green) VBus and LD8 (red) over-current
  • Two push buttons (user and reset)
  • USB OTG FS with micro-AB connector
  • Extension header for all LQFP100 I/Os for quick connection to prototyping board and easy probing
Comment List
Anonymous
Parents
  • Congratulations to all of those VERY lucky winners, that's a really nice eval kit you guys got your hands on!!!

     

    I was really hoping that I would be chosen to evaluate this board, if I had the money I would 100% consider buying one right now but alas, it's not in the cards for me, my kids take priority of ALL of my extra cash. lol

     

    There's always the next road test, here's to hoping that it's a really good eval board (I'm crossing my fingers for a Kenetis tower or (if I could be one of the luckiest people alive) a nice Digital Multimeter like the one by Techtronix featured a few months back as a Roadtest.

     

    As always, this site is one of my favorite places to visit when I get some free time away from the kids.

     

    Keep up the great work guys and gals (staff of Element14 and members of the site) you're all great people!

Comment
  • Congratulations to all of those VERY lucky winners, that's a really nice eval kit you guys got your hands on!!!

     

    I was really hoping that I would be chosen to evaluate this board, if I had the money I would 100% consider buying one right now but alas, it's not in the cards for me, my kids take priority of ALL of my extra cash. lol

     

    There's always the next road test, here's to hoping that it's a really good eval board (I'm crossing my fingers for a Kenetis tower or (if I could be one of the luckiest people alive) a nice Digital Multimeter like the one by Techtronix featured a few months back as a Roadtest.

     

    As always, this site is one of my favorite places to visit when I get some free time away from the kids.

     

    Keep up the great work guys and gals (staff of Element14 and members of the site) you're all great people!

Children
No Data