STMicroelectronics STM32F4DISCOVERY Discovery kit for STM32 F4 series

Table of contents

image

Introduction

 

 

The STM32F4DISCOVERY helps you to discover the STM32F4 high-performance features and to develop your applications easily. It includes everything required for beginners and experienced users to get started quickly.

 

 

 

Based on the STM32F407VGT6, it includes an ST-LINK/V2 embedded debug tool, two ST MEMS, digital accelerometer and digital microphone, one audio DAC with integrated class D speaker driver, LEDs and push buttons and an USB OTG micro-AB connector.

 

Key Features

 

  • STM32F407VGT6 microcontroller featuring 32-bit ARM Cortex-M4F core, 1 MB Flash, 192 KB RAM in an LQFP100 package
  • On-board ST-LINK/V2 with selection mode switch to use the kit as a standalone ST-LINK/V2 (with SWD connector for programming and debugging)
  • Board power supply: through USB bus or from an external 5 V supply voltage
  • External application power supply: 3 V and 5 V
  • LIS302DL, ST MEMS motion sensor, 3-axis digital output accelerometer
  • MP45DT02, ST MEMS audio sensor, omni-directional digital microphone
  • CS43L22, audio DAC with integrated class D speaker driver
  • Eight LEDs:
    • LD1 (red/green) for USB communication
    • LD2 (red) for 3.3 V power on
    • Four user LEDs, LD3 (orange), LD4 (green), LD5 (red) and LD6 (blue)
    • 2 USB OTG LEDs LD7 (green) VBus and LD8 (red) over-current
  • Two push buttons (user and reset)
  • USB OTG FS with micro-AB connector
  • Extension header for all LQFP100 I/Os for quick connection to prototyping board and easy probing
Comment List
Anonymous
Parents
  • Is this all the comments so far? ..

     

    I purchase the STM32F Discovery board from mouser about 4 months ago and it took me forever to figure out the toolchain. The software is proprietary, commercial & closed source. I watched several videos of RTOS being ran on this mcu but the free version of the IDE but the upload cap of the IDE prevents the ability to upload RTOS.

     

    I wound up intstalling somewhere around ten different programs. I spent hours on each one trying to get the settings right and the ST-link to work. I finally was able to instal a sample code that utilized the CS43L22 audio DAC to play 3 seconds of an audio file.

     

    Perhaps I'm simply unexperienced or maybe a slow learner but it the learning curve of the tool chain associated with this board seemed counter intuitive. I could see working for a large company who has full versions of the software and perhaps trains you to use it but for the basement dwelling prototypers &  self taught engineers just starting out like myself, expect to spend a bit of time wrapping your head around the process of utilizing all the great attractive features of this board.

     

    I wish luck to all those who have this board and hope that you had a better experience than me. I don't want to steer anyone away from this product because its a dreamy board at a price you can't beat. So for those that didn't have trouble getting to know the ins and outs of the STM32F4, please spread the wisdom in tutorials/posts/blogs.

     

    Thank you for your time and I would really like to hear from others about your experience with this board. Did you find programming and debugging it easier than I did? I gave around  48 hours to this board and haven't touched it since but a good tutorial may be what inspires me to dive back in. Have a nice day.

  • I have been using the STM32F4 Discovery for a few months now, it is an excellent piece of kit for the price!

    I am developing touch screen LCD applications, and am the moment finishing an OV7670 cmos camera module driver which outputs RGB565 and scales to QVGA (YUV) for the HY32D LCD, take a look at my Blog if you are interested...if not, will be happy to help you  with any problems you may have with IDE's or any other issues around the STM32F4.

Comment
  • I have been using the STM32F4 Discovery for a few months now, it is an excellent piece of kit for the price!

    I am developing touch screen LCD applications, and am the moment finishing an OV7670 cmos camera module driver which outputs RGB565 and scales to QVGA (YUV) for the HY32D LCD, take a look at my Blog if you are interested...if not, will be happy to help you  with any problems you may have with IDE's or any other issues around the STM32F4.

Children
No Data