STMicroelectronics STM32F4DISCOVERY Discovery kit for STM32 F4 series

Table of contents

image

Introduction

 

 

The STM32F4DISCOVERY helps you to discover the STM32F4 high-performance features and to develop your applications easily. It includes everything required for beginners and experienced users to get started quickly.

 

 

 

Based on the STM32F407VGT6, it includes an ST-LINK/V2 embedded debug tool, two ST MEMS, digital accelerometer and digital microphone, one audio DAC with integrated class D speaker driver, LEDs and push buttons and an USB OTG micro-AB connector.

 

Key Features

 

  • STM32F407VGT6 microcontroller featuring 32-bit ARM Cortex-M4F core, 1 MB Flash, 192 KB RAM in an LQFP100 package
  • On-board ST-LINK/V2 with selection mode switch to use the kit as a standalone ST-LINK/V2 (with SWD connector for programming and debugging)
  • Board power supply: through USB bus or from an external 5 V supply voltage
  • External application power supply: 3 V and 5 V
  • LIS302DL, ST MEMS motion sensor, 3-axis digital output accelerometer
  • MP45DT02, ST MEMS audio sensor, omni-directional digital microphone
  • CS43L22, audio DAC with integrated class D speaker driver
  • Eight LEDs:
    • LD1 (red/green) for USB communication
    • LD2 (red) for 3.3 V power on
    • Four user LEDs, LD3 (orange), LD4 (green), LD5 (red) and LD6 (blue)
    • 2 USB OTG LEDs LD7 (green) VBus and LD8 (red) over-current
  • Two push buttons (user and reset)
  • USB OTG FS with micro-AB connector
  • Extension header for all LQFP100 I/Os for quick connection to prototyping board and easy probing
Comment List
Anonymous
Parents
  • I'm Using keil software on STM32f4Discovery at the uniwersity (we recently won it in one competition) and as I know keil is free but just has the restriction of 32k of software size. I do not reaaly know if this sestriction is just for code you write and for kompiled file or just for debugging. But it is free, just need to register and get a serial. I have not tryed using it much, because I do not have so much free time, but I liked this software. Atleest for me it seems better when other I have seen but didn't tryed. So I might be wrong. image

    Its just my opinion.

Comment
  • I'm Using keil software on STM32f4Discovery at the uniwersity (we recently won it in one competition) and as I know keil is free but just has the restriction of 32k of software size. I do not reaaly know if this sestriction is just for code you write and for kompiled file or just for debugging. But it is free, just need to register and get a serial. I have not tryed using it much, because I do not have so much free time, but I liked this software. Atleest for me it seems better when other I have seen but didn't tryed. So I might be wrong. image

    Its just my opinion.

Children
No Data