Agilent 33522B 30MHz 2-Channel Waveform Generator with Arbitrary Waveform Generation

View table of contents ...  

image
Agilent’s 33500B Series waveform generators with exclusive Trueform signal generation technology offer more capability, fidelity and flexibility than traditional DDS generators. Easily generate the full range of signals you need to test your devices with confidence the signal generator is outputting the signals you expect with 12x less jitter and 5x less harmonic distortion.  Take advantage of deep memory (1M points standard and optional 16M points) and waveform sequencing.  Two-channel models allow you to use the channels independently or sync them in time, amplitude or both. 
Q&A
What we would like to see in the road test?
Applications that take advantage of our Trueform technology. Some examples:
  • Applications that use multiple waveforms; sine waves, square waves, pulses, or custom waveforms.
  • Applications requiring low harmonic distortion sine waves
  • Applications that need pulses or square waves with low jitter.
  • Applications that need point-by-point arbitrary waveform capability – more accurate user defined waveforms.
  • Applications requiring deep memory or can take advantage of sequencing to create user defined waveforms.
  • An application that uses IQ signals or needs to output a data pair. E.g. A dual channel custom waveform
Are there certain application areas we would like folks working on?
We believe that most of the applications requiring Trueform Technology will be in: Research, Design, Product Development, Hardware Qualification, and Design Verification. It is less likely to find these applications in; Service, Installation, or Maintenance.
Reference Material
Terms & Conditions
  • Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
  • Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
  • Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
RoadTest Reviews
Comment List
Anonymous
Parents
  • Dear all,

    I'd rather not post personal information as I don’t think it is at all dignified but has there has been some comments about delayed road tests I think I need to.

    You can see I posted that I had unexpectedly received the Agilent 33522B on the 23rd of October.

     

    To my great grief my father passed away on their 24th and I was interstate with my mother until the funeral on 2nd of Nov. On the day of the funeral my material grandmother passed away, meaning I had to travel back for this funeral as well.

    This is too much information for group like this and maybe I am reacting in anger  but I think the members of the group need to moderate their comments about slow reviews and understand that some people have a life outside work and electronics.

     

    I will post a full review within a matter of days

     

    Michael

  • Dear Michael,

     

    First of all my condolences to your father and grandmother passing. I can't imagine it is easy for anyone.

     

    Please do not worry about the review, do it when you feel ready for that. I find it honorable that you wanted to bring it to the attention of the community, even when it is an enormous emotional load to take on.

     

    Do not feel pressured about the roadtest, just let the test organizer know of the situation in general and it will all be fine.

     

    My sincere apologies that you have received an additional burden from this, I'm sure it was never anyones intention.

     

    You are honest and have nothing to explain for, keep strong!

     

     

    Regards,

     

     

    Elias Sajo

Comment
  • Dear Michael,

     

    First of all my condolences to your father and grandmother passing. I can't imagine it is easy for anyone.

     

    Please do not worry about the review, do it when you feel ready for that. I find it honorable that you wanted to bring it to the attention of the community, even when it is an enormous emotional load to take on.

     

    Do not feel pressured about the roadtest, just let the test organizer know of the situation in general and it will all be fine.

     

    My sincere apologies that you have received an additional burden from this, I'm sure it was never anyones intention.

     

    You are honest and have nothing to explain for, keep strong!

     

     

    Regards,

     

     

    Elias Sajo

Children
No Data