Agilent 33522B 30MHz 2-Channel Waveform Generator with Arbitrary Waveform Generation

View table of contents ...  

image
Agilent’s 33500B Series waveform generators with exclusive Trueform signal generation technology offer more capability, fidelity and flexibility than traditional DDS generators. Easily generate the full range of signals you need to test your devices with confidence the signal generator is outputting the signals you expect with 12x less jitter and 5x less harmonic distortion.  Take advantage of deep memory (1M points standard and optional 16M points) and waveform sequencing.  Two-channel models allow you to use the channels independently or sync them in time, amplitude or both. 
Q&A
What we would like to see in the road test?
Applications that take advantage of our Trueform technology. Some examples:
  • Applications that use multiple waveforms; sine waves, square waves, pulses, or custom waveforms.
  • Applications requiring low harmonic distortion sine waves
  • Applications that need pulses or square waves with low jitter.
  • Applications that need point-by-point arbitrary waveform capability – more accurate user defined waveforms.
  • Applications requiring deep memory or can take advantage of sequencing to create user defined waveforms.
  • An application that uses IQ signals or needs to output a data pair. E.g. A dual channel custom waveform
Are there certain application areas we would like folks working on?
We believe that most of the applications requiring Trueform Technology will be in: Research, Design, Product Development, Hardware Qualification, and Design Verification. It is less likely to find these applications in; Service, Installation, or Maintenance.
Reference Material
Terms & Conditions
  • Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
  • Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
  • Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
RoadTest Reviews
Comment List
Anonymous
Parents
  • Hi Everyone.

     

    Thank you all for applying. This RoadTest is now closed. We are pleased to announce the following members that have been selected to receive this Road Test:

     

    • Troy Mills
    • Kyle Krupinski
    • David Weight

     

    Congratulations! Your product will be shipped to the address each of you provided when you applied for this RoadTest. As a reminder, element14 and our supplier partners send these products free-of-charge because we place high value upon your unbiased, detailed product review. Please post your review back here within 3-6 weeks of receiving your item.

     

    For those who were not selected to win this product, we have the NXP LPC4330-Xplorer Board Road Test open for applicants

     

    Enroll today and Good Luck!!!  image

  • Hi Joann,

     

    Sorry I'm a little bit behind on turning in the review. I haven't had as much time as i would have liked due to some extra scheduleing they threw me into for one of my classes, and as a result, I honestly just forgot to post my wright up. Where exactly do I post it at? Is it just a comment here or else where? I'm still kind of new to the format of things around here.

  • Kyle -

     

    You submit your RoadTest in the following manner -

     

    If you look above at the list of "RoadTesters", you should be able to find your name - next to it will be a link that says "Write Review".  Click this, and write your review on the subsequent page.

     

    Please ensure you fill in all the fields and be as thorough as possible. 

     

    Many thanks.

  • Kyle - another way to get there is to log in, then use the New menu at the top of the screen.. select Road Test Review from the list. Let us know if you hit any problems.

     

    Matt.

Comment Children
No Data