The U1273AX OLED handheld digital multimeter, the latest addition to U1270 Series, is capable of operating in winter weather down to –40°C temperature.
Even in frigid conditions, the U1273AX enables you to achieve immediate and accurate results without the need to warm up in advance.
OLED for more display clarity
Designed with OLED display, you can experience crystal-clear measurement readings with its outstanding 2000:1 contrast ratio. The display also allows wider viewing angles up to 160 degrees ensuring you get the right readings at the first glance even in poorly lit environments.
Increase productivity with Bluetooth® wireless connectivity
For wireless connectivity to smartphones and tablets, the U1270 Series is compatible with the U1177A infrared-to-Bluetooth adapter for maximum efficiency and productivity in completing measurements tasks.
Adding the optional U1177A to a U1270 Series you can easily perform remote monitoring and data logging via Android devices or Windows®-based PC.
Promotions
For customers in Europe, click on the following link to view promotion to get a free U1177A Bluetooth adapter for wireless logging and data transfer: [LINK]
Based in the US or Canada? Click here instead to view related promotions from Agilent Technologies: [LINK]
Product Videos
This video is unavailable.
You don't have permission to edit metadata of this video.
This video is unavailable.
You don't have permission to edit metadata of this video.
Terms & Conditions
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
A little diffuculty in believing that one can touch an object which is just taken from a -40°C chamber with his bare hands.
Its just my preconception about low temperature,i havn't experimented a temperature below 0°C. If i am little wierd do laugh at me,all goes in a sportsman spirit.
A little diffuculty in believing that one can touch an object which is just taken from a -40°C chamber with his bare hands.
Its just my preconception about low temperature,i havn't experimented a temperature below 0°C. If i am little wierd do laugh at me,all goes in a sportsman spirit.
I had a few times below 0°C (Winter maintenance), but not in any way like it is said to be capable.....where are the Skandinavians?!?!?! :-D
My biggest plus is that it's said to be accurate at low temp from the start on. So no need to warm it up and let it stabilize, just grab and measure at low temperatures?!
At work we handle bits straight out of the chamber down to -70 or so. If it was metal or a material that conducts heat quickly, you'd be right. But as it's plastic, -40 isn't too bad at all and doesn't make your hands particularly cold. Keeping the accuracy of that meter working down to -40 though, pretty impressive.
Do anybody has an idea of techology used inside this multimIeter to keep it working in so lower temperatures?.I hope for some superconductivty related technologies used with great structural design. Lets hope we get a chance to open it up.
I wouldn't be surprised if it's just in the insulation of the case - would be a lot easier to design a rugged outer shell that protects the stuff inside from the cold than to use electronics specifically designed for low temperatures. Don't expect superconductors though, even "high temperature" superconductors have transition temperatures around -135°C (bismuth strontium calcium copper oxide/BSCCO is an exampe)
As for the OLED display, there might be a small onboard heater that turns on when it's cold, but I'm not sure - as you say, we'll just have to tear it apart to find out
Top Comments
At work we handle bits straight out of the chamber down to -70 or so. If it was metal or a material that conducts heat quickly, you'd be right. But as it's plastic, -40 isn't too bad at all and doesn't…
Yes, well, but it is an modified U1273A.
All the Agilent Handheld Multimeter have Bluetooth capability. It's just an attachment you clip on the IR-Port.....working pretty nice and I often use it with my…
-
rufzalta
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
rufzalta
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children