The U1273AX OLED handheld digital multimeter, the latest addition to U1270 Series, is capable of operating in winter weather down to –40°C temperature.
Even in frigid conditions, the U1273AX enables you to achieve immediate and accurate results without the need to warm up in advance.
OLED for more display clarity
Designed with OLED display, you can experience crystal-clear measurement readings with its outstanding 2000:1 contrast ratio. The display also allows wider viewing angles up to 160 degrees ensuring you get the right readings at the first glance even in poorly lit environments.
Increase productivity with Bluetooth® wireless connectivity
For wireless connectivity to smartphones and tablets, the U1270 Series is compatible with the U1177A infrared-to-Bluetooth adapter for maximum efficiency and productivity in completing measurements tasks.
Adding the optional U1177A to a U1270 Series you can easily perform remote monitoring and data logging via Android devices or Windows®-based PC.
Promotions
For customers in Europe, click on the following link to view promotion to get a free U1177A Bluetooth adapter for wireless logging and data transfer: [LINK]
Based in the US or Canada? Click here instead to view related promotions from Agilent Technologies: [LINK]
Product Videos
This video is unavailable.
You don't have permission to edit metadata of this video.
This video is unavailable.
You don't have permission to edit metadata of this video.
Terms & Conditions
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
I guess this one is the latest one with bluetooth capability it will be awesome to make a app which can receive data on the fly and could be sent on server using this device.That will be great to see what else we can do with it.
I guess this one is the latest one with bluetooth capability it will be awesome to make a app which can receive data on the fly and could be sent on server using this device.That will be great to see what else we can do with it.
All the Agilent Handheld Multimeter have Bluetooth capability. It's just an attachment you clip on the IR-Port.....working pretty nice and I often use it with my smartphone.
With the free Apps (android) you can log the data and send it via email or so. Or you use the PC Software or write your own code. When the meter is in logging mode it is sending the logged values over the IR port as Data as well. So you can let it run in logging mode and just grab the data over the IR-Bluetooth connection.
My U1253B and U1272A do this and I guess the U1273AX will do it as well .
Top Comments
At work we handle bits straight out of the chamber down to -70 or so. If it was metal or a material that conducts heat quickly, you'd be right. But as it's plastic, -40 isn't too bad at all and doesn't…
Yes, well, but it is an modified U1273A.
All the Agilent Handheld Multimeter have Bluetooth capability. It's just an attachment you clip on the IR-Port.....working pretty nice and I often use it with my…
-
Former Member
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
Former Member
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children