Arduino Due

View table of contents ...  

image
Summary
The Arduino Due is a microcontroller board based on the Atmel SAM3X8E ARM Cortex-M3 CPU (datasheet). It is the first Arduino board based on a 32-bit ARM core microcontroller. It has 54 digital input/output pins (of which 12 can be used as PWM outputs), 12 analog inputs, 4 UARTs (hardware serial ports), a 84 MHz clock, an USB OTG capable connection, 2 DAC (digital to analog), 2 TWI, a power jack, an SPI header, a JTAG header, a reset button and an erase button.
The board contains everything needed to support the microcontroller; simply connect it to a computer with a micro-USB cable or power it with a AC-to-DC adapter or battery to get started. The Due is compatible with all Arduino shields that work at 3.3V and are compliant with the 1.0 Arduino pinout. The Due follows the 1.0 pinout:
  • TWI: SDA and SCL pins that are near to the AREF pin.
  • The IOREF pin which allows an attached shield with the proper configuration to adapt to the voltage provided by the board. This enables shield compatibility with a 3.3V board like the Due and AVR-based boards which operate at 5V.
  • An unconnected pin, reserved for future use.
The specified item was not found.
Features
MicrocontrollerAT91SAM3X8E
Operating Voltage3.3V
Input Voltage (recommended)7-12V
Input Voltage (limits)6-20V
Digital I/O Pins54 (of which 12 provide PWM output)
Analog Input Pins12
Analog Outputs Pins2 (DAC)
Total DC Output Current on all I/O lines130 mA
DC Current for 3.3V Pin800 mA
DC Current for 5V Pin800 mA
Flash Memory512 KB all available for the user applications
SRAM96 KB (two banks: 64KB and 32KB)
Clock Speed84 MHz
Terms & Conditions
  • Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
  • Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
  • Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.

image

RoadTest Reviews
Comment List
Anonymous
Parents
  • Okay, who's smart idea was it to hold a contest that involved spamming a forum with non-content?  It would be interesting to see just how many people have un-subscribed from receiving this forum as emails.  I certainly have!  This is rediculous.  Way to go Element14!  (There goes my chances of ever being picked as a road tester now...)

Comment
  • Okay, who's smart idea was it to hold a contest that involved spamming a forum with non-content?  It would be interesting to see just how many people have un-subscribed from receiving this forum as emails.  I certainly have!  This is rediculous.  Way to go Element14!  (There goes my chances of ever being picked as a road tester now...)

Children