Enrollment closes in
Days 0 Hours 0 Mins 0 Secs 0
| Microcontroller | AT91SAM3X8E |
| Operating Voltage | 3.3V |
| Input Voltage (recommended) | 7-12V |
| Input Voltage (limits) | 6-20V |
| Digital I/O Pins | 54 (of which 12 provide PWM output) |
| Analog Input Pins | 12 |
| Analog Outputs Pins | 2 (DAC) |
| Total DC Output Current on all I/O lines | 130 mA |
| DC Current for 3.3V Pin | 800 mA |
| DC Current for 5V Pin | 800 mA |
| Flash Memory | 512 KB all available for the user applications |
| SRAM | 96 KB (two banks: 64KB and 32KB) |
| Clock Speed | 84 MHz |
Top Comments
Andy -
Most of the time, the units are shipped promptly after selection (selection usually takes 2 weeks); I am aware of the issue to which you refer, but please keep in mind this is atypical, which is…
Marc,
You should have no problem. The programming is easy to follow. The Arduino site (arduino.cc) has more references than you can stand and examples programs are everywhere.. And because you are already…
thank you
-
awneil
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
-
doctorcdf
in reply to awneil
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
-
awneil
in reply to doctorcdf
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
awneil
in reply to doctorcdf
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children