The Model 2110 5½-Digit Dual-Display Digital Multimeter combines a compelling price with a comprehensive set of capabilities, superior measurement accuracy, and high speed for a broad range of applications. It features 15 measurement functions and 7 math functions and has dual-line display capability, which allows it to display two different measurements concurrently. The Model 2110 is an unbeatable value for production, R&D, and test engineers, scientists, and students making a wide variety of measurements in portable, bench, and system applications.
High Accuracy, Abundant Capabilities, Low Cost
The Model 2110 provides precision and a rich set of capabilities at a value price. It has 0.012% one-year basic DC voltage accuracy and 0.020% one-year basic resistance accuracy up to the 100kW range.
The Model 2110 provides a wide number of measurement ranges and functions:
DC voltage: 0.1V, 1V, 10V, 100V, and 1000V
AC voltage: 0.1V, 1V, 10V, 100V, and 750V
DC current: 10mA, 100mA, 1A, 3A, and 10A
AC current: 1A, 3A, and 10A
Two- and four-wire resistance: 100W, 1kW, 10kW, 100kW, 1MW, 10MW, and 100MW
Programmable A-D converter and filter settings for signal to noise optimization. Additionally, seven mathematical operations can be performed on measurement readings: percentage, average, min/max, NULL, limits, mX+b, dB, and dBm testing.
Speed
At 5½ digits, the Model 2110 delivers up to 200 readings/s via the USB remote interface. At the fast 4½-digit setting, it reads up to 50,000 readings/s and up to 30,000 readings/s into the buffer, making it ideal for production and monitoring applications in which speed is critical.
Video
You don't have permission to edit metadata of this video.
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
I received the meter the other day. I have commitments over the next couple of weeks but will post shortly after that. I hope to make the review will be of use to the community - If anyone wish to know anything specific I will be happy to oblige if I can.
There is some time limit set from when road test is "in review" to when it is "past". Nothing to worry about. Only minor nuisance is that "review" link is not shown for the item you want to post review. Workaround is to click on some other item's "review" link and then select from dropdown your specific item.
I would love to hear your opinion whether Keithley (and OEM) should have used the entire screen area for display and avoid having that black bezel arround the LCD?
Hi Nermin, thanks for the response. I will be doing the review next weekend I hope. I will go into detail on the display, its an important part of a bench DMM. Gerry
Top Comments
This multimeter is beautiful!
I will be very envious of the lucky people chosen to review this fine piece of hardware!
Good morning -
After careful consideration, we have picked the following applicants for this RoadTest -
Please note, I will be administering the RoadTest programme until…
-
doctorcdf
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
-
Former Member
in reply to doctorcdf
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
-
Former Member
in reply to Former Member
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
Former Member
in reply to Former Member
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children