Introduction to the Agilent 34461A Digital Multimeter, 6½ Digit Truevolt DMM
Easily set up and see your results and get actionable information faster
See your results clearly on a bright, 4.3-inch (109 mm), high-resolution, color graphical display. Get answers faster using the intuitive, menu-driven interface. If you have questions about a key or functionality, press and hold the key to display built-in help on the subject.
Customize display operation to meet your needs. Configure your preferences and pull them up automatically at the next instrument start-up.
Add customized labels to describe the instrument’s measurement your way.
Get quick insight with graphical views of your measurement results: View readings, long-term trends and measurement histograms for a statistical view.
Save and document your DMM’s data to your PC or mobile device using your preferred I/O:
Control, capture and view your DMM’s data on your PC with a single click using the Digital Multimeter Connectivity Utility via USB, GPIB, LAN, or RS-232 (for older generation Agilent DMMs).
Easily access the fi les on your DMM using drag-and-drop to transfer fi les via USB – no software required.
Choose the I/O that works best for you: USB, LAN/LXI Core (optional on 34460A), GPIB (optional on 34460A & 34461A).
Easily access the front-panel USB memory connector.
Blogging Challenge
Successful RoadTesters will be invited to blog on the Test & Measurement area in addition to providing the standard RoadTest review of the product; the blogs should fully describe use of the product in practical scenarios. Blogs should incorporate videos and images whenever possible. The winner will be announced on Monday, October 28, 2013 and a Grand Prize of a bundle of Truevolt Measurement Tools will be awarded shortly thereafter.
You don't have permission to edit metadata of this video.
Terms & Conditions
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product and your approach for blogging about it.
Testers are required to produce a full, comprehensive and well thought out review, we also expect a minimum of 3 blog posts about this product in the Test & Measurement area of element14. Both are due by October 25, 2013.
Failure to provide the review and blogs within the above timescale will result in the enrollee being excluded from future Road Tests.
Thank you Christian, that does help. Its good to know that those chosen can actually use the stuff they get and wont just "pass" it on once the review is done especially when you guys give away such awesome and useful gear.
how do you know you don't throw the baby with the bathwater?
I'm asking this because again, as with most of the previous road tests, people very new to, and with little activity (level 0 and 1) on element14 are selected for this roadtest, while people who are active for years are repeatedly ignored.
I wonder how seriously I should take this whole roadtest thing.
how do you know you don't throw the baby with the bathwater?
I'm asking this because again, as with most of the previous road tests, people very new to, and with little activity (level 0 and 1) on element14 are selected for this roadtest, while people who are active for years are repeatedly ignored.
I wonder how seriously I should take this whole roadtest thing.
There are two criteria I look at when I see applications -
1. The quality of the application itself. For this particular one, I had to favour applicants who had shown - in detail - what they planned to do, in particular in relation to the three blog posts that were going to be required in addition to the review. Some applicants went so far as to prepare a separate document as a proposal for this roadtest. This is by no means unusual when a high value product is on offer.
2. Was this person in a RoadTest before, and did they provide a review? Under normal circumstances if they haven't provided a review, I'm unlikely to trust them again.
I understand your point about people who continually participate, but we have to be strictly fair in how we judge applications. The rule is fairly simple: the best quality applications will be the ones we are likely to select.
@Gerrit I can underestand your frustration, I recently was awarded a review and I am not a long standing member and have certainly not had as much participation as many others. I think the fact that element14 are going to the trouble of running the RoadTest program is a really good thing though, they are afterall encouraging manufacturers to make these kits available and that is to be commended. I wish I could have reviewed this meter, I have a lot of Agilent kit myself and I like it so the RoadTest was attractive and I applied too but I don't feel like I am missing out, at the ent of the day it is a competition and of the quality of the application is the judging criteria then thats fair enough, I think Cristian is being quite open which is good thing and long may it continue. The point you might be making though, is the quality of the application alone might not feel like a fair criteria, other things like quality of review (baded on past reviews), contribution to the element14 community etc which is also reasonable. I think on balance the community are better off with the RoadTest program than without it. Just my 10 cents...
Top Comments
Gerrit -
There are two criteria I look at when I see applications -
1. The quality of the application itself. For this particular one, I had to favour applicants who had shown - in detail - what they planned…