The drive to enhance motion control in a wide range of commercial and industrial applications has seen a number of recent motor developments. Whether that is sensorless, brushless DC motors (BLDC) or permanent magnet synchronous motors (PMSM) with Field Oriented Control (FOC), these development offer significant energy efficiency improvements, lower acoustic noise and better reliability. However they are more difficult to control and often require more time and effort to tune and calibrate. A situation further exaggerated by the greater variations inherent in low-cost motors.
To help simplify the task and make it easy to tune and calibrate different motors, NXP has developed a dedicated hardware and firmware motor control solution. Using an ARM Cortex-M3 core, the LPC1500 includes an extensive set of motor control peripherals (dual ADCs, QEI, SCTimer / PWMs and comparators) that provide exceptional flexibility in a low-cost, low-power format. This microcontroller is supported by dedicated PMSM / BLDC Field Oriented Control (FOC) software, which includes a fast control algorithm and provides tunable performance for both speed and torque control.
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
I just posted my first entry in my blog for the LPC1500 road test but this is the first time for me and I am not sure whether the blog is visible or not to people who have added me as a contact (I assume they are interested in the upcoming review on the LPC1500). Can anyone reply and say whether it is or isn't to them? I have noticed I don't get copies of alerts referring to post made by myself so I assume the same for the blogs I make too. Or is this wrong?
Anyone who knows for a fact what really happens?
My previous reviews had no blog entries. Hence the ignorance.
I just posted my first entry in my blog for the LPC1500 road test but this is the first time for me and I am not sure whether the blog is visible or not to people who have added me as a contact (I assume they are interested in the upcoming review on the LPC1500). Can anyone reply and say whether it is or isn't to them? I have noticed I don't get copies of alerts referring to post made by myself so I assume the same for the blogs I make too. Or is this wrong?
Anyone who knows for a fact what really happens?
My previous reviews had no blog entries. Hence the ignorance.