The FRDM-K64FFRDM-K64F is an ultra-low-cost development platform for Kinetis K64, K63, and K24 MCUs. The FRDM-K64FFRDM-K64F hardware is form-factor compatible with the Arduino™ R3 pin layout, providing a broad range of expansion board options. The FRDM-K64FFRDM-K64F is feature packed with a lot of peripherals to enable rapid prototyping, including a 6-axis digital accelerometer and magnetometer to create full eCompass capabilities, a tri-colored LED and 2 user push-buttons for direct interaction and feedback, expansion memory with a microSD card slot, and connectivity options using onboard Ethernet port and headers for use with Bluetooth and 2.4 GHz radio add-on modules. The FRDM-K64FFRDM-K64F platform features OpenSDAv2, the Freescale open source hardware embedded serial and debug adapter running an open source bootloader. This circuit offers several options for serial communication, flash programming, and run-control debugging.
Dual role USB interface with micro-B USB connector
RGB LED
FXOS8700CQ accelerometer and magnetometer
Two user push buttons
Flexible power supply option – OpenSDAv2 USB, Kinetis K64 USB, and external source
Easy access to MCU input/output through Arduino™ R3 compatible I/O connectors
Programmable OpenSDAv2 debug circuit supporting the CMSIS-DAP Interface software that provides:
Mass storage device (MSD) flash programming interface
CMSIS-DAP debug interface over a driver-less USB HID connection providing run-control debugging and compatibility with IDE tools
Virtual serial port interface
Open source CMSIS-DAP software project
Ethernet
SDHC
Add-on RF module: nRF24L01+ Nordic 2.4GHz Radio
Add-on Bluetooth module: JY-MCU BT board V1.05 BT
Product Video
This video is unavailable.
You don't have permission to edit metadata of this video.
Terms & Conditions
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future RoadTests.
I have a question Is it possible to upload/update content if I submit my roadtest review? Is it like, I have to write all the review at once or I can keep on updating my review untill the end date?
Woah, that was quick. Thanks for clearing that up Yes, I was quiet busy with my projects and I just had enough time to keep track of few things happening here in this community(as you know, once you get in here you just can't go far from this world, isn't it? ) I am still worried about my roatest review, I need to complete it asap and many things are still pending till date. What about you? I guess you already have operated that kit succesfully with all your tools, drill machines, lasers beams, hammers, acids etc. etc.
Woah, that was quick. Thanks for clearing that up Yes, I was quiet busy with my projects and I just had enough time to keep track of few things happening here in this community(as you know, once you get in here you just can't go far from this world, isn't it? ) I am still worried about my roatest review, I need to complete it asap and many things are still pending till date. What about you? I guess you already have operated that kit succesfully with all your tools, drill machines, lasers beams, hammers, acids etc. etc.
Top Comments
I already have this board , Thanks to Freescale for sending one around, so if anyone has some trouble please feel free to contact
Thank you to everyone for your patience, there has been a severe shortage of FRDM-K64F's due to high demand. In order to ameliorate the issue, we have been talking to IBM and ARM who have produced…
Those of you who received the ARM / IBM kit may find this interesting -
BBC News - Internet of things starter kit unveiled by ARM and IBM