Gizmo 2

Table of contents

imageGIZMO 2GIZMO 2 is the second generation open source x86 development board presented by GizmoSphere. Gizmo 2 provides the power of a high performance computer and the I/O capabilities of a microcontroller through the use of an AMD Embedded G-Series System-on-Chip (SOC). The board includes the AMD GX-210HA dual-core processor, combined on a single die with AMD Radeon HD 8210E discrete-class graphics, providing 85 GFLOPS performance while drawing only 9 watts TDP.
Gizmo 2 is among the highest performing Open Source x86 development boards available, providing a wealth of leading features and capabilities including an HDMI dedicated port, an mSATA port for connecting SSDs and a microSD card slot.
Key Applications: Gizmo 2 can be used in do-it-yourself (DIY) designs, embedded development, PC replacement, microcontroller applications, parallel processing, multi-core engineering, industrial control and automation, digital signage, electronic gaming systems, SMB storage, IP-TV, medical and network appliances, set-top boxes and more. Any type of application that would require high processing power, high graphics performance, and the ability to control external objects (relays, motors, lights, etc) as well as take inputs from many types of sources (sensors, keyboard, Internet)
Key Features
  • AMD G-Series SOC
  • 1GB DDR3-1600 SDRAM
  • HDMI Video/Audio Output
  • 85 GFLOPS performance
  • HD Audio In/Out
  • mSATA/mini PCIe Connector
  • microSD Card Slot
  • Onboard Gigabit Ethernet
  • USB 3(2) and 2(2) Connectors
  • AMD Debug Header
  • High-speed and Low-speed Special Features Card Edge Connectors
  • 4" x 4" Form Factor
  • Support for DirectX® 11.1, OpenGL 4.2x and OpenCL™ 1.2, enabling parallel processing and high-performance graphics processing
  • Supported operating systems include Windows Embedded 8 and Linux
Product Video
Terms & Conditions
  • Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
  • Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
  • Failure to provide this review within the above timescale will result in the enrolee being excluded from future RoadTests.
Comment List
Anonymous
Parents
  • Former Member
    Former Member

    Yay!!!

     

    I'm so looking forward to using the Gizmo2 for a retro games console project; Along the way, there'll be regular blog posts detailing how the project is progressing and hopefully will be complete by the time the review is due.

     

    The blog's and additional content should be linked to from here in due course and also in the final review which will be created once I've had chance to fully evaluate the Gizmo2 and everything it has to offer.

     

    It's great to have the opportunity to work with the latest generation of small board computers utilising modern system on chip technologies (which I am sure will be the direction that present and future computing will progress) and thank Element14, Christian ( ), Gizmosphere and everyone involved in the selection process.

     

    Lucie

Comment
  • Former Member
    Former Member

    Yay!!!

     

    I'm so looking forward to using the Gizmo2 for a retro games console project; Along the way, there'll be regular blog posts detailing how the project is progressing and hopefully will be complete by the time the review is due.

     

    The blog's and additional content should be linked to from here in due course and also in the final review which will be created once I've had chance to fully evaluate the Gizmo2 and everything it has to offer.

     

    It's great to have the opportunity to work with the latest generation of small board computers utilising modern system on chip technologies (which I am sure will be the direction that present and future computing will progress) and thank Element14, Christian ( ), Gizmosphere and everyone involved in the selection process.

     

    Lucie

Children