Silicon Labs' EFM32ZG-STK3200EFM32ZG-STK3200 provides an excellent tool to get familiar with the EFM32™ Zero Gecko 32-bit microcontrollers (MCUs), the industry’s most energy-friendly MCU based on the ARM® Cortex®-M0+ processor.
Supported by Simplicity Studio, the starter kit contains sensors and peripherals demonstrating some of the MCU's many capabilities and can serve as a starting point for application development. The EFM32ZG-STK3200EFM32ZG-STK3200 features an on-board SEGGER J-Link debugger and an Advanced Energy Monitoring system, allowing you to program, debug and perform real-time current profiling of your application without using external tools.
Features
EFM32ZG222F32 Zero Gecko MCU
Advanced Energy Monitoring v2
Real-time energy and power profiling
Backup Capacitor for RTC mode
USB interface for Host/Device/OTG
LESENSE demo ready
Light, LC and touch sensors
SEGGER J-Link debugger
Free evaluation compiler versions
Supported by Simplicity Studio
Sensor Expansion Card for EFM32™ Zero Gecko Starter Kit
The SENSOR-EXP-EVB card provides a convenient development platform for Silicon Labs’ Si701x/2x Relative Humidity and Temperature Sensors and Si114x UV Index, Ambient Light, Proximity and 3D Gesture Sensors.. The card plugs directly into the expansion header of the EFM32™ Zero Gecko Starter Kit and is fully supported in Simplicity Studio for fast prototyping and development. Example software and source code is available in Simplicity Studio for a standalone weather station application using the SENSOR-EXP-EVB.
Webinar
You don't have permission to edit metadata of this video.
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test these particular products.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the products.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future RoadTests.
The EFM32 Sensor Kits are presently being held by Indian customs; the Bangalore team is negotiating with them in order to get the units released. This is what we believe happened to the previous units that were sent.
You have to apply for a Road test. If you get selected based on the quality of the application. E14 will send the Kit free to you. In return you have to Review the product sent as well as describe how u used the product in your project. There may be some more requirement like, writing blogs etc.
Top Comments
I got board two weeks back. I hope everybody would have received that. Started working on project....!!!!!
I haven't received one of the items yet for Wireless charging Beyond the Phone challenge.
one can follow up with order no.Phone: 1800 3000 3888
Fax: +91 (0) 80 4000 3880
Email: in-sales@element14.co…
That's really sad. .Isn't the challenge over ?? and as we dont get an Order ID/No. how can we follow up the order this may be really helpful .