Enrollment closes in
Days 0 Hours 0 Mins 0 Secs 0
Silicon Labs' EFM32ZG-STK3200EFM32ZG-STK3200 provides an excellent tool to get familiar with the EFM32™ Zero Gecko 32-bit microcontrollers (MCUs), the industry’s most energy-friendly MCU based on the ARM® Cortex®-M0+ processor.
The SENSOR-EXP-EVB card provides a convenient development platform for Silicon Labs’ Si701x/2x Relative Humidity and Temperature Sensors and Si114x UV Index, Ambient Light, Proximity and 3D Gesture Sensors.. The card plugs directly into the expansion header of the EFM32™ Zero Gecko Starter Kit and is fully supported in Simplicity Studio for fast prototyping and development. Example software and source code is available in Simplicity Studio for a standalone weather station application using the SENSOR-EXP-EVB.
Top Comments
I got board two weeks back. I hope everybody would have received that. Started working on project....!!!!!
I haven't received one of the items yet for Wireless charging Beyond the Phone challenge.
one can follow up with order no.Phone: 1800 3000 3888
Fax: +91 (0) 80 4000 3880
Email: in-sales@element14.co…
That's really sad.
.Isn't the challenge over ?? and as we dont get an Order ID/No. how can we follow up the order this may be really helpful
.
-
ss_shrenik
-
Cancel
-
Up
+2
Down
-
-
Reply
-
More
-
Cancel
Comment-
ss_shrenik
-
Cancel
-
Up
+2
Down
-
-
Reply
-
More
-
Cancel
Children