RoadTest the ADS7042 BoosterPack and MSP430FR4133

Table of contents

    What? nanoWatt?: Acquiring Sensor Data with nanoWatts of Power Consumption

 

 

{tabbedtable} Tab LabelTab Content
About this RoadTest

The ADS7042 Ultra-Low Power Data Acquisition BoosterPack is a stand-alone system that converts analog sensor data into digital SPI data using the TI ADS7042 Successive Approximation Register Analog-to-Digital Converter.  This BoosterPack has been designed to be compatible with the TI LaunchPad™ ecosystem to enable a complete data acquisition system from analog sensor input via either the on-board ambient light sensor or the SMA input jack to digital data output over UART via the USB port on the LaunchPad.

 

  • Designed using the ADS7042 precision analog-to-digital converter, OPA316 precision ADC driver, and REF3330 precision voltage reference
  • Nanowatt power consumption of the ADS7042 ADC when sampling at 1 KSPS
  • ADC sampling rates betwen 1 KSPS and 1 MSPS
  • SMA jack for optional external analog signal input
  • User-programmable push button and LEDs
  • On-board ambient light sensor

image

The MSP-EXP430FR4133MSP-EXP430FR4133 LaunchPad development kit is an easy to use evaluation kit for the MSP430FR4133 microcontroller. The MSP430FR4133 is a 16bit microcontroller with 16KB FRAM, 16bit RISC architecture, 8MHz FRAM access and 16MHz system clock speed. The kit contains everything needed to start developing on the MSP430 ultra low power (ULP) FRAM based microcontroller platform, including onboard emulation for programming, debugging and energy measurements. The board features onboard buttons and LEDs for quick integration of a simple user interface as well as a liquid crystal display (LCD) display which showcases the integrated driver with flexible software configurable pins. Free software development tools are also available, including TI's Eclipse based Code Composer Studio (CCSTUDIO) and IAR Embedded Workbench IAR-KICKSTART. Both of these integrated development environments (IDEs) support EnergyTrace technology when paired with the MSP430FR4133 LaunchPad.

  • EnergyTrace technology available for ultra low power debugging
  • 20 pin BoosterPack plug-in module headers
  • Onboard eZ-FET emulation
  • Backchannel UART through USB to PC

The MSP-EXP430FR4133 LaunchPad supports EnergyTrace technology but does not have support for EnergyTrace++ technology.

image

RoadTesters

Thank you for all that have applied. We have selected the following RoadTesters:

alricliew

Terms and Conditions

Texas Instruments ADS7042 BoosterPack and MSP430FR4133

 

These are the terms and conditions which govern the The Texas Instruments TI ADS7042 BoosterPack and MSP430FR4133 RoadTest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials.. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

1. 1 The Principal terms of the Contest:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

RoadTest: TI ADS7042 BoosterPack and MSP430FR4133 RoadTest (or the Contest)

Key dates:

Applications Close: midnight (GMT) on 30 September 2016

Judging Close: 11:59PM (GMT) on 14 September  2016

Announcement of Winner(s) (estimated):  14 September 2016

RoadTest Item(s): TI ADS7042 BoosterPack and MSP430FR4133

 

RoadTest Site: www.element14.com/community/roadTests/XXXX

Site or element14 Community: www.element14.com

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria: All of the following which will have equal weighting:

1.1 • Demonstrated competence with the technologies including links or descriptions of past projects

1.2 • Qualifications as indicated by current job role and/or schooling/vocational training;

1.3 • A thorough description of how the prize would be tested

1.4 • Likelihood that the Applicant will blog about the prize and provide a review on element14.com

1.5 • Originality;

1.6 • Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

1.7 • Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Minimum number of Prizes: 5

Terms: these terms and conditions which govern the Contest and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

1. 2 Eligibility

2. 3 Applications:

3. 4 Selecting Winners:

4. 5 Liability:

5. 6 General:

1.8 2.1 Save as set out in these Terms, the RoadTest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.9 2.2 All Applicants must be aged at least 18 at the time of their application.

1.10 2.3 Applicants must not enter the Contest if doing so or taking part may:

1.10.1 2.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.10.2 2.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.10.3 2.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in contests such as these or receiving prizes under them and the Organiser respects those policies and practices.

1.10.4 The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.11 2.4 Multiple applications are not permitted.

1.12 2.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.13 2.6 The Contest is NOT open to:

1.13.1 2.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.13.2 2.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser.

1.14 3.1 Each Applicant must fully complete and submit a response by the Application Close.

1.15 3.2 By submitting a response, each Applicant:

1.15.1 3.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

1.15.2 3.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

1.15.3 3.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

1.15.4 3.2.4 Authorises the Organiser to copy, reproduce and use the application or subsequent Blogs submitted for the purposes of the Contest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

1.15.5 3.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

1.15.6 3.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

1.15.7 3.2.7 Agrees to participate positively in all publicity surrounding the Contest;

1.15.8 3.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

1.15.9 3.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

1.15.10 3.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the Contest.

1.16 3.3 All applications submitted to this Contest must meet the following criteria:

1.16.1 3.3.1 Applications must not include or propose any of the following, the inclusion of which shall render any application null and void:

(a) (a) Applications or designs which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) (b) Applications or designs that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser and/or the Judges;

(c) (c) Applications or applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

1.17 3.4 No proposed Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

1.18 3.5 A proposed Application must not have been entered into any other Contest, unless that Contest has closed and the Application did not win a prize.

1.19 4.1 Winners will be selected by the Organiser on the basis of the quality of his or her Application and its adherence to these Terms.

1.20 4.2 The total number of Winners selected will be at least the minimum number set out in condition 1 above but the actual number is at the sole discretion of the Organizer.

1.21 4.3 The Organiser will use all reasonable efforts to announce the Participants within 10 business days the Applications Close.

1.22 4.4 The winner(s) will be selected by the Organiser in their absolute discretion based on the Judging Criteria. Winners must meet all eligibility requirements of these Terms. There shall be such number of winners as the Organiser shall determine.

1.23 4.5 The Organiser’s decision is final and without right of appeal. No correspondence will be entered into. The Organiser reserves the right not to select a winner if, in their sole discretion, they do not consider any of the applications to merit the Prize.

1.24 4.6 The Organiser will use all reasonable efforts to complete judging by Judging and Voting Close and to notify the winner(s) via a blog posted on the Contest Site by the Announcement of Winner Date.

1.25 4.7 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

1.26 4.8 Details of the Winners will also be published in the media.

1.27 5.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

1.28 5.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

1.29 5.3 Subject to 10.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Contest or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Contest, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

1.30 6.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

1.31 6.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a Contest of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

1.32 6.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

1.33 6.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the RoadTest Site and it is a condition of entry to the RoadTest that Applicants and Winners agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

1.34 6.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

1.35 6.6 These Terms and the operation of the RoadTest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

1.36 the exclusive jurisdiction of the English courts.

Comment List
Anonymous
Parents
  • alricliew

     

    Texas Instruments contacted me today. They would like to see your RoadTest Review. So, please post your review asap or give me a status on your progress. If you choose not to write the review, please message me at Thanks.

     

    Randall Scasny

    RoadTest Program Manager

  • Hello Randall

    First I want to apologize for the delayed response.

    I received the board in December.
    I had a lot of troubles with the board, I keep getting errors when installing the drivers (I even stopped the Antivirus scanner and it still does not work).

    I tried to install manually the drivers (not ok)
    I tried to install with CSS. Still not ok
    The computer has preset some drivers for the board instead of COM it set to HID (because of this I think I can't upload from energia IDE)

     

    I have most of the parts set up and the plan ready, I can't get the board to start. Because the project is important for me, I continued to experiment with Arduino, due to the lack of time. Now that I saw how urgent everything became, I'm continuing to work with the board (still the same problems)

    I did not give up, will only take a longer time to receive my review if it is ok.
    If anyone has any helpful information, please feel free to contact me.
    Thank you for your time and understanding

  • Hi Mihai,

     

    I personally think that documenting your trouble getting the part to work is valuable information for your review.
    This can draw the attention of the vendor in finding a solution for easier installation or better compatibility.

     

    Reviews don't have to be about all the good things. If the board doesn't work, that's also (part of) a review.

  • I agree with FV. Why not create a review with all that you've done so far - your plan for the review (it sounds like you have a project of some sort, which would be interesting to read about), pictures of the board, screenshots of the IDE installation and the error messages, what you've done so far to sort the problem, and finish with asking for help in the comments?  That way you'll keep Randall and TI happy for now and it will be useful because it will help people who may face the same problems as you've had. Then later you can extend it, when you get some help and as you continue the project.

     

    We've already had one really excellent project with this kit from . I'd like to see what you are doing with it come to fruition too and add to that - there are enough people here with experience of the TI boards that they should be able to get you on track again.

Comment
  • I agree with FV. Why not create a review with all that you've done so far - your plan for the review (it sounds like you have a project of some sort, which would be interesting to read about), pictures of the board, screenshots of the IDE installation and the error messages, what you've done so far to sort the problem, and finish with asking for help in the comments?  That way you'll keep Randall and TI happy for now and it will be useful because it will help people who may face the same problems as you've had. Then later you can extend it, when you get some help and as you continue the project.

     

    We've already had one really excellent project with this kit from . I'd like to see what you are doing with it come to fruition too and add to that - there are enough people here with experience of the TI boards that they should be able to get you on track again.

Children
No Data