The U1620A is the world’s first handheld scope with a VGA display. This 200 MHz handheld scope offers a floating measurement capability with two CAT III 600 V isolated channels. With a 2 Mpts memory depth, it captures more waveforms from signals such as pulse width modulated circuit, in rush, transient, and motor start up sequences. Its benchtop-like display and dual window zoom function allow you to easily identify problem areas and zooming for more detailed analysis. Now, you can view signals in detail and detect glitches easily.
Q&A
What we would like to see in a person doing the Road Test?
Maximizing the combination of the high sampling rate, deep memory and dual zoom to see more and do more. Feel the difference of using the 3 viewing modes in an indoor, dark or in bright sunlight environments.
Are there certain application areas we would like folks working on?
Any application in the industrial or electronics segment.
thanks for that informations, so I´ve read through the text and can say if the package isn´t send untill now there is a chance to get it free of all tax and charges when the DSO get´s an unremovable sign which mark´s it as sample (like an element 14 logo and the word sample which could be get onto the case with some hot iron)
I am not sure if that is sufficient. They are generally speaking about low value products which is not applicable for the Scopemeter I guess .
Beginning next week (Mon. or Tuesday) I will have to go to our customs office for an export clearing and I can ask them what to expect and what would be applicable. Then we could at least give advice and a fixed state for further shippings to Germany.
As I said I am not sure if marking it as sample is enough. Well, I wouldn't mind a mark (as most people won't mind it) as long as the product still works fine. A friend has tested an U1272 which had a sticker "sample" on it, but I am not sure how customs handled it in his case......he is living in Greece anyway. So that is another story.
I am not sure if that is sufficient. They are generally speaking about low value products which is not applicable for the Scopemeter I guess .
Beginning next week (Mon. or Tuesday) I will have to go to our customs office for an export clearing and I can ask them what to expect and what would be applicable. Then we could at least give advice and a fixed state for further shippings to Germany.
As I said I am not sure if marking it as sample is enough. Well, I wouldn't mind a mark (as most people won't mind it) as long as the product still works fine. A friend has tested an U1272 which had a sticker "sample" on it, but I am not sure how customs handled it in his case......he is living in Greece anyway. So that is another story.
Top Comments
Indeed, it is very impressive.
But there is something that they have forgotten : They should give away about 1000 kits. Otherwise, there will be so much people to be sad
Firat
Quick comparison of the key features
Please click to open document...
Very impressive spec sheet. The uses for a small scope with the measurement capability of this unit would be a welcome addition to anyone's workbench.
I think Agilent has a winner here.
DAB