Raspberry Pi Zero 2W

Table of contents

Eligibility

You must be a member of the element14 community to apply for this roadtest. To register go here. Click the green Register button in the upper right corner of your browser.

What the official Roadtesters will receive:

Raspberry Pi Zero 2W SanDisk 32GB MicroSd Power Supply

About the Raspberry Pi 2W

Raspberry Pi Zero 2 W is the latest product in our most affordable range of single-board computers. The successor to the Raspberry Pi Zero W, Raspberry Pi Zero 2 W is a form factor–compatible drop-in replacement for the original board. The board incorporates a quad-core 64-bit Arm Cortex-A53 CPU, clocked at 1GHz. At its heart is a Raspberry Pi RP3A0 system-in-package (SiP), integrating a Broadcom BCM2710A1 die with 512MB of LPDDR2 SDRAM. The upgraded processor provides Raspberry Pi Zero 2 W with 40% more single-threaded performance, and five times more multi-threaded performance, than the original single-core Raspberry Pi Zero. Raspberry Pi Zero 2 W offers 2.4GHz 802.11 b/g/n wireless LAN and Bluetooth 4.2, along with support for Bluetooth Low Energy (BLE), and modular compliance certification. The board has a microSD card slot, a CSI-2 camera connector, a USB On-The-Go (OTG) port, and an unpopulated footprint for a HAT-compatible 40-pin GPIO header. It is powered via a micro USB socket. Video output is via a mini HDMI port; composite video output can easily be made available via test points if needed. Sharing the same form factor as the original Raspberry Pi Zero, Raspberry Pi Zero 2 W fits inside most existing Raspberry Pi Zero cases. 

Additional Information

Important Dates

Enrollment Begins Jan 9 2022
Enrollment Ends Feb 9 2022
Roadtesters Selected Feb 12 2022
Products Shipped  Feb 17 2022
Testing Begins Feb 22 2022
element14 Team Email Follow up Mar 22 2022
Post Reviews by  April 22 2022

Terms and Conditions

Click here for the Terms and conditions

Official Roadtesters

The following applicants have been selected as official roadtesters

Sean Conway

Dimiter Kendri

Chinmay Bohra

RoadTest Reviews
Comment List
Anonymous
Parents
  • I went through all the applications. Some were really complex ideas. And of course for some the applicant sent me pictures of a green square with a white vertical bar or a potted plat or a multimeter---not a test plan. 

    Of the 63 applicants, I selected 22 applicants with good applications.

    I have to bring that down to 3 in the next view, which will be hard to do because they all are good. I wish I had more than 3 kits to roadtest. 

    Randall Scasny

    RoadTest Program Manager

  • Till when will we receive the kits?

Comment Children
No Data