R&S® MXO 4 Oscilloscope

Table of contents

Community Comments about this Roadtest 
This oscilloscope plus options and accessories has a list price of about $20,000 (US). What makes this product standout out so much?? I'll let some element14 members explain:

  • "The MXO4 manages to combine ridiculous hardware speed, a very quiet front-end, and a very well thought-out user interface in a general-purpose form factor."
  • "It's an awesome scope indeed - some of those specs almost seem impossibly good to be true! I'm sure whoever gets to RoadTest this is going to be really happy about it."
  • "I got to try one out at the R&S Scopetoberfest at [a] local office last month. It had all the options enabled (1.5GHz, AWG, etc). Quite an impressive instrument with an awesome HD display. I'd love to roadtest this instrument."

To read more about what our members think, scroll down to the bottom of this page read the rest of the comments.

Testing Goals
Conduct a comprehensive set of performance tests in order to review its significant capabilities and features. The tests conducted should be of a highly technical nature that an experienced oscilloscope user would value.

Product Variants
There are several versions of this product. You can find them here.

Description
The MXO44-245 is a 4 channel R&S® MXO 4 series oscilloscope with a 13.3-inch high-definition (1,920 x 1,080) display. Many applications, such as embedded systems, three-phase power electronics, automotive electronics, power supply design, and DC-to-DC power converters, require the observation of more than four analogue signals to verify and characterize device performance, and to debug challenging system issues.

Overall, the R&S®MXO 4 series is the first of a new generation of oscilloscopes that excels in both performance and value. The instruments deliver accelerated insight and have a real-time update rate of 4.5 million waveforms/s, meaning engineers can see more infrequent events than with any other instrument. With its 12-bit ADC, the R&S®MXO 4 series has 16 times the resolution of traditional 8-bit oscilloscopes at all sample rates without any compromises for more precise measurements. With a standard acquisition memory of 400 Mpoints on all four channels and an optional 800 Mpts interleaved, the instrument has up to 100 times the standard memory of comparable instruments. R&S®MXO 4 series oscilloscopes sport an impressive 13.3" Full HD capacitive touchscreen and an intuitive user interface with a learning curve of less than 15 minutes. All R&S®MXO 4 series oscilloscopes have the R&S®MXO4-B1 MSO hardware built into every instrument. The MSO option offers the logic probes required to start using the 16 digital channels.

At the heart of each R&S®MXO 4 series oscilloscope is a Rohde&Schwarz-developed application specific integrated circuit (ASIC): MXO-EP (extreme performance). MXO-EP processes 200 Gbit/s to deliver the world’s fastest update rate of up to 4.5 million acquisitions/s. See and capture more of your signal, faster. Find rare signal anomalies quickly. Experience the most responsive oscilloscope in the industry.

MXO-EP ASICs incorporate advanced digital triggering that evaluates the A/D converter samples in the acquisition path in real time. Trigger on small events of less than 1/10000 vertical division that no other oscilloscope can isolate. Choose your own trigger hysteresis. Apply digital filters to suppress noise to get the most precise triggering available.

Measurement accuracy is highly dependent on the components in the signal path, e.g. amplifiers, samplers and A/D converters. The workhorse of the R&S®MXO 4 series is an extremely low noise signal path including a 12 bit ADC. High definition mode (HD) increases vertical resolution to industry best 18 bit architecture.

R&S®MXO 4 series oscilloscopes come equipped with the industry’s deepest standard acquisition memory of 400 Mpoints per channel. Capture up to 80 ms of power up or power down sequences with the highest sample resolution of 200 ps. The memory controller in the MXO-EP ASIC ensures the oscilloscope stays responsive with deep memory.


Features
• 500MHz bandwidth, 4 analogue channel, 16 digital channel
• 12bit ADC, 18bit vertical architecture
• Up to 5Gsample/s sample rate
• Standard memory of 400Mpoints per channel with option for 800Mpoints
• Minimal noise of 104µV at 1GHz with 1mV/div sensitivity
• ±5V offset range with 500µV/div sensitivity
• History and segmented memory to capture up to 1 million acquisitions
• Industry's most sensitive trigger: 1/1000 vertical division
• Best-in-class trigger jitter of just 1ps
• Adjustable digital trigger filters with user-selectable hysteresis
• World’s first oscilloscope with update rate exceeding
• 4.5 million waveforms per second
• Industry-best 18 bit architecture
• Fastest and most accurate spectrum analysis in its class
• Industry’s fastest trigger rearm time of 21 ns
• First in class to incorporate newer digital triggering technology
• Industry’s most sensitive trigger of 1/10 000 div
• First oscilloscope with dual-path protocol analysis
• First in class with R&S®SmartGrid user interface

Contents
• 500 MHZ 4-channel ®MXO 4 series oscilloscope (MXO44-245)
• MX04-B1 option: (two) RT-ZL04 400MHZ logic probes, 8-channel
• EU plug to C13 power cord
• (four) 700MHZ passive voltage probe RT-ZP11
• Safety instructions, manuals

Additional Information
Product Brief
Product Info
Flyer
Datasheet
User Manual
Getting Started Manual
Other Documentation
Downloads
Variants

Important Dates

Begin enrollment: Nov 4, 2022
End enrollment: Dec 9, 2022
Select roadtesters: Jan 18, 2023
Ship unit: Jan 19, 2023
Begin roadtesting:  Jan 26 2023
Element14 follow up: Feb 26 2023
Post reviews by: April 10 2023

Official Roadtesters

  • michaelkellett (review due date Apr 10 2023)
  • shabaz (review due date Apr 10 2023)

RoadTest Forum

Please use this forum post for any questions you may have about this RoadTest.

Terms and Conditions

Click Here to read the Terms and Conditions.

Taxes

  • If you are a U.S.-based roadtester the U.S.1099 rule applies to you and says for prizes that are valued at $660, you will be required to complete an W-9 form and the company will issue you a 1099 form, as income, at the end of the year.
  • If you are not a U.S.based roadtester, it would be up to the individual recipient to determine what the rules are for their country of residence. We cannot dictate or recommend what their tax requirements would be for their respective countries.
RoadTest Reviews
Comment List
Anonymous
Parents
  • Thanks very much to E14 for the opportunity to test this scope.

    I know there has been a lot of interest in this Road Test instrument and I shall do my best to put it through it's paces. If any members have some specific aspects of they would like me to look at I shall be happy to do so (subject to feasibility of course.)

    MK

Comment
  • Thanks very much to E14 for the opportunity to test this scope.

    I know there has been a lot of interest in this Road Test instrument and I shall do my best to put it through it's paces. If any members have some specific aspects of they would like me to look at I shall be happy to do so (subject to feasibility of course.)

    MK

Children
No Data