Enroll to Review the Arduino GIGA R1 WiFi + Camera

View table of contents ...  

RoadTest Goals

  • Working with the documentation, open the box and test the out of the box experience.
  • Show us what you discovered through text, images, videos, and/or any other media, so the reader understands what is involved in using the product.

Description

ABX00063 Arduino GIGA R1 WiFi brings the power of the STM32H7 to the Mega form factor, being the first Mega board to include onboard Wi-Fi® and Bluetooth® connectivity. The board provides 76 digital inputs/outputs (12 with PWM capability), 14 analog inputs and 2 analog outputs (DAC) all easily accessible via pin headers. The STM32 microprocessor with dual-core Cortex® M7 and Cortex® M4, together with onboard memory and audio jack enables you to perform machine learning and signal processing on the edge. Target areas are 3D printing, signal processing, maker and robotics. It features camera: 20 pin Arducam camera connector, display: D1N, D0N, D1P, D0P, CKN, CKP, D68-D75, audio jack: DAC0, DAC1, A7 and JTAG connector.

Features

  • STM32H747XIH6 dual core microcontroller, full set of DSP instructions, memory protection unit (MPU)
  • Murata 1DX Wi-Fi®/Bluetooth® module, Wi-Fi® 802.11b/g/n 65Mbps, micro UFL conn for external antenna
  • Bluetooth® low energy (version 5.X via Cordio stack, version 4.2 via Arduino Stack)
  • STM32H747XI (2MB flash, 1MB RAM), AT25SF128A-MHB-T (16MB NORflash, QSPI), AS4C4M16SA (8MB SDRAM)
  • Digital I/O pins: 76, analog input pins: 12, PWM pins: 12 analog output pins
  • USB peripheral: USB-C®, logic level: 3.3V, VRTC: to power the RTC while the board is off
  • 4x UART, 3x I2C, 2x SPI, 1x CAN (external transceiver required), (DAC0/DAC1): 2, USB host: USB 2.0 A
  • Secure element ATECC608A-MAHDA-T module
  • USB host USB 2.0 Type A (host), USB Peripheral USB-C® (programming port, HID)
  • Circuit operating voltage: 3.3V, input voltage (VIN): 6-24V, DC current per I/O pin: 8mA

OV7675 VGA Color 20-pin DVP Camera Module
The camera is based on OmniVision 0.3MP OV7675 image sensor, which excels in image capture with its advanced features and exceptional performance. Its pixel array captures intricate details with precision and clarity, while its low-light imaging capabilities reveal hidden elements in challenging lighting conditions.

The low consumption camera module is equipped with a 63.9°(DFOV) stock Lens. It supports RAW/RGB/YUV output format.
It is fully compatible with Arduino GIGA R1 board, a professional-grade microcontroller development board recently launched by Arduino. Seamlessly integrates with our camera module, unlocking versatile image capture and processing capabilities. Harness the power of Arduino GIGA R1 and gain a competitive edge in your projects.



Documentation

Contents

  • GIGA R1 board and micro UFL antenna
  • Camera

Important Dates

Begin enrollment:  June 15, 2023
End enrollment:  July 16, 2023
Select roadtesters:  July 17, 2023
Ship unit:  July 19 2023
Begin Roadtesting: July 24 2023
Element14 follow up: August 24 2023
Post Reviews by: September 24 2023

Terms and Conditions


RoadTest Reviews
Comment List
Anonymous
  • I put about a week in the schedule for selection. But that is only an estimate. If it is a roadtest where the sponsor wants to review our selections, the time for notification could be several weeks. If it is a roadtest where more time is needed to review all the applications, a delay could occur. Finally, any applicant considered as an official roadtest needs to be approved for shipment by our company's Trade & Compliance department. Generally, that take a day or so., Once an applicant is approved for shipment, he is notified. I should also say that if there is a delay in selection, the deadlines would be adjusted. The roadtest time is 60 days from the receipt of the product. 

  • Hello, a question .
    How long does it take for the selected candidates to be notified once the registration period closes and the selected ones are chosen?

    Thanks and best regards.

  • Looks like big bad brother of arduino due

  • What a beast of a microcontroller!

  • DroneBot Workshop has an excellent video on the board - 1h long.

  • The Arduino Portenta H7 also uses a STM32H747 chipset. So it will be interesting to see if this GIGA R1 board follows the same approach and will also be MbedOS based.

  • "has no official support for the board"

    It's still somewhat early days for this Arduino board, which is something to be wary of.

  • I love it. It has a wide range of inputs and the Arducam connection is a killer feature.

    The MicroPython support is also a great feature. More people will be using it because of that. I know I will.

    Although Edge Impulse has no official support for the board (yet), there's already one project using it . I will definitely enroll for a project with this board. 

  • This roadtest is open for enrollment