Raspberry Pi Compute Module 3 Development Kit

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The Raspberry Pi Compute Module 3 Development Kit consists of a main development kit IO board into which the Compute Module SODIMM board is connected. It also contains all of the necessary interface ports to allow an engineer to design and test their own prototype application. The modules simplify the design process engineers need to undertake when developing a System on Module (SoM) solution into their final product.

 

Engineers do not need to concern themselves with the complexities of interfacing with the BCM2837 processer directly and instead can concentrate on designing the interfaces to their own IO board and their application software . This simplicity fosters rapid development.

 

A Raspberry Pi Compute Module IO Board Camera Display Adapter is included in the kit to connect a standard Raspberry Pi camera board or Raspberry Pi display to the Compute Module IO Board. The IO board contains the following interfaces:

 

  • Multiple GPIO interfaces on 2 60 way 0.1” Headers
  • 1 x Micro USB connector type B – USB Slave
  • 1 x USB connector type A – USB Host
  • 2 x CSI ports for camera boards
  • 2 x DSI ports for display boards
  • Full size HDMI port
  • Micro USB power connector
  • Micro SD connector
  • SOFTWARE - ARMv7 Instruction Set, and a mature and stable Linux software stack

 

image

Important Dates

Enrollment Begins: June 4 2017

Enrollment Ends: July 14 2017

RoadTesters Selected:July 18 2017

Product Shipped: July 18 2017

RoadTesting Begins: July 25 2017

Reminder/Update Email: Sept 11 2017*

Submit Reviews By: Sept 25 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected as official RoadTesters:

 

Terms & Conditions

Raspberry Pi Compute Module 3 Development Kit – RoadTest

Terms and Conditions

These are the terms and conditions which govern the Raspberry Pi Compute Module 3 Development Kit RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Raspberry Pi Compute Module 3 Development Kit

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on July 14  2017

Announcement of Winner (estimated): July 21 2017

 

Prize:Raspberry Pi Compute Module 3 Development Kit
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
  • The RPi CM3 Dev Kit has performed exceptionally. It is beyond understanding why others had issues with this Road Test. The only real issue that was encountered with the CM3 was that the Raspbian Stretch with Desktop Image with a size of 4.57Gbyte is too large to fit onto the 4Gbyte eMMC Flash. This was not really a deal breaker as the 4Gbyte eMMC is sufficient for installation of the Raspbian Stretch Lite Image and any additional software required for the intended application.

     

    The CM3L has been running non-stop in the application of tracking Hurricanes for over a month now. I find this as a very positive sign of stability and dependable operation. The potential use for the CM3 and CM3L in an industrial environment is immense.

  • Hello!

     

    Despite the fact I had an issue but it is just some bad luck (a piece was broken in the connector and the CM3 is not responsive with the I2C protocol for an unknown cause), I perfectly agre with you. This is the reason that this board has been adopted for the PONF project as the core unit of an innovative device, open and exactly focused in the typical industrial application. IMHO blocking issues are excuses

     

    Enrico

  • Were you able to resolve the problem with I2C?

    The default I2C pins are located on the J5 Header. GPIO Pin #2 is SDA and GPIO Pin #3 is SCL.

    Connection can be verified with i2cdetect -y 1 or i2cdetect -y 0 dependant on wiring.

Comment Children
  • Hi, Ninatrent!

     

    All what you say has been obviously tested and more. Then I bought a second kit and the problems was totally in charge of the CM3 (not the CM3 light) kit. Inverted the boards, inverted the dev boards, tried with all the most recent Jessie and the last Strech versions of Raspbian but the problem is certified inside the Compute Module. Unpredictable event.

     

    Enrico

  • Hello Enrico,

     

    It was not with intention to imply any lack of experience or knowledge. My apologies if this was perceived.

    It is with hope that a solution might be found.

     

    Trent