Raspberry Pi Compute Module 3 Development Kit

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The Raspberry Pi Compute Module 3 Development Kit consists of a main development kit IO board into which the Compute Module SODIMM board is connected. It also contains all of the necessary interface ports to allow an engineer to design and test their own prototype application. The modules simplify the design process engineers need to undertake when developing a System on Module (SoM) solution into their final product.

 

Engineers do not need to concern themselves with the complexities of interfacing with the BCM2837 processer directly and instead can concentrate on designing the interfaces to their own IO board and their application software . This simplicity fosters rapid development.

 

A Raspberry Pi Compute Module IO Board Camera Display Adapter is included in the kit to connect a standard Raspberry Pi camera board or Raspberry Pi display to the Compute Module IO Board. The IO board contains the following interfaces:

 

  • Multiple GPIO interfaces on 2 60 way 0.1” Headers
  • 1 x Micro USB connector type B – USB Slave
  • 1 x USB connector type A – USB Host
  • 2 x CSI ports for camera boards
  • 2 x DSI ports for display boards
  • Full size HDMI port
  • Micro USB power connector
  • Micro SD connector
  • SOFTWARE - ARMv7 Instruction Set, and a mature and stable Linux software stack

 

image

Important Dates

Enrollment Begins: June 4 2017

Enrollment Ends: July 14 2017

RoadTesters Selected:July 18 2017

Product Shipped: July 18 2017

RoadTesting Begins: July 25 2017

Reminder/Update Email: Sept 11 2017*

Submit Reviews By: Sept 25 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected as official RoadTesters:

 

Terms & Conditions

Raspberry Pi Compute Module 3 Development Kit – RoadTest

Terms and Conditions

These are the terms and conditions which govern the Raspberry Pi Compute Module 3 Development Kit RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Raspberry Pi Compute Module 3 Development Kit

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on July 14  2017

Announcement of Winner (estimated): July 21 2017

 

Prize:Raspberry Pi Compute Module 3 Development Kit
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
  • Randall, this is a great opportunity image

     

    It is not yet official (this is the first time I write about) but - it is just a couple of days ago - I am the official project manager for the electronic part of a new product. Until now the company has worked with the Leeds University and other private groups with a EU and Scottish financial support developing some parts of the mechanics and optics for a new concept of reflex camera with two backs: one for digital (20 MegaPix) and one for analog film. The interesting aspect is that I have in mind to use as the computing engine of the system a Raspberry Pi 3 compute module around which I will build the design for lens management, shutter control, exposure and light and other innovative sensors, WiFi, Bluetooth and the UI parts (screen touch and LCD for the analog back.

    So it was already my idea to start with a PI3 computer module first "road test" (unofficial until now) and next week I will contact also some other people of Element14 and raspberry pi.org to see their level of interest for a presentation of the project next July or September.

    As well as the PI3 computer module some parts will be commercial like the sensor, the lenses system, the shutter module etc. ut the entire machine architecture and the software / firmware / interfacing protocol (USB / WiFi / BLE) will be OSHW and Open Source.

     

    PONF Camera official site: https://ponfcamera.com/

     

    Enrico

Comment
  • Randall, this is a great opportunity image

     

    It is not yet official (this is the first time I write about) but - it is just a couple of days ago - I am the official project manager for the electronic part of a new product. Until now the company has worked with the Leeds University and other private groups with a EU and Scottish financial support developing some parts of the mechanics and optics for a new concept of reflex camera with two backs: one for digital (20 MegaPix) and one for analog film. The interesting aspect is that I have in mind to use as the computing engine of the system a Raspberry Pi 3 compute module around which I will build the design for lens management, shutter control, exposure and light and other innovative sensors, WiFi, Bluetooth and the UI parts (screen touch and LCD for the analog back.

    So it was already my idea to start with a PI3 computer module first "road test" (unofficial until now) and next week I will contact also some other people of Element14 and raspberry pi.org to see their level of interest for a presentation of the project next July or September.

    As well as the PI3 computer module some parts will be commercial like the sensor, the lenses system, the shutter module etc. ut the entire machine architecture and the software / firmware / interfacing protocol (USB / WiFi / BLE) will be OSHW and Open Source.

     

    PONF Camera official site: https://ponfcamera.com/

     

    Enrico

Children