Microchip CAN Bus Analyser Tool

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The APGDT002 is a CAN bus analyser tool intended to be a simple to use, low cost CAN bus monitor which can be used to develop and debug a high speed CAN network. The CAN analyser tool supports CAN 2.0b and ISO 11898-2 (high speed CAN with transmission rates of up to 1Mbit/s).

 

The tool can be connected to the CAN network using the DB9 connector or through a screw terminal interface. The CAN BUS analyser has the standard functionality expected in an industry tool such as trace, transmit, trace filter, log file capability, and group CAN message transmit. All of these features make it a very versatile tool, allowing fast and simple debugging in any high speed CAN network.

image

 

Features

  • Supports CAN 2.0b and ISO11898-2
  • Intuitive PC User Interface for functions such as configuration, trace, transmit, filter, log etc
  • Enhanced features in the PC GUI for PIC MCU support such as ECAN register view in the GUI
  • Direct access to CAN H and CAN L, CAN TX and CAN RX signals for robust debugging
  • Flexible CAN bus interface options i.e. standard DB9 connector or screw terminals
  • Software control of termination resistance and LED display for status, traffic, BUS error
Important Dates

Enrollment Begins: August 23 2017

Enrollment Ends: Oct 9 2017

RoadTesters Selected: Oct 16 2017 (estimated)

Product Shipped: Oct 13 2017

RoadTesting Begins: Oct 20 2017

Reminder/Update Email:Nov 20 2017*

Submit Reviews By: Dec 17 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants have been selected as official RoadTesters:

 

Terms & Conditions

Microchip CAN Bus Analyser Tool– RoadTest

Terms and Conditions

These are the terms and conditions which govern the Microchip CAN Bus Analyser Tool RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Microchip CAN Bus Analyser Tool

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 9 2017

Announcement of Winner (estimated): Oct 16  2017

 

Prize: Microchip CAN Bus Analyser Tool
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
  • , is Microchip available for questions on the device? I am trying the trigger connections and don't find doco on that.

     

    It says "The tool can also be set up to send out a pulse upon reception of certain CAN messages, which is useful during development or debugging issues with an oscilloscope."

    The doco doesn't explain it though and I don't find that functionality back int the software.

     

    Also would like them to explain the filter logic that's mentioned at the announcement of this roadtest ("Intuitive PC User Interface for functions such as [...] filter [...]"). Filter doesn't seem to be implemented with the device I got and the latest software.

Comment
  • , is Microchip available for questions on the device? I am trying the trigger connections and don't find doco on that.

     

    It says "The tool can also be set up to send out a pulse upon reception of certain CAN messages, which is useful during development or debugging issues with an oscilloscope."

    The doco doesn't explain it though and I don't find that functionality back int the software.

     

    Also would like them to explain the filter logic that's mentioned at the announcement of this roadtest ("Intuitive PC User Interface for functions such as [...] filter [...]"). Filter doesn't seem to be implemented with the device I got and the latest software.

Children
No Data