Microchip CAN Bus Analyser Tool

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The APGDT002 is a CAN bus analyser tool intended to be a simple to use, low cost CAN bus monitor which can be used to develop and debug a high speed CAN network. The CAN analyser tool supports CAN 2.0b and ISO 11898-2 (high speed CAN with transmission rates of up to 1Mbit/s).

 

The tool can be connected to the CAN network using the DB9 connector or through a screw terminal interface. The CAN BUS analyser has the standard functionality expected in an industry tool such as trace, transmit, trace filter, log file capability, and group CAN message transmit. All of these features make it a very versatile tool, allowing fast and simple debugging in any high speed CAN network.

image

 

Features

  • Supports CAN 2.0b and ISO11898-2
  • Intuitive PC User Interface for functions such as configuration, trace, transmit, filter, log etc
  • Enhanced features in the PC GUI for PIC MCU support such as ECAN register view in the GUI
  • Direct access to CAN H and CAN L, CAN TX and CAN RX signals for robust debugging
  • Flexible CAN bus interface options i.e. standard DB9 connector or screw terminals
  • Software control of termination resistance and LED display for status, traffic, BUS error
Important Dates

Enrollment Begins: August 23 2017

Enrollment Ends: Oct 9 2017

RoadTesters Selected: Oct 16 2017 (estimated)

Product Shipped: Oct 13 2017

RoadTesting Begins: Oct 20 2017

Reminder/Update Email:Nov 20 2017*

Submit Reviews By: Dec 17 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants have been selected as official RoadTesters:

 

Terms & Conditions

Microchip CAN Bus Analyser Tool– RoadTest

Terms and Conditions

These are the terms and conditions which govern the Microchip CAN Bus Analyser Tool RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Microchip CAN Bus Analyser Tool

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 9 2017

Announcement of Winner (estimated): Oct 16  2017

 

Prize: Microchip CAN Bus Analyser Tool
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
  •   wrote:

     

    I found some interesting information on the HP website about CAN.

    http://www.ni.com/pdf/manuals/370289k.pdf

    Not sure if it helps you or not.

    Thank you Mark. I've been checking for good explanations of CAN. The one in this document is rather short though. Less than one page to introduce CAN and LIN.

    There is more useful info in that document, often embedded in an explanation of a particular function in the LabVIEW CAN modules and software API (bus power requirements, possible fault situations, standard connector wiring, termination and cabling, timing!! , protocol features).

  • I found some interesting information on the HP website about CAN.

    http://www.ni.com/pdf/manuals/370289k.pdf

    Not sure if it helps you or not.

  • That handbook is a goldmine

    Glad someone else found it interesting.

    I have some bus signals to hack, and see if I can find out some data.

     

    As I indicated in my application

    My latest car has a few areas that need tweaking and while you can purchase an rather expensive box that connects and tweaks a couple of parameters, the software is limited, and not cheap.

    In my case there are a few other signals that need to be extracted and either displayed or captured for display.

     

    One of these is the APM where it shuts down to 4 cylinders. Some other makes have an indication, but sadly Chevrolet didn't provide this on a Camaro.

    There are a few other pieces of data that are best not mentioned here, but affect the performance, that I would like to tweak, but I'm not sure which module controls it.

    We've also talked about data logging and more specifically Geotracking.

    As I understand most modern vehicles have GPS data running around, so the ability to identify this data with a view to logging it is another feature to demonstrate.

    At the very least being able to log and pass on vehicle speed means that alarms systems can be designed to report to an owner when their vehicle is being moved without them on board.

     

    I was surprised that the GeoTracking devices plug into the OBD port. I presume the data is only there if the vehicle has GPS (an option on a Camaro).

     

    So if anyone else has some info to share, I'd be very interested.

     

    Mark

  • That handbook is a goldmine. Thanks .

  • I’m learning CAN. I have a few automotive microcontrollers. I’ve connected them via CAN on a logic level (skipping the physical layer). I’m now building CAN driver PCBs that implement that physical layer.

     

    My logic analyser doesn’t know about CAN. The Microchip analyser does, on the logic level and on the physical bus level. It will be a great help. It can even push messages on the bus, ideal for debugging.

  •   wrote:

     

    Thank you for the opportunity to road test this tool.  I currently have two projects I can use this with, a motor control project, and an actuator project.

     

    The motor control project is a equipment stabilization platform for use on research ships and is currently off the coast of California, but I have some parts I can test in the lab.

     

    The second project is an actuator controller for truck turbochargers using PICAN2 DUO.

     

    Scott

    interested in both. Especially the truck project. I worked in a truck factory as electronics prototyper in the 80’s and 90’s. The love is still strong image.

  • What were you intending to connect

  • Thanks to element14 for the chance to start digging into the inner workings of CAN bus.

    It also explains the email from UPS .... man that was quick.

     

     

    There was a comment earlier about ODB 2 to DB9 and I looked at the links.

    https://www.sparkfun.com/products/10087      USD$9.95 +p&p

    https://www.dfrobot.com/product-1309.html    USD$6.90 +p&p

    https://www.seeedstudio.com/DB9-to-OBD2-Cable-With-Switch-p-2872.html    USD$9.90 +p&p

     

    Luckily my local supplier was carrying one of the sparkfun leads and it's now on it's way.

     

     

    I think you were interested in CAN bus messages.

     

    I also picked up this link some time ago.

    https://hackaday.com/2016/06/23/books-you-should-read-the-car-hackers-handbook/

    and you can find it here

    Car Hacker's Handbook

     

     

    Cheers

    Mark

  • So happy. I'm working on a CAN series of blogs. This instrument will serve me well.

    Really looking forward to start using and assessing it.

     

     

     

    Note to self: submit PCB order now:

     

    image

  • Congratulations to the road testers. I am looking forward to reading the reviews.