Raspberry Pi 3 Camera Bundle

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The Raspberry Pi 3 Model B builds upon the features of its predecessors with a new, faster processor on board to increase its speed. It also features WiFi and Bluetooth Low Energy capabilities to enhance the functionality and the ability to power more powerful devices over the USB ports.

 

image

The Raspberry Pi Camera Module v2 is a high quality 8 megapixel Sony IMX219 image sensor custom designed add-on board for Raspberry Pi, featuring a fixed focus lens. It's capable of 3280 x 2464 pixel static images, and also supports 1080p30, 720p60 and 640x480p60/90 video. It attaches to Pi by way of one of the small sockets on the board upper surface and uses the dedicated CSi interface, designed especially for interfacing to cameras. The board itself is tiny, at around 25mm x 23mm x 9mm. It also weighs just over 3g, making it perfect for mobile or other applications where size and weight are important. It connects to Raspberry Pi by way of a short ribbon cable. The high quality Sony IMX219 image sensor itself has a native resolution of 8 megapixel, and has a fixed focus lens on-board. In terms of still images, the camera is capable of 3280 x 2464 pixel static images, and also supports 1080p30, 720p60 and 640x480p90 video.

image

Important Dates

Enrollment Begins: August 30 2017

Enrollment Ends: October 3 2017

RoadTesters Selected: Oct 10 2017 (estimated)

Product Shipped:Oct 6 2017

RoadTesting Begins: Oct 13 2017

Reminder/Update Email: Nov 12 2017*

Submit Reviews By: Dec 12 2017*

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The supplier chose the following applicants as official roadtesters:

 

Terms & Conditions

Raspberry Pi 3 Camera Bundle– RoadTest

Terms and Conditions

These are the terms and conditions which govern the Raspberry Pi 3 Camera Bundle RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Raspberry Pi 3 Camera Bundle

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 3 2017

Announcement of Winner (estimated): Oct 10  2017

 

Prize: Raspberry Pi 3 Camera Bundle