VeriSafe Panel-Mtd. Voltage Tester

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

As per the NFPA 70E, prior to the commencement of safety-related work an electrically safe work condition must be verified. One of the requirements of this verification is ensuring that a voltage verification test has been conducted to validate the absence of voltage.

 

 

This process includes a number of stages that can be complex and time-consuming when using hand-held portable test instruments. The VeriSafe™ Absence of Voltage Tester from Panduit simplifies this process by automating the voltage verification process.

image

 

The VeriSafe™ Absence of Voltage Tester minimizes risk by verifying the absence of voltage before equipment is accessed, making it easier for qualified electrical workers to determine an electrically safe environment in a fraction of the time compared to hand-held portable test instruments.

image

 

Once installed, a simple push of a button enables qualified electrical workers to verify the absence of voltage and see an active indication when the absence of voltage is confirmed. This provides a new and innovative way to safely, reliably, and efficiently verify the absence of voltage before accessing potentially dangerous electrical equipment.

 

By automating this process, the VeriSafe™ Absence of Voltage Tester provides the following:

  • Reduces the risk of exposure of electrical hazards for improved worker safety
  • Reduces testing procedure time and complexity to improve productivity
  • Supports compliance when used as part of the lockout/tagout process described in NFPA 70E.

 

Sample Applications of the VeriSafe™ Absence of Voltage Tester

image

 

 

Additional Information

NFPA 70E: Standard for Electrical Safety in the Workplace®

Important Dates

Enrollment Begins: Sept 14 2017

Enrollment Ends: Oct 23 2017

RoadTesters Selected: Nov 9 2017 (estimated)

Product Shipped: Nov 10 2017

RoadTesting Begins: Nov 17 2017

Reminder/Update Email: Dec 17 2017*

Submit Reviews By: Jan 16 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected for this roadtest:

 

Terms & Conditions

INDUSTRIAL: VeriSafe Absence of Voltage Tester– RoadTest

Terms and Conditions

These are the terms and conditions which govern the VeriSafe Absence of Voltage Tester RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

VeriSafe Absence of Voltage Tester

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 23 2017

Announcement of Winner (estimated): Oct 30  2017

 

Prize:VeriSafe Absence of Voltage Tester
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
Parents Comment
  • That's a very comprehensive document.

    It details a lot of what we used to cover with EST, but for some reason they sort of don't cover it.

     

    While the ladder in the swimming pool gets laughed at, the guy trapped in the chain of the drum is a more "makes you think" picture.

     

    Lately H&S has gone overboard to the point of excess.

    I'm not condoning bad or unsafe practices, but the noise being generated from all the minor H&S hype is clouding the much more serious stuff.

     

    Mark

Children
  • @

     

    Hello Mark,

    Oh yes, that's is often. But here is nothing to laughing.
    In this pdf the man in the chain this is a very strong point.
    I thought about a long time whether to write it here or not ...

    When I saw the picture, I had to look a bit to the side, so I could handle it,

    because in detail you can see how the poor man is possibly dying and his

    colleague is watching and unfortunately can not really help, except calm.

     

    I've been working a lot on building site construction, have seen a lot,

    but this picture has been the most horrific picture so far.

    Every day I talk to my colleagues, also to myself:

    "Take care, pay attention to safety, that's in the first place before you start working."

    That was it what I wanted to write this from that pdf.

     

    Gerald

    ---

     

  • "Take care, pay attention to safety, that's in the first place before you start working."


    I agree 100%