STM Discovery Board for Makers

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The STM32F769I-DISCO is a discovery kit with STM32F769NI microcontroller. This MCU has 2Mbytes of flash, 512+16+4 Kbytes of RAM & comes in 216 pin BGA package. Discovery kit allows user to develop, share applications with STM327 series microcontrollers based on ARM Cortex-M7 core. Kit enables a wide diversity of applications taking benefit from audio multi sensor support, graphics, security, video and high speed connectivity features. The Arduino connectivity support provides unlimited expansion capabilities with a large choice of specialized add-on boards. It has on-board ST-LINK/V2-1 supporting USB reenumeration capability, USB ST-LINK functions such as virtual COM port, mass storage and debug port, 2 audio line jacks, 1 for input & 1 for output and stereo speaker outputs, 4 ST MEMS microphones on DFSDM inputs, 2 SPDIF RCA input & output connectors, 2 push buttons (user and reset), 512Mbit quad-SPI flash memory, 128Mbit SDRAM, connector for microSD card.

 

image

Front

 

image

Back

 

Features

  • USB OTG HS with Micro-AB connector, SAI audio codec
  • Ethernet connector compliant with IEEE-802.3-2002
  • 5 power supply options, ST LINK/V2-1, USB HS connector, 5V from RJ45 (power over Ethernet)
  • Power over Ethernet based on IEEE 802.3af (powered device, 48V to 5V, 3W)
  • 5V from Arduino or external connector, USB charger
  • Power supply output for external applications is 3.3V or 5V, Arduino Uno V3 connectors
  • Compatible with windows OS (XP, 7, 8) or linux 64-bit or OS X
  • Supports Keil, IAR and GCC-based IDEs (free AC6: SW4STM32, Atollic TrueSTUDIO) development tools
  • WIFI or Ext-EEP daughterboard connector

 

Additional Information

Discovery kit with STM32F769NI MCU

Important Dates

Enrollment Begins: Sept 15 2017

Enrollment Ends: Nov 1 2017

RoadTesters Selected: Oct 8 2017

Product Shipped: Nov 2 2017

RoadTesting Begins: Nov 9 2017

Reminder/Update Email: Dec 9 2017*

Submit Reviews By: Jan 8 2018**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected as official roadtesters:

 

Terms & Conditions

32F769IDISCOVERY RoadTest

Terms and Conditions

These are the terms and conditions which govern the 32F769IDISCOVERY RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

32F769IDISCOVERY

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Nov 1 2017

Announcement of Winner (estimated): Nov 8  2017

 

Prize:  32F769IDISCOVERY
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
  • Well Tim,

                  I am sorry you feel that way I have been apart of the community for some time now and yes this will be my 3rd roadtest which I am excited for.   Now it is not about you me or anyone else.  The only one it is about is the supplier and their needs and what they want.  Sometimes what we want to do with a board or other item  listed on the roadtest is really not what they want so they go on to the next just because the project seems exciting new and fresh to you it might not be to them.

     

    Since looking at your profile you have just recently joined and have started posting and all in the roadtest here.  Start taking part in groups become a helpful and thoughtful member of the community before you start slamming something it just shows how ignorant and such a poor looser you are. 

     

    Using curse words in your response to those picked shows exactly why to me you where not chosen.  And as well it looks like you didn't submit your application correctly if you had done one.

     

    Now my apologies and don't mean to offend you if I have done so this far was not my attention.

     

    When I first started applying for road tests I was doing actually what Randall posted above really short blurbs and not going into description of any of my intent for the product.  I will use an example.   On a recent roadtest a user was given a product a really expensive product and all they did was basically take a few photos and wrote what was on the box.  Because really the roadtest page had more information listed about the product then their roadtest.  No actual test where done.

    So would this make a supplier happy?  would it make me want to buy the item?  would it make me want to continue to send e14 items for review.    Chances are all those are a no.   This is not what the intent of the program is for as they have people to do reviews on youtube and other social media but they want to allow for our community members to get involved with their product and review and discuss it.  So that leads me to the social media aspect the person was a new member with no posting found on any social media site at all.   Check my instagram youtube twitter facebook and website your gonna see me talking about my roadtests and projects that I have on the go with element14.com   Because really they could just send everything to Ben for review and scrap us. 

     

    So if you see where I am going with this great if your first response is "whatever".  Then that's fine too you can say whatever you like about E14.com but the users will just laugh at you because your statement is completely funny and not warranted.

     

    Just so you know I have applied for many roadtests and have only gotten a few. Sure it disappoints me but life goes on and I always have more projects ready to go.

     

    My tips for any NEW applicants is:

     

    1. Make sure to be detailed on your application and your intent for the device/product.
    2. Feel free to let the supplier know how they would benefit from you taking part in the roadtest.
    3. Be different.
    4. if you application is only 2 sentences or less time to spend more time on it.
    5. Remember they are giving you product for free (if it was something I made I would make sure its going to the right people)
    6. Remember there is more then one roadtest to take part in.
    7. Don't post your frustration about the decisions (gets old)
    8. Read those rules and check out the threads on making your roadtest.

     

    Now another think I would like to mention is when some road testers have completed their roadtest they are done with that board it goes back into the box or bag and sits there most are willing to trade or share their stuff.

    Along with their knowledge.

     

    I know this is a bit much to be posting in a road test spot here and if possible to have this thread cleaned up.

     

    There is no scam its equal opportunity here on the roadtests and its up to you to get the suppliers attention once its been passed on to them.

     

    I hope you take the time to look back and realize how silly your post there was on my comment as it was inappropriate and uncalled for and I didn't appreciate it. 

     

    So my final words, don't be discouraged if you don't get in the first time or 8 or 9th like me.  Learn from your previous applications and grow from there.

     

    Best of luck to everyone and hope to see some great roadtest reviews here on this board.

  • Hello,

     

    I have received this email in error; I’m not Tim, my name is Angela and the Element 14 road tester TamarB).

     

    This is the second email today along similar lines.

     

    Thank you, Angela

  • Since you were selected as a roadtester any posts from here will get emailed to you Angela.  Any updates/news or changes, this is a typical thing to happen when accepted into a roadtest.  Check the page STM Discovery Board for Makers  and you will see.

Comment Children
No Data