STM Discovery Board for Makers

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The STM32F769I-DISCO is a discovery kit with STM32F769NI microcontroller. This MCU has 2Mbytes of flash, 512+16+4 Kbytes of RAM & comes in 216 pin BGA package. Discovery kit allows user to develop, share applications with STM327 series microcontrollers based on ARM Cortex-M7 core. Kit enables a wide diversity of applications taking benefit from audio multi sensor support, graphics, security, video and high speed connectivity features. The Arduino connectivity support provides unlimited expansion capabilities with a large choice of specialized add-on boards. It has on-board ST-LINK/V2-1 supporting USB reenumeration capability, USB ST-LINK functions such as virtual COM port, mass storage and debug port, 2 audio line jacks, 1 for input & 1 for output and stereo speaker outputs, 4 ST MEMS microphones on DFSDM inputs, 2 SPDIF RCA input & output connectors, 2 push buttons (user and reset), 512Mbit quad-SPI flash memory, 128Mbit SDRAM, connector for microSD card.

 

image

Front

 

image

Back

 

Features

  • USB OTG HS with Micro-AB connector, SAI audio codec
  • Ethernet connector compliant with IEEE-802.3-2002
  • 5 power supply options, ST LINK/V2-1, USB HS connector, 5V from RJ45 (power over Ethernet)
  • Power over Ethernet based on IEEE 802.3af (powered device, 48V to 5V, 3W)
  • 5V from Arduino or external connector, USB charger
  • Power supply output for external applications is 3.3V or 5V, Arduino Uno V3 connectors
  • Compatible with windows OS (XP, 7, 8) or linux 64-bit or OS X
  • Supports Keil, IAR and GCC-based IDEs (free AC6: SW4STM32, Atollic TrueSTUDIO) development tools
  • WIFI or Ext-EEP daughterboard connector

 

Additional Information

Discovery kit with STM32F769NI MCU

Important Dates

Enrollment Begins: Sept 15 2017

Enrollment Ends: Nov 1 2017

RoadTesters Selected: Oct 8 2017

Product Shipped: Nov 2 2017

RoadTesting Begins: Nov 9 2017

Reminder/Update Email: Dec 9 2017*

Submit Reviews By: Jan 8 2018**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants were selected as official roadtesters:

 

Terms & Conditions

32F769IDISCOVERY RoadTest

Terms and Conditions

These are the terms and conditions which govern the 32F769IDISCOVERY RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

32F769IDISCOVERY

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Nov 1 2017

Announcement of Winner (estimated): Nov 8  2017

 

Prize:  32F769IDISCOVERY
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
  • Wow! Awesome! Thank you Randall and STM!  I cant wait to get my hands on it....should be a fun time.

  • What a load of *** three of those people have been testers in the past

  •  

    Three people may have been testers before.

    There is nothing saying each Road Test has to be fresh testers.

     

    Each applicant put in a proposal, after the ones that are in-ellligable to test have been removed, they are passed to the supplier to decide.

    This also happens with Design challenges.

     

     

    Can I presume from the comment that you applied and were not selected.?

     

    Mark

  • Exactly unfair fix from your own words

  • There is nothing saying each Road Test has to be fresh testers

     

     

    Scam Alert posting everywhere social media

  • Hi Tim, this was quite a popular roadtest with nearly 60 applicants. There's many reasons why people are picked for roadtesting, it might be simply that the supplier wants to promote a particular usecase or they simply liked the style or approach of the application.

     

    There are a couple of other similar roadtests still recruiting. Think about how you can redo you application to have a better chance of getting to roadtest those.

    You need to think about how your roadtest can help the supplier and communtity.

    What can make your application stand out?

    How will your test be better than the others?

    What skills / ideas do you have that others dont?

     

    There are some tips for writing a good application here How to Write a Winning RoadTest Application

     

    Good luck with your next application.

  • Oh our man Tim is well versed with the document you linked.

    This was the comment he posted ....

     

    image

     

    Sadly I think the proper term for the participation to date is "Trolling"

     

    Even the responses to my comment are nonsense and I'm finding it hard to link

    Exactly unfair fix from your own words

    to something I put in my comment ....

     

    Cheers

    Mark

  • Quite true Mark but there's still another 52 applicants who may want to apply for the other road tests and could do with some hints on how they can do a better roadtest application and report.

     

    Cypress PSoCRegistered 6 BLE Pioneer Kit (CY8CKIT-062-BLE)

    STMicroelectronics Discovery Kit for IoT node

  • Tim,

     

    First off, I don't appreciate your foul language. State your opinion without resorting to expletives.

     

    I went back to the applicants. I do not see that you applied. Why not?

     

    Why don't you try applying and write a decent application and you will pop up to the short list of finalists.

     

    Roadtests are competitive. An applicant being selected a winner starts with a decent application. So, let's look at some applications. Here is what I get:

     

    Applicant 1. Not sure what you want here

     

    Applicant 2, I need to use the board for testing the possibility of the project

     

    Applicant3. j

     

    Applicant4. I would want to help road test this product by Seeing if it mets my companys standers

     

    Applicant5. I need to use the board for testing the possibility of the project

     

    Applicant6. Interested in helping the community while gaining exposure to products I may not be able to gain access to otherwise.

     

    Applicant7. I will be glad if selectred to test the product

     

    Applicant8. I want to learn how to develop PCBs.

     

    Applicant9. man there is a lot of room to write in here.  I'll just simply state you wont be dissapointed in allowing me to join in the RoadTest.   have a great day!

     

    Applicant10. I run a private industrial training institute with electrician trade.

     

    Applicant 11. nothing

     

    This is all they wrote, for heaven sakes!!! So, Tim, would you award the free kit to any of these 11 applicants above?

     

    Now, let';s look at the application of one of the winners (anonymously):

     

    Just about a month ago I backed the Librem 5 Phone developer kit (https://puri.sm/shop/librem-5/) to try my hand at developing GTK apps for the phone. When I saw this STM Discovery Board for Makers come across for Roadtest I was stoked! and thought of trying to build a phone with very basic features. My intention if selected for the Roadtest is to try out a couple of projects for which I will post as separate blog posts in addition to the Roadtest review.

     

    Project #1 – Build a basic phone – I have an Arduino GSM module(Seeed SLD01098P GPRS/GSM Shield V2.0) which I plan to use with a ting SIM card to build basic phone functionality, by taking advantage of the microphones on the board and hookup speaker to the audio jack. In addition I would like to add texting functionality using the screen on the board. Now I am not sure if the GSM module that I have will be compatible with the discovery board, so as a backup just in case I am not able to get the GSM module to work, I plan to use Twilio over wifi to achieve the functionality https://www.twilio.com. In addition, I would also like to add a feature to test connecting a USB web came to OTG connector to take picture and video and store it on a SD card, I have an old Logitech UVC camera handy for this. I had done a project a while back using a GSM module here is an image of the prototype, but with the Discovery Board the idea is to add a UI, you can read about this at - https://www.instructables.com/id/Arduino-Phone-for-Visually-Impaired/

    image

    Project #2 – Posting sensor data to AWS IoT/AZURE , as part of this project I would like to test posting data via GSM so that I can make the whole module mobile and take it around the city to compare the pollution level at various spots, for this I have Seeedstudio Gas sensor, Air quality sensor and Temperature sensor handy.  Here I am going to try and use AWS IoT, and if the GSM module does not work then I will fall back on my wifi router. I have previous experience in posting data to both AWS IoT and Azure IoT.

     

    In addition, per the documentation it mentions that the module is compatible with linux 64 bit, so this means I will also provide feedback/my experience on this, as I have Debain stretch installed on my laptop and Ubuntu 16.04 on my desktop.

    --

    Tim, this is a guy that has made an effort. He or she has demonstrated to me that he really wants to get this kit and do something with it. If an applicant puts this kind of effort in the application, she or he will be noticed.

     

    I always try to recommend new roadtesters to the supplier. If you have any more questions, feel free to contact me. I would love to have you participate in the RoadTest Program.

     

    Ranbdall Scasny

    RoadTest Program Manager

Comment
  • Tim,

     

    First off, I don't appreciate your foul language. State your opinion without resorting to expletives.

     

    I went back to the applicants. I do not see that you applied. Why not?

     

    Why don't you try applying and write a decent application and you will pop up to the short list of finalists.

     

    Roadtests are competitive. An applicant being selected a winner starts with a decent application. So, let's look at some applications. Here is what I get:

     

    Applicant 1. Not sure what you want here

     

    Applicant 2, I need to use the board for testing the possibility of the project

     

    Applicant3. j

     

    Applicant4. I would want to help road test this product by Seeing if it mets my companys standers

     

    Applicant5. I need to use the board for testing the possibility of the project

     

    Applicant6. Interested in helping the community while gaining exposure to products I may not be able to gain access to otherwise.

     

    Applicant7. I will be glad if selectred to test the product

     

    Applicant8. I want to learn how to develop PCBs.

     

    Applicant9. man there is a lot of room to write in here.  I'll just simply state you wont be dissapointed in allowing me to join in the RoadTest.   have a great day!

     

    Applicant10. I run a private industrial training institute with electrician trade.

     

    Applicant 11. nothing

     

    This is all they wrote, for heaven sakes!!! So, Tim, would you award the free kit to any of these 11 applicants above?

     

    Now, let';s look at the application of one of the winners (anonymously):

     

    Just about a month ago I backed the Librem 5 Phone developer kit (https://puri.sm/shop/librem-5/) to try my hand at developing GTK apps for the phone. When I saw this STM Discovery Board for Makers come across for Roadtest I was stoked! and thought of trying to build a phone with very basic features. My intention if selected for the Roadtest is to try out a couple of projects for which I will post as separate blog posts in addition to the Roadtest review.

     

    Project #1 – Build a basic phone – I have an Arduino GSM module(Seeed SLD01098P GPRS/GSM Shield V2.0) which I plan to use with a ting SIM card to build basic phone functionality, by taking advantage of the microphones on the board and hookup speaker to the audio jack. In addition I would like to add texting functionality using the screen on the board. Now I am not sure if the GSM module that I have will be compatible with the discovery board, so as a backup just in case I am not able to get the GSM module to work, I plan to use Twilio over wifi to achieve the functionality https://www.twilio.com. In addition, I would also like to add a feature to test connecting a USB web came to OTG connector to take picture and video and store it on a SD card, I have an old Logitech UVC camera handy for this. I had done a project a while back using a GSM module here is an image of the prototype, but with the Discovery Board the idea is to add a UI, you can read about this at - https://www.instructables.com/id/Arduino-Phone-for-Visually-Impaired/

    image

    Project #2 – Posting sensor data to AWS IoT/AZURE , as part of this project I would like to test posting data via GSM so that I can make the whole module mobile and take it around the city to compare the pollution level at various spots, for this I have Seeedstudio Gas sensor, Air quality sensor and Temperature sensor handy.  Here I am going to try and use AWS IoT, and if the GSM module does not work then I will fall back on my wifi router. I have previous experience in posting data to both AWS IoT and Azure IoT.

     

    In addition, per the documentation it mentions that the module is compatible with linux 64 bit, so this means I will also provide feedback/my experience on this, as I have Debain stretch installed on my laptop and Ubuntu 16.04 on my desktop.

    --

    Tim, this is a guy that has made an effort. He or she has demonstrated to me that he really wants to get this kit and do something with it. If an applicant puts this kind of effort in the application, she or he will be noticed.

     

    I always try to recommend new roadtesters to the supplier. If you have any more questions, feel free to contact me. I would love to have you participate in the RoadTest Program.

     

    Ranbdall Scasny

    RoadTest Program Manager

Children
  • Whatever, posting has been uploaded to Facebook and Youtube, fake scammers

    always the same people, 3 for sure.

    Don't contact me you guys are scammers

  • Fake Scammer, is that not a double negative and therefor a positive image

     

    We pretend to be a scammer but were fake so really were good guys

     

    Thanks for that...

     

    But seriously, new comers are selected frequently for roat tests, and they often will post a good review, but often will also just grab and run, successful road testers are also selected for more road tests as the vendors like what they see and trust they can do it again, but at the end of the day, it is down to your APPLICATION, if you dont apply then you can hardly complain... stop trolling and try co-operating, you might like the outcome

  • Hello Randall,

     

    I think the following email has come through to myself by mistake………….

     

    Kind regards,

     

    Anela

  • I'm not sure how you can call the folks associated with the Element14 RoadTests Scammers.   Element14 is not asking you for any money or buy anything and just ask the selected RoadTesters to post their experience and opinion of the product. You even get to keep the product for free after the RoadTest. How cool is that?

     

     

    Randall and the folks that run this are awesome and do a great job keeping things on track despite the number of RoadTests and other Projects that Element14 is running.  That must be a tough job.

     

    As far as the selection of the RoadTesters, it was my understanding that the Product vendor and others outside of Element14 were involved in selecting the folks that partake in a RoadTest.  If certain folks are selected repeatedly, I suspect it is due to both the Application they provided as well as other content they have posted on the Element14 web site.  It's sort of a guarantee that at least some folks that receive the RoadTest device will actually post something by the assigned due date, which can be quite challenging at times.

     

    I would suggest rather than get frustrated, look at the 3 repeat RoadTesters and see what they have posted in the past.  Heck, maybe even contact them to get advice as to how to improve your own application thus increasing your chances of being selected next time.