Review of Wolfson Microelectronics WM7110

Table of contents

RoadTest: Wolfson Microelectronics WM7110

Author: DAB

Creation date:

Evaluation Type: Independent Products

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: I am building a system to record and analyze thunder so I wanted to see if the MEMs technology was better than the current Electret.

What were the biggest problems encountered?: The website provided all of the documentation I needed. However, my initial test setup was incomplete, so I am building up a second one to conduct the tests.

Detailed Review:

September 17, 2011

You can read my final review in the attached word document.

To summarize, the new MEMS technology was much superior to the current Electret technology.  If you are designing a new audio device, take a good look at the Wolfston line.  They have a great product.

 

 

Road Test Report on Wolfson Microphone

by

Donald Bertke

 

 

I would like to thank Element 14 and Wolfson for providing their MEMS microphone board for testing.

 

Summary

 

The Wolfson microphone performed as specified, providing a nice flat response from 20Hz to 20KHz.  The detection sensitivity remained flat across the angle to the sound source from perpendicular to parallel (0 to 90 degrees).  The sound level detection at 1KHz was a good 10dBm better than the standard commercial Electret microphone.

 

I was amazed that a device this small was such an improvement over the current Electret devices in use.  The actual detection area for the MEMS device was roughly 1-mm squared compared to the Electret area of about 18-mm squared.  The MEMS device was better even though it was 18 times smaller.  No doubt about it, the MEMS technology will replace the Electret devices.  They are really superior in performance.  If they are priced close to the current devices, they should quickly replace the Electret devices in all applications.

 

Test Plan

 

After reviewing the Wolfson specifications, which were easy to find on line, I decided to compare the microphone with the current Electret microphone installed in most current commercial audio devices.

 

What I wanted to see was how it stacked up in Sensitivity, Bandwidth and Direction of signal reception.  To accomplish the tests, I decided to use my new UNO32 connected to my Dell laptop.

I would use identical transistor amplifiers for both microphones (I found the circuit in the new book "30 Arduino Projects for the Evil Scientist by Simon Morese.) and use the UNO32 to measure the detected values and send them to the Laptop for display.

To generate the sound, I used the software TRUERTA (www.trueaudio.com, by John L. Murphy, version 3.5.2.

 

Test 1

To measure the frequency bandwidth of the microphones, I put them side-by-side in front of the Laptop speaker and ran the TrueRTA software to output a signal from 20Hz to 20,000 Hz.  For each frequency, I let the UNO32 sample for several seconds and took the peak value measured from each microphone.

 

Test 2

To measure the angle to microphone sensitivity, I put both in the same configuration as for Test 1 and then I used a protractor to change the angle to the Speaker from 0 to 90 degrees.  As in test 1, I moved the angle and let the UNO32 sample and display the peak value over several seconds.

 

Test 3

To measure the sensitivity, I used the same configuration as for Test 1.  I set the software up to output a 1KHz tone and adjusted the output level to -60dbm.  I first recorded a no tone background level measurement.  I then increased the output level until I reached 0.0dbm, which was fully detectable by both microphones.

 

Test data

 

Test 1

Figure 1 graphically shows the bandwidth response across the frequencies.  Table 1 is the raw data I recorded during the test.  Watching the data as it was being measured, the Wolfson device was much quieter than the Electret.  The Electret measurements would be plus or minus 20%, where the Wolfson measurements were well within 5%.

 

As you can see from the data, both had a mostly flat response over the frequency range tested.

 

One issue I noticed was that the TrueRTA software output was not consistent from frequency to frequency, so I manually adjusted the output level so that the microphones saw the same peak to peak level for each frequency during the test.

 

Note, I could not figure out how to insert my excel graphs, sorry.

Figure 1, Frequency Response Test

 

Table 1, Frequency Peak Value Measurements

 

Frequency

Wolfson

Electret

20

249

280

40

256

275

60

260

280

80

268

270

100

270

292

200

295

296

300

293

288

400

273

278

500

285

307

600

277

280

700

315

300

800

293

300

900

312

322

1000

276

285

2000

277

274

3000

292

286

4000

282

280

5000

286

273

6000

277

289

7000

284

275

8000

259

250

9000

289

290

10000

320

290

11000

324

305

12000

275

275

13000

273

273

14000

324

272

15000

290

275

16000

286

274

17000

281

272

18000

292

277

19000

267

272

20000

305

271

 

 

Test 2

 

Figure 2 shows the signal detection by angle of alignment of the microphones to the speakers.  Since I used only one Frequency, there was no need to adjust the volume as I rotated the microphone position in relation to the speaker.

 

Again, the Electret measurements showed a decidedly high variation of signal measurement, where as the Wolfson held to a much tighter range of values.

 

Note, I could not figure out how to insert my excel graphs, sorry.

Figure 2, Angle to Source Measurements

 

Table 2, Angle to Source Measurements

 

Angle to Speaker

Wolfson

Electret

90

271

272

80

269

240

70

269

260

60

269

280

50

265

300

40

266

250

30

263

262

20

265

260

10

260

260

0

271

250

 

 

Test 3

 

Figure 3 shows the signal level sensitivity of both microphones at 1KHz, starting at no signal and then raising the output from -60dbm to 0.0dbm.

 

As in Test 1 and Test 2, the Electret showed wildly varying values during the measurements, where the Wolfson remained fairly steady.

 

Note, I could not figure out how to insert my excel graphs, sorry.

Figure 3, Sound Level Detection Measurements

 

Table 3, Sound Level Detection Measurements

 

Sound Level in DB

Wolfson

Electret

off

249

270

-60

249

271

-50

249

273

-40

249

272

-30

252

272

-20

264

272

-10

303

280

0

338

315

 

 

Test Results

 

In all three tests, the Wolfson MEMS microphone proved to be superior to a standard Electret microphone.  The MEMS technology was more sensitive, had a better angle to signal detection capability and demonstrated a flat response sensitivity from 20 to 20,000 Hz.

 

Based upon these measurements, the MEMS technology used by Wolfson has provided designers with a superior microphone in a much smaller package than is currently available with Electret technology.

 

August 2011

This is just my initial update.  After getting the two microphone chips, I researched the part and decided on a test plan.

1.  Check the sensitivity of the Wolfson device against a standard Electret microphone.

2.  Compare the frequency response for each microphone.

3.  Compare the angle of incidence sensitivity of each microphone.

 

I first tried to build my test rig without using amplifiers, but that did not work.  Therefore I have ordered the parts to build two equal amplifiers so that I do not inadvertantly give one of the microphones an advantage.  Once I get the parts in, I will run the tests and do the analysis.

 

So for now, all I can say is that the MEMs are much smaller than the Electrets, so it will be interesting to see if they are as good or better.

 

Thanks,

DAB

Anonymous
Parents
  • Here is my detailed review:

     

     
    Road Test Report on Wolfson Microphone
    by
    Donald Bertke
     
     
    I would like to thank Element 14 and Wolfson for providing their MEMS microphone board for testing.
     
    Summary
     
    The Wolfson microphone performed as specified, providing a nice flat response from 20Hz to 20KHz.  The detection sensitivity remained flat across the angle to the sound source from perpendicular to parallel (0 to 90 degrees).  The sound level detection at 1KHz was a good 10dBm better than the standard commercial Electret microphone.
     
    I was amazed that a device this small was such an improvement over the current Electret devices in use.  The actual detection area for the MEMS device was roughly 1-mm squared compared to the Electret area of about 18-mm squared.  The MEMS device was better even though it was 18 times smaller.  No doubt about it, the MEMS technology will replace the Electret devices.  They are really superior in performance.  If they are priced close to the current devices, they should quickly replace the Electret devices in all applications.
     
    Test Plan
     
    After reviewing the Wolfson specifications, which were easy to find on line, I decided to compare the microphone with the current Electret microphone installed in most current commercial audio devices.
     
    What I wanted to see was how it stacked up in Sensitivity, Bandwidth and Direction of signal reception.  To accomplish the tests, I decided to use my new UNO32 connected to my Dell laptop.
    I would use identical transistor amplifiers for both microphones (I found the circuit in the new book “30 Arduino Projects for the Evil Scientist by Simon Monk.) and use the UNO32 to measure the detected values and send them to the Laptop for display.
    To generate the sound, I used the software TRUERTA (www.trueaudio.com, by John L. Murphy, version 3.5.2.
     
    Test 1
    To measure the frequency bandwidth of the microphones, I put them side-by-side in front of the Laptop speaker and ran the TrueRTA software to output a signal from 20Hz to 20,000 Hz.  For each frequency, I let the UNO32 sample for several seconds and took the peak value measured from each microphone.
     
    Test 2
    To measure the angle to microphone sensitivity, I put both in the same configuration as for Test 1 and then I used a protractor to change the angle to the Speaker from 0 to 90 degrees.  As in test 1, I moved the angle and let the UNO32 sample and display the peak value over several seconds.
     
    Test 3
    To measure the sensitivity, I used the same configuration as for Test 1.  I set the software up to output a 1KHz tone and adjusted the output level to –60dbm.  I first recorded a no tone background level measurement.  I then increased the output level until I reached 0.0dbm, which was fully detectable by both microphones.
     
    Test data
     
    Test 1
    Figure 1 graphically shows the bandwidth response across the frequencies.  Table 1 is the raw data I recorded during the test.  Watching the data as it was being measured, the Wolfson device was much quieter than the Electret.  The Electret measurements would be plus or minus 20%, where the Wolfson measurements were well within 5%.
     
    As you can see from the data, both had a mostly flat response over the frequency range tested.
     
    One issue I noticed was that the TrueRTA software output was not consistent from frequency to frequency, so I manually adjusted the output level so that the microphones saw the same peak to peak level for each frequency during the test.
     
     
    Figure 1, Frequency Response Test
     
    Table 1, Frequency Peak Value Measurements
     
                    Frequency
                Wolfson
                 Electret
    20
    249
    280
    40
    256
    275
    60
    260
    280
    80
    268
    270
    100
    270
    292
    200
    295
    296
    300
    293
    288
    400
    273
    278
    500
    285
    307
    600
    277
    280
    700
    315
    300
    800
    293
    300
    900
    312
    322
    1000
    276
    285
    2000
    277
    274
    3000
    292
    286
    4000
    282
    280
    5000
    286
    273
    6000
    277
    289
    7000
    284
    275
    8000
    259
    250
    9000
    289
    290
    10000
    320
    290
    11000
    324
    305
    12000
    275
    275
    13000
    273
    273
    14000
    324
    272
    15000
    290
    275
    16000
    286
    274
    17000
    281
    272
    18000
    292
    277
    19000
    267
    272
    20000
    305
    271
     
     
    Test 2
     
    Figure 2 shows the signal detection by angle of alignment of the microphones to the speakers.  Since I used only one Frequency, there was no need to adjust the volume as I rotated the microphone position in relation to the speaker.
     
    Again, the Electret measurements showed a decidedly high variation of signal measurement, where as the Wolfson held to a much tighter range of values.
     
     
    Figure 2, Angle to Source Measurements
     
    Table 2, Angle to Source Measurements
     
          Angle to Speaker
               Wolfson
                 Electret
    90
    271
    272
    80
    269
    240
    70
    269
    260
    60
    269
    280
    50
    265
    300
    40
    266
    250
    30
    263
    262
    20
    265
    260
    10
    260
    260
    0
    271
    250
     
     
    Test 3
     
    Figure 3 shows the signal level sensitivity of both microphones at 1KHz, starting at no signal and then raising the output from –60dbm to 0.0dbm.
     
    As in Test 1 and Test 2, the Electret showed wildly varying values during the measurements, where the Wolfson remained fairly steady.
     
     
    Figure 3, Sound Level Detection Measurements
     
    Table 3, Sound Level Detection Measurements
     
         Sound Level in DB
                Wolfson
                 Electret
    off
    249
    270
    -60
    249
    271
    -50
    249
    273
    -40
    249
    272
    -30
    252
    272
    -20
    264
    272
    -10
    303
    280
    0
    338
    315
     
     
    Test Results
     
    In all three tests, the Wolfson MEMS microphone proved to be superior to a standard Electret microphone.  The MEMS technology was more sensitive, had a better angle to signal detection capability and demonstrated a flat response sensitivity from 20 to 20,000 Hz.
     
    Based upon these measurements, the MEMS technology used by Wolfson has provided designers with a superior microphone in a much smaller package than is currently available with Electret technology.
     
    Thanks,
    DAB
     
    PS, I will try to get the figures into this review.
Comment
  • Here is my detailed review:

     

     
    Road Test Report on Wolfson Microphone
    by
    Donald Bertke
     
     
    I would like to thank Element 14 and Wolfson for providing their MEMS microphone board for testing.
     
    Summary
     
    The Wolfson microphone performed as specified, providing a nice flat response from 20Hz to 20KHz.  The detection sensitivity remained flat across the angle to the sound source from perpendicular to parallel (0 to 90 degrees).  The sound level detection at 1KHz was a good 10dBm better than the standard commercial Electret microphone.
     
    I was amazed that a device this small was such an improvement over the current Electret devices in use.  The actual detection area for the MEMS device was roughly 1-mm squared compared to the Electret area of about 18-mm squared.  The MEMS device was better even though it was 18 times smaller.  No doubt about it, the MEMS technology will replace the Electret devices.  They are really superior in performance.  If they are priced close to the current devices, they should quickly replace the Electret devices in all applications.
     
    Test Plan
     
    After reviewing the Wolfson specifications, which were easy to find on line, I decided to compare the microphone with the current Electret microphone installed in most current commercial audio devices.
     
    What I wanted to see was how it stacked up in Sensitivity, Bandwidth and Direction of signal reception.  To accomplish the tests, I decided to use my new UNO32 connected to my Dell laptop.
    I would use identical transistor amplifiers for both microphones (I found the circuit in the new book “30 Arduino Projects for the Evil Scientist by Simon Monk.) and use the UNO32 to measure the detected values and send them to the Laptop for display.
    To generate the sound, I used the software TRUERTA (www.trueaudio.com, by John L. Murphy, version 3.5.2.
     
    Test 1
    To measure the frequency bandwidth of the microphones, I put them side-by-side in front of the Laptop speaker and ran the TrueRTA software to output a signal from 20Hz to 20,000 Hz.  For each frequency, I let the UNO32 sample for several seconds and took the peak value measured from each microphone.
     
    Test 2
    To measure the angle to microphone sensitivity, I put both in the same configuration as for Test 1 and then I used a protractor to change the angle to the Speaker from 0 to 90 degrees.  As in test 1, I moved the angle and let the UNO32 sample and display the peak value over several seconds.
     
    Test 3
    To measure the sensitivity, I used the same configuration as for Test 1.  I set the software up to output a 1KHz tone and adjusted the output level to –60dbm.  I first recorded a no tone background level measurement.  I then increased the output level until I reached 0.0dbm, which was fully detectable by both microphones.
     
    Test data
     
    Test 1
    Figure 1 graphically shows the bandwidth response across the frequencies.  Table 1 is the raw data I recorded during the test.  Watching the data as it was being measured, the Wolfson device was much quieter than the Electret.  The Electret measurements would be plus or minus 20%, where the Wolfson measurements were well within 5%.
     
    As you can see from the data, both had a mostly flat response over the frequency range tested.
     
    One issue I noticed was that the TrueRTA software output was not consistent from frequency to frequency, so I manually adjusted the output level so that the microphones saw the same peak to peak level for each frequency during the test.
     
     
    Figure 1, Frequency Response Test
     
    Table 1, Frequency Peak Value Measurements
     
                    Frequency
                Wolfson
                 Electret
    20
    249
    280
    40
    256
    275
    60
    260
    280
    80
    268
    270
    100
    270
    292
    200
    295
    296
    300
    293
    288
    400
    273
    278
    500
    285
    307
    600
    277
    280
    700
    315
    300
    800
    293
    300
    900
    312
    322
    1000
    276
    285
    2000
    277
    274
    3000
    292
    286
    4000
    282
    280
    5000
    286
    273
    6000
    277
    289
    7000
    284
    275
    8000
    259
    250
    9000
    289
    290
    10000
    320
    290
    11000
    324
    305
    12000
    275
    275
    13000
    273
    273
    14000
    324
    272
    15000
    290
    275
    16000
    286
    274
    17000
    281
    272
    18000
    292
    277
    19000
    267
    272
    20000
    305
    271
     
     
    Test 2
     
    Figure 2 shows the signal detection by angle of alignment of the microphones to the speakers.  Since I used only one Frequency, there was no need to adjust the volume as I rotated the microphone position in relation to the speaker.
     
    Again, the Electret measurements showed a decidedly high variation of signal measurement, where as the Wolfson held to a much tighter range of values.
     
     
    Figure 2, Angle to Source Measurements
     
    Table 2, Angle to Source Measurements
     
          Angle to Speaker
               Wolfson
                 Electret
    90
    271
    272
    80
    269
    240
    70
    269
    260
    60
    269
    280
    50
    265
    300
    40
    266
    250
    30
    263
    262
    20
    265
    260
    10
    260
    260
    0
    271
    250
     
     
    Test 3
     
    Figure 3 shows the signal level sensitivity of both microphones at 1KHz, starting at no signal and then raising the output from –60dbm to 0.0dbm.
     
    As in Test 1 and Test 2, the Electret showed wildly varying values during the measurements, where the Wolfson remained fairly steady.
     
     
    Figure 3, Sound Level Detection Measurements
     
    Table 3, Sound Level Detection Measurements
     
         Sound Level in DB
                Wolfson
                 Electret
    off
    249
    270
    -60
    249
    271
    -50
    249
    273
    -40
    249
    272
    -30
    252
    272
    -20
    264
    272
    -10
    303
    280
    0
    338
    315
     
     
    Test Results
     
    In all three tests, the Wolfson MEMS microphone proved to be superior to a standard Electret microphone.  The MEMS technology was more sensitive, had a better angle to signal detection capability and demonstrated a flat response sensitivity from 20 to 20,000 Hz.
     
    Based upon these measurements, the MEMS technology used by Wolfson has provided designers with a superior microphone in a much smaller package than is currently available with Electret technology.
     
    Thanks,
    DAB
     
    PS, I will try to get the figures into this review.
Children
No Data