Review of Agilent U1273AX Handheld Digital Multimeter

View table of contents ...  

RoadTest: Agilent U1273AX Handheld Digital Multimeter

Author: migration.user

Creation date:

Evaluation Type: Independent Products

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: FLUKE - 115

What were the biggest problems encountered?: Nearly perfect for me ! I would prefer a rechargeable system with li-po batteries...

Detailed Review:

Firstly I would like to thank Element14 and Agilent who gave me the opportunity to roadtest this multimeter !

The package include :

- Multimeter

- bluetooth module (shipped later by Agilent)

- Standard test leads

- test probes with 4-mm tips

- K-type thermocouple

- Lithium Batteries

 

The first impression is that multimeter is well ruggedized, IP-54 needed joint on rear door for batteries...

The Oled display is quite readable even outdoor in direct sunlight conditions ! I didn"t have any test with negative temperatures and condensation but it seems ready to support harsh environemental conditions.

 

The overall size is a bit bigger than my current multimeter but its quite easy to handle.

I did some tests with capacitor measurement and it seems quite accurate.

I had some tests also with the thermocouple... and got a very accurate temperature also, very close to our reference calibrated thermometer.

I didn't have any tests with the bluetooth module yet but I prefer to log measurement directly on my computer Lab rather than on android gadgets !

Reading docs show that bluetooth protocol is spp and Agilent GUI Data Logger can be found here : http://www.home.agilent.com/agilent/software.jspx?cc=FR&lc=fre&ckey=878442&nid=-536902463.803464.02&id=878442&cmpid=zzfindhh-logger

This one shows the setup of the module : http://cp.literature.agilent.com/litweb/pdf/U1177-90101.pdf

And this one the configuration guide : http://cp.literature.agilent.com/litweb/pdf/U1177-90002.pdf

To conclude this multimeter is very well rugedized and ready for the worst temperatures (-40 to 55°c)  and humitdity conditions (80%RH)  ! The display is quite readable in direct sunlight.

The interface is quite usual, I didn't felt lost in settings.

The lithium batteries offers long time but I would prefer rechargeables ones... but not sure to find batteries for this temperature range.




Anonymous