RoadTest: Fluke 190 Series Oscilloscope
Author: migration.user
Creation date:
Evaluation Type: Independent Products
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?:
What were the biggest problems encountered?: The power adapter isn't compatible with the local line voltage (here 230V is use, insead of 120V)
Detailed Review:
Package Content:
The scope came in a cardboard box, and inside I found a nice hard case.
Besides the scope itself, the hard case contained the following:
Some important feature:
Connect and view feature:
This feature sets the trigger automatically and when the signal is changes, this feature automatically adjusted the trigger again.
Eligible bandwidth
If you work in a noisy envionment such as high power inverters, or with a noisy waveforms the eligible bandwidth is a good feature. You can choose 3 different bandwidth, 20kHz, 20MHz or 200MHz. It can supress the high frequeny noise. The other way to supress the noise is the averaging function. With this function you can average 2, 4, 8, or 64 consecutive acquistions.
Automatic scope measurements
This scope offers a wide range of automatic measurement. You can choose up to four of the following measurement:
Spectrum function
You can select either input to the spectrum function, and you can select three type window (Hanning, Hamming or auto), but the user manual recommend the auto windowing function, because it automatically adapt the part of the signal to a complete number of cycles. This reduces the side-lobes.
100 most recent screen
The scope automatically stores the 100 most recent screens and when you press the hold key, the memory contents are frozen. After this, if you use the replay button you can step back through the stored screens.
Zoom function and cursor measurements
You can measure time, frequency, amplitude with te cursor function.
Rise time measurement
If you choose the auto mode the upper and the lower cursor will automatically move to the trace high, and the reading will display the rise time between te 10% and the 100%.
Connectivity
The scope has two USB connector. The first is a USB host connector to connect a USB stick. It only can handles the stick of maximum 2GB. You can use this port to save screens in .bmp format..
The other connector is a mini-USB connector which allowes you to connect the scope direct to the PC. To use this feature you have to install the FlukeView software, the software is allowes make screen shots, and remote control the scope.
Battery capacity
The scope runs approximately 400 minutes with a full charged battery.
-
DAB
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
-
Former Member
in reply to DAB
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Comment-
Former Member
in reply to DAB
-
Cancel
-
Up
0
Down
-
-
Reply
-
More
-
Cancel
Children